<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>PowerQUICC ProcessorsのトピックMPC855T versus MPC860DP</title>
    <link>https://community.nxp.com/t5/PowerQUICC-Processors/MPC855T-versus-MPC860DP/m-p/1243660#M3591</link>
    <description>&lt;P&gt;Is the MPC860DP pin for pin compatible with the MPC855T?&amp;nbsp; The MPC855T is now on LTB, but the MPC860DP still is ACTIVE.&amp;nbsp; Basically I need to replace the MPC855T with either a drop-in equivalent or do a PCB spin and port the code to the next closest variant.&amp;nbsp; Can someone please give me advise on this?&amp;nbsp; Also, if the MPC860DP can be used, how long will it be available?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
    <pubDate>Wed, 10 Mar 2021 22:43:36 GMT</pubDate>
    <dc:creator>steven_keeter</dc:creator>
    <dc:date>2021-03-10T22:43:36Z</dc:date>
    <item>
      <title>MPC855T versus MPC860DP</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/MPC855T-versus-MPC860DP/m-p/1243660#M3591</link>
      <description>&lt;P&gt;Is the MPC860DP pin for pin compatible with the MPC855T?&amp;nbsp; The MPC855T is now on LTB, but the MPC860DP still is ACTIVE.&amp;nbsp; Basically I need to replace the MPC855T with either a drop-in equivalent or do a PCB spin and port the code to the next closest variant.&amp;nbsp; Can someone please give me advise on this?&amp;nbsp; Also, if the MPC860DP can be used, how long will it be available?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Wed, 10 Mar 2021 22:43:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/MPC855T-versus-MPC860DP/m-p/1243660#M3591</guid>
      <dc:creator>steven_keeter</dc:creator>
      <dc:date>2021-03-10T22:43:36Z</dc:date>
    </item>
  </channel>
</rss>