<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MPC8349E Boot ROM and Reset Configuration Words in PowerQUICC Processors</title>
    <link>https://community.nxp.com/t5/PowerQUICC-Processors/MPC8349E-Boot-ROM-and-Reset-Configuration-Words/m-p/1233999#M3561</link>
    <description>&lt;P&gt;I am considering using parallel NOR flash connected through local bus GPCM for storing MPC8349E's booting image and reset configuration words.&lt;/P&gt;&lt;P&gt;According to the reference manual, there are examples of EEPROMs for storing the boot ROM and reset configuration words.&lt;/P&gt;&lt;P&gt;I wonder if I must use the EEPROM or if I can use the equivalent nonvolatile memory, such as the aforementioned NOR flash.&lt;/P&gt;</description>
    <pubDate>Mon, 22 Feb 2021 00:23:18 GMT</pubDate>
    <dc:creator>youngho_cho</dc:creator>
    <dc:date>2021-02-22T00:23:18Z</dc:date>
    <item>
      <title>MPC8349E Boot ROM and Reset Configuration Words</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/MPC8349E-Boot-ROM-and-Reset-Configuration-Words/m-p/1233999#M3561</link>
      <description>&lt;P&gt;I am considering using parallel NOR flash connected through local bus GPCM for storing MPC8349E's booting image and reset configuration words.&lt;/P&gt;&lt;P&gt;According to the reference manual, there are examples of EEPROMs for storing the boot ROM and reset configuration words.&lt;/P&gt;&lt;P&gt;I wonder if I must use the EEPROM or if I can use the equivalent nonvolatile memory, such as the aforementioned NOR flash.&lt;/P&gt;</description>
      <pubDate>Mon, 22 Feb 2021 00:23:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/MPC8349E-Boot-ROM-and-Reset-Configuration-Words/m-p/1233999#M3561</guid>
      <dc:creator>youngho_cho</dc:creator>
      <dc:date>2021-02-22T00:23:18Z</dc:date>
    </item>
    <item>
      <title>Re: MPC8349E Boot ROM and Reset Configuration Words</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/MPC8349E-Boot-ROM-and-Reset-Configuration-Words/m-p/1234026#M3562</link>
      <description>&lt;P&gt;Parallel NOR Flash can be used.&lt;/P&gt;
&lt;P&gt;Please refer to the MPC8349EA PowerQUICC II Pro Integrated Host Processor Family Reference Manual, &lt;EM&gt;4.3.2 Reset Configuration Words&lt;/EM&gt;:&lt;/P&gt;
&lt;P&gt;"The reset configuration words are loaded from the &lt;STRONG&gt;local bus&lt;/STRONG&gt; or from the I2C interface or from hard-coded values during the power-on or hard reset flows."&lt;/P&gt;
&lt;P&gt;&lt;EM&gt;4.3.1.1 Reset Configuration Word Source&lt;/EM&gt;:&lt;/P&gt;
&lt;P&gt;CFG_RESET_SOURCE[0:2] = 000&amp;nbsp; (Reset configuration word is loaded from a local bus EEPROM.)&lt;/P&gt;
&lt;P&gt;&lt;EM&gt;4.3.3.1 Loading from Local Bus EEPROM&lt;/EM&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 22 Feb 2021 02:15:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/MPC8349E-Boot-ROM-and-Reset-Configuration-Words/m-p/1234026#M3562</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2021-02-22T02:15:50Z</dc:date>
    </item>
  </channel>
</rss>