<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic T2080 EMI2 in PowerQUICC Processors</title>
    <link>https://community.nxp.com/t5/PowerQUICC-Processors/T2080-EMI2/m-p/1229934#M3554</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am working on a T2080 board, and I am experimenting some issues with the EMI2 bus.&lt;/P&gt;&lt;P&gt;I have a 10GB phy connected to one of the XFI interfaces of the SerDes, and the MDIO/MDC signals to the EMI2 bus.&lt;BR /&gt;In the same design I have two 1Gb phys connected to the EMI1.&lt;BR /&gt;I am finding that from uboot, I can 'find' the two phys on the EMI1 bus, but nothing from the EMI2.&lt;BR /&gt;I am measuring with an oscilloscope the signals, to check the integrity. The MDC signal is okey, and what I am experimenting is that MDIO has no movement when executing 'mii info'. This signal is always at 1V2, due to the pull up of the line.&lt;BR /&gt;What could be the issue? Eventhough the PHY configuration is wrong, it shouldn't affect to the MDIO/MDC bus, right?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Here's the commands on uboot:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;=&amp;gt; mii dev FSL_MDIO0&lt;BR /&gt;=&amp;gt; mii info&lt;BR /&gt;PHY 0x06: OUI = 0x0885, Model = 0x22, Rev = 0x02, 10baseT, HDX&lt;BR /&gt;PHY 0x07: OUI = 0x0885, Model = 0x22, Rev = 0x02, 10baseT, HDX&lt;BR /&gt;=&amp;gt; mii dev FM_TGEC_MDIO&lt;BR /&gt;=&amp;gt; mii info&lt;BR /&gt;=&amp;gt;&lt;BR /&gt;=&amp;gt; mii info&lt;BR /&gt;=&amp;gt; mii info&lt;BR /&gt;=&amp;gt; mii info 0&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you in advance!&lt;/P&gt;</description>
    <pubDate>Thu, 11 Feb 2021 15:07:26 GMT</pubDate>
    <dc:creator>paulagarcía-mor</dc:creator>
    <dc:date>2021-02-11T15:07:26Z</dc:date>
    <item>
      <title>T2080 EMI2</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/T2080-EMI2/m-p/1229934#M3554</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am working on a T2080 board, and I am experimenting some issues with the EMI2 bus.&lt;/P&gt;&lt;P&gt;I have a 10GB phy connected to one of the XFI interfaces of the SerDes, and the MDIO/MDC signals to the EMI2 bus.&lt;BR /&gt;In the same design I have two 1Gb phys connected to the EMI1.&lt;BR /&gt;I am finding that from uboot, I can 'find' the two phys on the EMI1 bus, but nothing from the EMI2.&lt;BR /&gt;I am measuring with an oscilloscope the signals, to check the integrity. The MDC signal is okey, and what I am experimenting is that MDIO has no movement when executing 'mii info'. This signal is always at 1V2, due to the pull up of the line.&lt;BR /&gt;What could be the issue? Eventhough the PHY configuration is wrong, it shouldn't affect to the MDIO/MDC bus, right?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Here's the commands on uboot:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;=&amp;gt; mii dev FSL_MDIO0&lt;BR /&gt;=&amp;gt; mii info&lt;BR /&gt;PHY 0x06: OUI = 0x0885, Model = 0x22, Rev = 0x02, 10baseT, HDX&lt;BR /&gt;PHY 0x07: OUI = 0x0885, Model = 0x22, Rev = 0x02, 10baseT, HDX&lt;BR /&gt;=&amp;gt; mii dev FM_TGEC_MDIO&lt;BR /&gt;=&amp;gt; mii info&lt;BR /&gt;=&amp;gt;&lt;BR /&gt;=&amp;gt; mii info&lt;BR /&gt;=&amp;gt; mii info&lt;BR /&gt;=&amp;gt; mii info 0&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you in advance!&lt;/P&gt;</description>
      <pubDate>Thu, 11 Feb 2021 15:07:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/T2080-EMI2/m-p/1229934#M3554</guid>
      <dc:creator>paulagarcía-mor</dc:creator>
      <dc:date>2021-02-11T15:07:26Z</dc:date>
    </item>
    <item>
      <title>Re: T2080 EMI2</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/T2080-EMI2/m-p/1230189#M3555</link>
      <description>&lt;P&gt;It seems that there is an issue with U-Boot which has to be debugged.&lt;/P&gt;
&lt;P&gt;On the T2080RDB I see:&lt;/P&gt;
&lt;P&gt;=&amp;gt; mdio list&lt;/P&gt;
&lt;P&gt;FSL_MDIO0:&lt;/P&gt;
&lt;P&gt;1 - RealTek RTL8211E &amp;lt;--&amp;gt; FM1@DTSEC3&lt;/P&gt;
&lt;P&gt;2 - RealTek RTL8211E &amp;lt;--&amp;gt; FM1@DTSEC4&lt;/P&gt;
&lt;P&gt;FM_TGEC_MDIO:&lt;/P&gt;
&lt;P&gt;0 - Generic 10G PHY &amp;lt;--&amp;gt; FM1@TGEC3&lt;/P&gt;
&lt;P&gt;1 - Generic 10G PHY &amp;lt;--&amp;gt; FM1@TGEC4&lt;/P&gt;
&lt;P&gt;12 - Cortina CS4315/CS4340 &amp;lt;--&amp;gt; FM1@TGEC1&lt;/P&gt;
&lt;P&gt;13 - Cortina CS4315/CS4340 &amp;lt;--&amp;gt; FM1@TGEC2&lt;/P&gt;
&lt;P&gt;=&amp;gt; mdio read FM_TGEC_MDIO 0 1.0&lt;/P&gt;
&lt;P&gt;Reading from bus FM_TGEC_MDIO&lt;/P&gt;
&lt;P&gt;PHY at address 0:&lt;/P&gt;
&lt;P&gt;1.0 - 0x2040&lt;/P&gt;
&lt;P&gt;=&amp;gt; mdio read FM_TGEC_MDIO 1 1.0&lt;/P&gt;
&lt;P&gt;Reading from bus FM_TGEC_MDIO&lt;/P&gt;
&lt;P&gt;PHY at address 1:&lt;/P&gt;
&lt;P&gt;1.0 - 0x2040&lt;/P&gt;
&lt;P&gt;=&amp;gt;&lt;/P&gt;</description>
      <pubDate>Fri, 12 Feb 2021 06:14:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/T2080-EMI2/m-p/1230189#M3555</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2021-02-12T06:14:22Z</dc:date>
    </item>
  </channel>
</rss>