<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: switching between QUICC slow and fast protocols in PowerQUICC Processors</title>
    <link>https://community.nxp.com/t5/PowerQUICC-Processors/switching-between-QUICC-slow-and-fast-protocols/m-p/1179428#M3463</link>
    <description>&lt;P&gt;1) The QEIWRM provides switching between protocol steps for all processors mentioned on the title page. (Only the MSC8144/MSC815x has bit numbering feature). Notice the LS1021A QUICC engine-lite is a Big-endian block.&lt;/P&gt;
&lt;P&gt;2) I am not sure what do you mean. The QEIWRM 6.8.5 Switching Protocols provides these steps. As code example see Example 25-1. QMC Re-Initialization Example in the QEIWRM (The QMC is a UCC slow protocol like the UART)&lt;/P&gt;
&lt;P&gt;3) What source code do you mean? I guess you mean some Linux driver source. In any case I am not driver programmer. I have never met any driver that can support UART and HDLC on the same port.&lt;/P&gt;</description>
    <pubDate>Mon, 09 Nov 2020 06:08:12 GMT</pubDate>
    <dc:creator>r8070z</dc:creator>
    <dc:date>2020-11-09T06:08:12Z</dc:date>
    <item>
      <title>switching between QUICC slow and fast protocols</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/switching-between-QUICC-slow-and-fast-protocols/m-p/1177877#M3456</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We were working on LS1021-atwr. We are working in QE engine drivers. I tested UCC_UART and HDLC in 2 different ports. Our actual requirement is to have both in the same port.My questions are&lt;/P&gt;&lt;P&gt;1) Did switching between protocol steps are same for all the processors? Don't know how to call pushsched command in ls1021.&lt;/P&gt;&lt;P&gt;2) Can anyone share the steps for LS1021-atwr for switching between same protocols?&lt;/P&gt;&lt;P&gt;3) In which source code, do I needs to implement switching between protocols steps mentioned in QEIWRM?&lt;/P&gt;</description>
      <pubDate>Wed, 04 Nov 2020 10:23:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/switching-between-QUICC-slow-and-fast-protocols/m-p/1177877#M3456</guid>
      <dc:creator>m_syed_ahmed</dc:creator>
      <dc:date>2020-11-04T10:23:40Z</dc:date>
    </item>
    <item>
      <title>Re: switching between QUICC slow and fast protocols</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/switching-between-QUICC-slow-and-fast-protocols/m-p/1179428#M3463</link>
      <description>&lt;P&gt;1) The QEIWRM provides switching between protocol steps for all processors mentioned on the title page. (Only the MSC8144/MSC815x has bit numbering feature). Notice the LS1021A QUICC engine-lite is a Big-endian block.&lt;/P&gt;
&lt;P&gt;2) I am not sure what do you mean. The QEIWRM 6.8.5 Switching Protocols provides these steps. As code example see Example 25-1. QMC Re-Initialization Example in the QEIWRM (The QMC is a UCC slow protocol like the UART)&lt;/P&gt;
&lt;P&gt;3) What source code do you mean? I guess you mean some Linux driver source. In any case I am not driver programmer. I have never met any driver that can support UART and HDLC on the same port.&lt;/P&gt;</description>
      <pubDate>Mon, 09 Nov 2020 06:08:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/switching-between-QUICC-slow-and-fast-protocols/m-p/1179428#M3463</guid>
      <dc:creator>r8070z</dc:creator>
      <dc:date>2020-11-09T06:08:12Z</dc:date>
    </item>
  </channel>
</rss>