<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>PowerQUICC Processorsのトピックrandom: nonblocking pool is initialized</title>
    <link>https://community.nxp.com/t5/PowerQUICC-Processors/random-nonblocking-pool-is-initialized/m-p/1175219#M3438</link>
    <description>&lt;P&gt;I am having a T1022 processor based board, the uboot is booting from spi and nand flash is used to boot kernel, device tree and file system. When i am booting kernel from nand flash it sometimes got struck in kernel. This behavior is very frequent . Please look into the attached kernel log for reference.&lt;/P&gt;&lt;P&gt;Processor : T1022&lt;/P&gt;&lt;P&gt;Nand flash - Micron MT29F8G08ABBCAH4&lt;/P&gt;&lt;P&gt;Reset Configuration Word (RCW):&lt;BR /&gt;00000000: 0c10000e 0e000000 00000000 00000000&lt;BR /&gt;00000010: 85000000 00400112 ec110000 21000000&lt;BR /&gt;00000020: 00000000 00000000 60000000 0003a000&lt;BR /&gt;00000030: 00000000 d416aa05 00000000 00000000&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 29 Oct 2020 10:16:54 GMT</pubDate>
    <dc:creator>hemwant</dc:creator>
    <dc:date>2020-10-29T10:16:54Z</dc:date>
    <item>
      <title>random: nonblocking pool is initialized</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/random-nonblocking-pool-is-initialized/m-p/1175219#M3438</link>
      <description>&lt;P&gt;I am having a T1022 processor based board, the uboot is booting from spi and nand flash is used to boot kernel, device tree and file system. When i am booting kernel from nand flash it sometimes got struck in kernel. This behavior is very frequent . Please look into the attached kernel log for reference.&lt;/P&gt;&lt;P&gt;Processor : T1022&lt;/P&gt;&lt;P&gt;Nand flash - Micron MT29F8G08ABBCAH4&lt;/P&gt;&lt;P&gt;Reset Configuration Word (RCW):&lt;BR /&gt;00000000: 0c10000e 0e000000 00000000 00000000&lt;BR /&gt;00000010: 85000000 00400112 ec110000 21000000&lt;BR /&gt;00000020: 00000000 00000000 60000000 0003a000&lt;BR /&gt;00000030: 00000000 d416aa05 00000000 00000000&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 29 Oct 2020 10:16:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/random-nonblocking-pool-is-initialized/m-p/1175219#M3438</guid>
      <dc:creator>hemwant</dc:creator>
      <dc:date>2020-10-29T10:16:54Z</dc:date>
    </item>
    <item>
      <title>Re: random: nonblocking pool is initialized</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/random-nonblocking-pool-is-initialized/m-p/1175704#M3444</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Please try whether this problem can be reproduce when using ramdisk boot, please refer to the following procedure.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;=&amp;gt; setenv bootargs "root=/dev/ram rw console=ttyS0,115200"&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;=&amp;gt; tftp 0x1000000 nxa22585/t1024/uImage&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;=&amp;gt; tftp 0x2000000 nxa22585/t1024/uImage-t1024rdb.dtb&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;=&amp;gt; tftp 0x5000000 nxa22585/t1024/fsl-image-minimal-t1040d4rdb.ext2.gz.u-boot&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;=&amp;gt; bootm 0x1000000 0x5000000 0x2000000&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;I uploaded fsl-image-minimal-t1040d4rdb.ext2.gz.u-boot in the following link.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&lt;A href="https://drive.google.com/file/d/1Dlnk-Cpn5im9IEdMGFv2mSduToIAYVoe/view?usp=sharing" target="_blank"&gt;https://drive.google.com/file/d/1Dlnk-Cpn5im9IEdMGFv2mSduToIAYVoe/view?usp=sharing&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;If this problem cannot be reproduced with ramdisk boot, please check NAND FLASH IFC timing configuration in u-boot source&amp;nbsp;include/configs/T102xRDB.h.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;For IFC timing configuration configuration on the custom board, please refer to&amp;nbsp;&lt;A href="https://community.nxp.com/t5/Layerscape-Knowledge-Base/IFC-Controller-Configuration-on-QorIQ-Custom-Boards/ta-p/1109156" target="_blank"&gt;https://community.nxp.com/t5/Layerscape-Knowledge-Base/IFC-Controller-Configuration-on-QorIQ-Custom-Boards/ta-p/1109156&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 30 Oct 2020 07:00:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/random-nonblocking-pool-is-initialized/m-p/1175704#M3444</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2020-10-30T07:00:02Z</dc:date>
    </item>
  </channel>
</rss>