<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>PowerQUICC Processors中的主题 Re: MPC8313 External USB Hub Create Test Packet</title>
    <link>https://community.nxp.com/t5/PowerQUICC-Processors/MPC8313-External-USB-Hub-Create-Test-Packet/m-p/1098243#M3335</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;The MPC8313 USB supports test mode using the PORTSC[PTC] bits. See the Section 16.3.13 of the MPC8313 Reference Manual:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;&lt;A href="https://www.nxp.com/docs/en/reference-manual/MPC8313ERM.pdf" target="test_blank"&gt;https://www.nxp.com/docs/en/reference-manual/MPC8313ERM.pdf&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;Is there problem for &lt;/SPAN&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;testing the USB eye patterns of the MPC8313 if USB hub is not used?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Pavel Chubakov&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 18 Aug 2020 04:43:10 GMT</pubDate>
    <dc:creator>Pavel</dc:creator>
    <dc:date>2020-08-18T04:43:10Z</dc:date>
    <item>
      <title>MPC8313 External USB Hub Create Test Packet</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/MPC8313-External-USB-Hub-Create-Test-Packet/m-p/1098242#M3334</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've been tasked with testing the USB eye patterns of the MPC8313 and the external hub it is connected to. In Linux I've been able to set the correct registers in the MPC8313 for it to create the test packets.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;To be able to test the external hub it is necessary to also set this hub up accordingly so it creates the test packets needed for the eye mask test.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The USB-IF has a tool for this, but it only works on windows. Does anyone know if there is an appnote concerning this situation or does anyone have any experience doing this?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind regards,&lt;/P&gt;&lt;P&gt;Ernst&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 17 Aug 2020 14:05:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/MPC8313-External-USB-Hub-Create-Test-Packet/m-p/1098242#M3334</guid>
      <dc:creator>ernst_verseput</dc:creator>
      <dc:date>2020-08-17T14:05:20Z</dc:date>
    </item>
    <item>
      <title>Re: MPC8313 External USB Hub Create Test Packet</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/MPC8313-External-USB-Hub-Create-Test-Packet/m-p/1098243#M3335</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;The MPC8313 USB supports test mode using the PORTSC[PTC] bits. See the Section 16.3.13 of the MPC8313 Reference Manual:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;&lt;A href="https://www.nxp.com/docs/en/reference-manual/MPC8313ERM.pdf" target="test_blank"&gt;https://www.nxp.com/docs/en/reference-manual/MPC8313ERM.pdf&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;Is there problem for &lt;/SPAN&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;testing the USB eye patterns of the MPC8313 if USB hub is not used?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Pavel Chubakov&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Aug 2020 04:43:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/MPC8313-External-USB-Hub-Create-Test-Packet/m-p/1098243#M3335</guid>
      <dc:creator>Pavel</dc:creator>
      <dc:date>2020-08-18T04:43:10Z</dc:date>
    </item>
  </channel>
</rss>