<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: ODT and additive latency in PowerQUICC Processors</title>
    <link>https://community.nxp.com/t5/PowerQUICC-Processors/ODT-and-additive-latency/m-p/1096340#M3317</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, CAS latency of 3, write latency of 2, and additive latency of 1 is ok to utilize ODT correctly.&lt;/P&gt;&lt;P&gt;RD_TO_PRE should be equal to tRTP,&amp;nbsp; ADD_LAT should not be added.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Bulat&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 29 Jun 2020 09:03:29 GMT</pubDate>
    <dc:creator>Bulat</dc:creator>
    <dc:date>2020-06-29T09:03:29Z</dc:date>
    <item>
      <title>ODT and additive latency</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/ODT-and-additive-latency/m-p/1096339#M3316</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The ODT_WR_CFG parameter of the CSn_CONFIG register indicates that write latency plus additive latency must be at least 3 to use ODT.&amp;nbsp; Our application uses an MPC8610 with 64-bit DDR2 w/ECC running at 200 MHz (DDR400).&amp;nbsp; Nominal CAS Latency is 3 and write latency is 2.&amp;nbsp; ODT is required.&amp;nbsp; Can CAS latency of 3, write latency of 2, and additive latency of 1 be used to meet this requirement and utilize ODT?&amp;nbsp; If so, should the RD_TO_PRE field of the TIMING_CFG_2 register include the additive latency (1 additional clock) or should it just include the t_RTP duration (2 clocks) when additive latency is used?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 29 Jun 2020 01:40:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/ODT-and-additive-latency/m-p/1096339#M3316</guid>
      <dc:creator>dallasclow</dc:creator>
      <dc:date>2020-06-29T01:40:23Z</dc:date>
    </item>
    <item>
      <title>Re: ODT and additive latency</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/ODT-and-additive-latency/m-p/1096340#M3317</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, CAS latency of 3, write latency of 2, and additive latency of 1 is ok to utilize ODT correctly.&lt;/P&gt;&lt;P&gt;RD_TO_PRE should be equal to tRTP,&amp;nbsp; ADD_LAT should not be added.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Bulat&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 29 Jun 2020 09:03:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/ODT-and-additive-latency/m-p/1096340#M3317</guid>
      <dc:creator>Bulat</dc:creator>
      <dc:date>2020-06-29T09:03:29Z</dc:date>
    </item>
  </channel>
</rss>