<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>PowerQUICC Processors中的主题 Re: Programming the MPC8360</title>
    <link>https://community.nxp.com/t5/PowerQUICC-Processors/Programming-the-MPC8360/m-p/1091776#M3309</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The MPC8360 &lt;SPAN style="font-size: 9.0pt; color: black;"&gt;CFG_RESET_SOURCE[0:2] pins is analog of the &lt;/SPAN&gt;MPC8260 RSTCONF pin. These pins select reset configuration word source. Correct operation of the JTAG interface requires configuration of a group of system control pins as described and demonstrated in the Design Checklist document&lt;BR /&gt; &lt;A href="https://www.nxp.com/docs/en/application-note/AN3097.pdf"&gt;https://www.nxp.com/docs/en/application-note/AN3097.pdf&lt;/A&gt;&lt;BR /&gt;See section " &lt;SPAN class=""&gt;JTAG and Debug&lt;/SPAN&gt;&amp;nbsp;".&amp;nbsp;The JTAG test interface (based on IEEE 1149.1) provides a means for boundary-scan testing of the core and the attached system logic. The hardware debug function accesses the JTAG test port, providing a&lt;/P&gt;&lt;P&gt;means for executing test routines and facilitating chip and software debugging. As guide&amp;nbsp;see for example Hardware Debugging Using the CodeWarrior™ IDE document&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN3830.pdf"&gt;https://www.nxp.com/docs/en/application-note/AN3830.pdf&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 29 Jun 2020 13:49:04 GMT</pubDate>
    <dc:creator>r8070z</dc:creator>
    <dc:date>2020-06-29T13:49:04Z</dc:date>
    <item>
      <title>Programming the MPC8360</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/Programming-the-MPC8360/m-p/1091775#M3308</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Good Day,&lt;/P&gt;&lt;P&gt;We are migrating from the MPC8260 Processor to the MPC8360. On the MPC8260 we pull the RSTCONF_ pin low to place the the Processor in defualt config to allow configuration.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there in Pin/ signal that needs to be asserted/negated to allow programming of the MPC8360 via the COP/JTAG signals? Is there a guide available that explains the physical programming or flashing of the MPC8360 processor cia the COP/JTAG signals?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 26 Jun 2020 06:55:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/Programming-the-MPC8360/m-p/1091775#M3308</guid>
      <dc:creator>hvdmerwe</dc:creator>
      <dc:date>2020-06-26T06:55:46Z</dc:date>
    </item>
    <item>
      <title>Re: Programming the MPC8360</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/Programming-the-MPC8360/m-p/1091776#M3309</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The MPC8360 &lt;SPAN style="font-size: 9.0pt; color: black;"&gt;CFG_RESET_SOURCE[0:2] pins is analog of the &lt;/SPAN&gt;MPC8260 RSTCONF pin. These pins select reset configuration word source. Correct operation of the JTAG interface requires configuration of a group of system control pins as described and demonstrated in the Design Checklist document&lt;BR /&gt; &lt;A href="https://www.nxp.com/docs/en/application-note/AN3097.pdf"&gt;https://www.nxp.com/docs/en/application-note/AN3097.pdf&lt;/A&gt;&lt;BR /&gt;See section " &lt;SPAN class=""&gt;JTAG and Debug&lt;/SPAN&gt;&amp;nbsp;".&amp;nbsp;The JTAG test interface (based on IEEE 1149.1) provides a means for boundary-scan testing of the core and the attached system logic. The hardware debug function accesses the JTAG test port, providing a&lt;/P&gt;&lt;P&gt;means for executing test routines and facilitating chip and software debugging. As guide&amp;nbsp;see for example Hardware Debugging Using the CodeWarrior™ IDE document&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN3830.pdf"&gt;https://www.nxp.com/docs/en/application-note/AN3830.pdf&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 29 Jun 2020 13:49:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/Programming-the-MPC8360/m-p/1091776#M3309</guid>
      <dc:creator>r8070z</dc:creator>
      <dc:date>2020-06-29T13:49:04Z</dc:date>
    </item>
    <item>
      <title>Re: Programming the MPC8360</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/Programming-the-MPC8360/m-p/1091777#M3310</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Thank you for the reply,&lt;P&gt;&lt;/P&gt;How does the PowerQuicc know that you want to program it with something new.&lt;P&gt;&lt;/P&gt;From what I can gather, the CFG_RESET_SOURCE[0:2] just tells the PowerQuicc where to look for the reset configuration word.&lt;P&gt;&lt;/P&gt;Is there a guide to explain how to program the Powerquicc, or how to program a local bus SRAM/Flash via the Powerquicc? I think that is what I am struggling most with at the time.&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 Jul 2020 12:21:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/Programming-the-MPC8360/m-p/1091777#M3310</guid>
      <dc:creator>hvdmerwe</dc:creator>
      <dc:date>2020-07-03T12:21:25Z</dc:date>
    </item>
    <item>
      <title>Re: Programming the MPC8360</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/Programming-the-MPC8360/m-p/1091778#M3311</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Yes as I wrote the MPC8360 CFG_RESET_SOURCE[0:2] are like the MPC8260 RSTCONF.&amp;nbsp;&lt;BR /&gt;There are guide for the tools which can&amp;nbsp;&lt;SPAN&gt;program a local bus SRAM/Flash via the Powerquicc only.&amp;nbsp; These tools use the JTAG/COP interface.&amp;nbsp; Special&amp;nbsp;COP protocol used to Displaying Memory and Registers like in the AN3830 it also permit download code and program Flash connected to the MPC8360. So&amp;nbsp;&lt;SPAN style="background-color: #ffffff;"&gt;the CodeWarrior™ includes FLASH programmer.&amp;nbsp;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 06 Jul 2020 08:13:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/Programming-the-MPC8360/m-p/1091778#M3311</guid>
      <dc:creator>r8070z</dc:creator>
      <dc:date>2020-07-06T08:13:16Z</dc:date>
    </item>
  </channel>
</rss>