<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Codewarrior Ethernet TAP Clarifcation in PowerQUICC Processors</title>
    <link>https://community.nxp.com/t5/PowerQUICC-Processors/Codewarrior-Ethernet-TAP-Clarifcation/m-p/1075740#M3262</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;1) The CodeWarrior TAP itself does not require any licensing, CodeWarrior IDE - does.&lt;/P&gt;&lt;P&gt;2) The CodeWarrior IDE is a must.&lt;/P&gt;&lt;P&gt;3) Possibly - yes, but this was not tested because CodeWarrior has its own C-compiler.&lt;/P&gt;&lt;P&gt;4) It is impossible to compare "lauterbach debugger and codewarrior tap" because Trace32 can be compared only with CodeWarrior IDE.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 12 May 2020 15:59:01 GMT</pubDate>
    <dc:creator>ufedor</dc:creator>
    <dc:date>2020-05-12T15:59:01Z</dc:date>
    <item>
      <title>Codewarrior Ethernet TAP Clarifcation</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/Codewarrior-Ethernet-TAP-Clarifcation/m-p/1075739#M3261</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi.&lt;/P&gt;&lt;P&gt;We are developing a product using MPC8349E. We are planning to buy CWH-CTP-BASE-HE along with CWH-CTP-COP-YE. I have the following clarifications on the same.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. Whether the above part number if purchased will support all the power architectures like powerquicc I, II,II Pro, T-Series, P-Series or there will be different licensing options that needs to be purchased separately.&lt;/P&gt;&lt;P&gt;2. Is it mandatory to purchase Codewarrior IDE for using the tool or there is a debugging IDE supplied along with the tool.&lt;/P&gt;&lt;P&gt;3. Can this be integrated with Windriver workbench IDE with DIAB compiler.&lt;/P&gt;&lt;P&gt;4. What is the difference between lauterbach debugger and codewarrior tap with regard to feature set.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and Regards&lt;/P&gt;&lt;P&gt;Harish Kumar&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 May 2020 08:40:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/Codewarrior-Ethernet-TAP-Clarifcation/m-p/1075739#M3261</guid>
      <dc:creator>harishkumar</dc:creator>
      <dc:date>2020-05-12T08:40:42Z</dc:date>
    </item>
    <item>
      <title>Re: Codewarrior Ethernet TAP Clarifcation</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/Codewarrior-Ethernet-TAP-Clarifcation/m-p/1075740#M3262</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;1) The CodeWarrior TAP itself does not require any licensing, CodeWarrior IDE - does.&lt;/P&gt;&lt;P&gt;2) The CodeWarrior IDE is a must.&lt;/P&gt;&lt;P&gt;3) Possibly - yes, but this was not tested because CodeWarrior has its own C-compiler.&lt;/P&gt;&lt;P&gt;4) It is impossible to compare "lauterbach debugger and codewarrior tap" because Trace32 can be compared only with CodeWarrior IDE.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 May 2020 15:59:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/Codewarrior-Ethernet-TAP-Clarifcation/m-p/1075740#M3262</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2020-05-12T15:59:01Z</dc:date>
    </item>
  </channel>
</rss>