<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>PowerQUICC ProcessorsのトピックRe: Writing UART Interrupt Handler for T104xRDB</title>
    <link>https://community.nxp.com/t5/PowerQUICC-Processors/Writing-UART-Interrupt-Handler-for-T104xRDB/m-p/961253#M3029</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You could refer to the sample project provided in CodeWarrior 10.5.1 for T1040RDB.&lt;/P&gt;&lt;P&gt;Please download and install CodeWarrior 10.5.1 from &lt;A class="link-titled" href="https://www.nxp.com/support/developer-resources/software-development-tools/codewarrior-development-tools/codewarrior-network-applications/codewarrior-development-suites-for-networked-applications-v11.4.0:CW-DS-NETAPPS?tab=Design_Tools_Tab" title="https://www.nxp.com/support/developer-resources/software-development-tools/codewarrior-development-tools/codewarrior-network-applications/codewarrior-development-suites-for-networked-applications-v11.4.0:CW-DS-NETAPPS?tab=Design_Tools_Tab"&gt;CodeWarrior Dev Tools for Networked Apps v11.4.0 | NXP&lt;/A&gt; .&lt;/P&gt;&lt;P&gt;Please create a bareboard project following new project wazards from File-&amp;gt;New-&amp;gt;CodeWarrior Bareboard Project.&lt;/P&gt;&lt;P&gt;Please refer to interrupt.c, pa_exception.asm and "Interrupt vectors initialization" section in T1040RDB_init.c in Sources folder in the sample project.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Yiping&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 30 Jun 2019 10:22:55 GMT</pubDate>
    <dc:creator>yipingwang</dc:creator>
    <dc:date>2019-06-30T10:22:55Z</dc:date>
    <item>
      <title>Writing UART Interrupt Handler for T104xRDB</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/Writing-UART-Interrupt-Handler-for-T104xRDB/m-p/961252#M3028</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm working on T1042RDB and The board have duart for serial communication.&amp;nbsp; I dont want to use polling method to receive or transmit data and&amp;nbsp; because of that i try to write an interrupt handler for UART but i am also new to powerpc family. I'll tell what I tried to write an interrupt handler but i'm sold i'm wrong : )&lt;/P&gt;&lt;P&gt;btw, i dont use any operating systems, the application which i try to write is standalone.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I firstly read the T1040 reference manual&amp;nbsp; and chapter 5 is about Interrupt Assignments.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;in that chapter ;&lt;/P&gt;&lt;P&gt;there is a table for internal interrupt sources and it says 20th internal interrupt corresponds to DUART 1 interrrupt source.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;the explanation for IVPR from e5500 reference manual ;&amp;nbsp;&lt;/P&gt;&lt;P&gt;"IVPR[0-47] provides the high-order 484 bits of the address of the exception processing routines. the 16-bit vector offsets(IVORs) are concatenated to the right of IVPR to form the address of the exception processing routine."&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;the explanation for IVOR from e5500 reference manual;&lt;/P&gt;&lt;P&gt;" ....... but use only IVORn[48-59], as shown in figure 2-5, to hold the quad-word index from the base address provided by the IVPR for each interrupt type".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;then, let's&amp;nbsp;assume i set IVOR20 register to 0x190 and IVPR register to 0.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;IVPR + IVOR20 = 0.....0 + 000110010000 +&lt;STRONG style="color: #333333; background-color: #ffffff; font-weight: bold;"&gt;&amp;nbsp;&lt;/STRONG&gt;0000 = 0x1900 is interrupt service routine address or interrupt handler address.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;and then i should place my interrupt service routine to 0x1900 memory address when i initialize some basic stuff.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;by the way, there is a IVOR20 register, isnt it ? i have doubt it's a register which we can access or not .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;and my question is rising, i'm wrong or not ? if i'm wrong, engliht me, and please , if dont use sophisticated word to explain, i will appericate you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks in advance.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Jun 2019 09:15:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/Writing-UART-Interrupt-Handler-for-T104xRDB/m-p/961252#M3028</guid>
      <dc:creator>love_hate_and_repeat</dc:creator>
      <dc:date>2019-06-24T09:15:43Z</dc:date>
    </item>
    <item>
      <title>Re: Writing UART Interrupt Handler for T104xRDB</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/Writing-UART-Interrupt-Handler-for-T104xRDB/m-p/961253#M3029</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You could refer to the sample project provided in CodeWarrior 10.5.1 for T1040RDB.&lt;/P&gt;&lt;P&gt;Please download and install CodeWarrior 10.5.1 from &lt;A class="link-titled" href="https://www.nxp.com/support/developer-resources/software-development-tools/codewarrior-development-tools/codewarrior-network-applications/codewarrior-development-suites-for-networked-applications-v11.4.0:CW-DS-NETAPPS?tab=Design_Tools_Tab" title="https://www.nxp.com/support/developer-resources/software-development-tools/codewarrior-development-tools/codewarrior-network-applications/codewarrior-development-suites-for-networked-applications-v11.4.0:CW-DS-NETAPPS?tab=Design_Tools_Tab"&gt;CodeWarrior Dev Tools for Networked Apps v11.4.0 | NXP&lt;/A&gt; .&lt;/P&gt;&lt;P&gt;Please create a bareboard project following new project wazards from File-&amp;gt;New-&amp;gt;CodeWarrior Bareboard Project.&lt;/P&gt;&lt;P&gt;Please refer to interrupt.c, pa_exception.asm and "Interrupt vectors initialization" section in T1040RDB_init.c in Sources folder in the sample project.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Yiping&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 30 Jun 2019 10:22:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/Writing-UART-Interrupt-Handler-for-T104xRDB/m-p/961253#M3029</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2019-06-30T10:22:55Z</dc:date>
    </item>
    <item>
      <title>Re: Writing UART Interrupt Handler for T104xRDB</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/Writing-UART-Interrupt-Handler-for-T104xRDB/m-p/961254#M3030</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;thanks for your reply but i have still some problems.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i wrote a interrupt handler but returning handler function to main function is never happened. the following application runs on u-boot as standalone application.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;void myInterruptHandler(void)&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; inline&amp;nbsp;&amp;nbsp;assembly code ;&amp;nbsp; isr_prologue from pa_exception.asm&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; printf("this is an interrupt\n");&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; inline assembly code; &amp;nbsp;isr_epilogue from pa_exception.asm here&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;int main(int argc, char *argv[])&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;while(1)&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;Printf("Here\n");&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;"here" message is always displayed but after first interrupt happens&amp;nbsp; "This is an interrupt" message is displayed and after that&amp;nbsp; "here" message is&amp;nbsp;not displayed.&lt;/P&gt;&lt;P&gt;Application is frozen forever and not returning to u-boot function which it calls the application.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;i guess returning from myInterruptHandler function to main function is not happened.&amp;nbsp; how can i solve this problem ?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks in advance.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 03 Aug 2019 12:05:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/Writing-UART-Interrupt-Handler-for-T104xRDB/m-p/961254#M3030</guid>
      <dc:creator>love_hate_and_repeat</dc:creator>
      <dc:date>2019-08-03T12:05:29Z</dc:date>
    </item>
    <item>
      <title>Re: Writing UART Interrupt Handler for T104xRDB</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/Writing-UART-Interrupt-Handler-for-T104xRDB/m-p/961255#M3031</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;void InterruptHandler(long cause);&lt;BR /&gt;extern void __init_hardware(void);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;#ifdef __cplusplus&lt;BR /&gt;}&lt;BR /&gt;#endif&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;void InterruptHandler(long cause)&lt;BR /&gt;{&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;unsigned long proc_id;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;/* recover computation mode */&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;__init_hardware();&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;/* read processor id */&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;asm ("mfpir %0" : "=r" (proc_id));&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;printf("Core%lu: InterruptHandler: %#lx exception.\r\n", proc_id&amp;gt;&amp;gt;5, cause);&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;#include &amp;lt;stdio.h&amp;gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;int main()&lt;BR /&gt;{&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;int i=0;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;unsigned long proc_id;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;asm ("mfpir %0" : "=r" (proc_id));&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;printf("Core%lu: Welcome to CodeWarrior!\r\n", proc_id&amp;gt;&amp;gt;5);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;asm("sc"); // generate a system call exception to demonstrate the ISR&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;while (1) { i++; } // loop forever&lt;BR /&gt;}&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 05 Aug 2019 09:59:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/Writing-UART-Interrupt-Handler-for-T104xRDB/m-p/961255#M3031</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2019-08-05T09:59:01Z</dc:date>
    </item>
    <item>
      <title>Re: Writing UART Interrupt Handler for T104xRDB</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/Writing-UART-Interrupt-Handler-for-T104xRDB/m-p/961256#M3032</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;thanks for your effort but the problem is same when interrupt happpens interrupt handler runs once and doesnt return to main function and application is pending i dont know how it's pending because it doesnt crash u-boot code but it's hanging forever.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 08 Aug 2019 12:19:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/Writing-UART-Interrupt-Handler-for-T104xRDB/m-p/961256#M3032</guid>
      <dc:creator>love_hate_and_repeat</dc:creator>
      <dc:date>2019-08-08T12:19:33Z</dc:date>
    </item>
  </channel>
</rss>