<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>PowerQUICC ProcessorsのトピックRe: Windows hosted gcc toolchains for Linux development</title>
    <link>https://community.nxp.com/t5/PowerQUICC-Processors/Windows-hosted-gcc-toolchains-for-Linux-development/m-p/957814#M3012</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A _jive_internal="true" data-content-finding="Community" data-userid="281784" data-username="wernerabt" href="https://community.nxp.com/people/wernerabt"&gt;Werner Abt&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please try to use powerpc-linux Toolchain provided in CodeWarrior 10.1.1, which is used to build Linux application project.&lt;/P&gt;&lt;P&gt;I uploaded it &lt;A class="link-titled" href="https://drive.google.com/open?id=1PYALj14Xc7pGtLBCrvCVHCRgAd2gIE26" title="https://drive.google.com/open?id=1PYALj14Xc7pGtLBCrvCVHCRgAd2gIE26"&gt;https://drive.google.com/open?id=1PYALj14Xc7pGtLBCrvCVHCRgAd2gIE26&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Yiping&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 07 Aug 2019 09:46:33 GMT</pubDate>
    <dc:creator>yipingwang</dc:creator>
    <dc:date>2019-08-07T09:46:33Z</dc:date>
    <item>
      <title>Windows hosted gcc toolchains for Linux development</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/Windows-hosted-gcc-toolchains-for-Linux-development/m-p/957812#M3010</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I need a Windows hosted gcc toolchain for the MPC8323E processor. This is a PowerQUICC 3 processor with an e300 core. Is there anybody that can provide the proper toolchain for me? I do not need an IDE, just the windows hosted gcc toolchain for cross-platform development to the linux system of the MPC8323 processor.&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 Aug 2019 12:43:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/Windows-hosted-gcc-toolchains-for-Linux-development/m-p/957812#M3010</guid>
      <dc:creator>wernerabt</dc:creator>
      <dc:date>2019-08-06T12:43:07Z</dc:date>
    </item>
    <item>
      <title>Re: Windows hosted gcc toolchains for Linux development</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/Windows-hosted-gcc-toolchains-for-Linux-development/m-p/957813#M3011</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;A generic&amp;nbsp;reply: the "CodeWarrior® Development Suite for Networked Applications" is installing (actually: two) GCC compiler(s) . If you look for the GCC part only, you can basically TAR this subtree, and/or remove the rest of the installation.&lt;/P&gt;&lt;P&gt;However, I can´t fully answer your question: the latest version definitely installs for the E500 core, but as our CW support page clearly lists the PQ3 family, I suspect the E300 is also supported. I will ask someone else to further comment.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Toni&lt;BR /&gt;NXP Support&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 Aug 2019 16:51:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/Windows-hosted-gcc-toolchains-for-Linux-development/m-p/957813#M3011</guid>
      <dc:creator>ToniZollikofer</dc:creator>
      <dc:date>2019-08-06T16:51:56Z</dc:date>
    </item>
    <item>
      <title>Re: Windows hosted gcc toolchains for Linux development</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/Windows-hosted-gcc-toolchains-for-Linux-development/m-p/957814#M3012</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A _jive_internal="true" data-content-finding="Community" data-userid="281784" data-username="wernerabt" href="https://community.nxp.com/people/wernerabt"&gt;Werner Abt&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please try to use powerpc-linux Toolchain provided in CodeWarrior 10.1.1, which is used to build Linux application project.&lt;/P&gt;&lt;P&gt;I uploaded it &lt;A class="link-titled" href="https://drive.google.com/open?id=1PYALj14Xc7pGtLBCrvCVHCRgAd2gIE26" title="https://drive.google.com/open?id=1PYALj14Xc7pGtLBCrvCVHCRgAd2gIE26"&gt;https://drive.google.com/open?id=1PYALj14Xc7pGtLBCrvCVHCRgAd2gIE26&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Yiping&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Aug 2019 09:46:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/Windows-hosted-gcc-toolchains-for-Linux-development/m-p/957814#M3012</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2019-08-07T09:46:33Z</dc:date>
    </item>
  </channel>
</rss>