<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic On Pci Data missing  in PowerQUICC Processors</title>
    <link>https://community.nxp.com/t5/PowerQUICC-Processors/On-Pci-Data-missing/m-p/946273#M2972</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have T1042 processor on PCIe interface with kintex 7 fpga board . I have test application where data communication b/w Processor &amp;amp; fpga we will be continuously . But moment Processor reads data from fpga it was observed data is getting missed . I meant if processor&amp;nbsp; expecting data for example 1,2,3,4,5 &amp;amp; soon , it will get like 1 ,8,9,15,22, &amp;amp; soon .&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On processor side I have checked AER register&amp;nbsp; &amp;amp; other also but could not find error on register level . Please find Log for processor &amp;amp; fpga below&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;&lt;STRONG&gt;PROCESSOR INFORMATION&amp;nbsp;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;vendor ID = 0x1957&lt;BR /&gt;device ID = 0x0825&lt;BR /&gt;command register = 0x0007&lt;BR /&gt;status register = 0x0010&lt;BR /&gt;revision ID = 0x11&lt;BR /&gt;class code = 0x0b&lt;BR /&gt;sub class code = 0x20&lt;BR /&gt;programming interface = 0x00&lt;BR /&gt;cache line = 0x10&lt;BR /&gt;latency time = 0x00&lt;BR /&gt;header type = 0x01&lt;BR /&gt;BIST = 0x00&lt;BR /&gt;base address 0 = 0x00000000&lt;BR /&gt;base address 1 = 0x00000000&lt;BR /&gt;primary bus number = 0x00&lt;BR /&gt;secondary bus number = 0x01&lt;BR /&gt;subordinate bus number = 0x01&lt;BR /&gt;secondary latency timer = 0x00&lt;BR /&gt;IO base = 0xf1&lt;BR /&gt;IO limit = 0x01&lt;BR /&gt;secondary status = 0x0000&lt;BR /&gt;memory base = 0xa000&lt;BR /&gt;memory limit = 0xa030&lt;BR /&gt;prefetch memory base = 0xfff1&lt;BR /&gt;prefetch memory limit = 0x0001&lt;BR /&gt;prefetch memory base upper = 0x00000000&lt;BR /&gt;prefetch memory limit upper = 0x00000000&lt;BR /&gt;IO base upper 16 bits = 0xffff&lt;BR /&gt;IO limit upper 16 bits = 0x000f&lt;BR /&gt;expansion ROM base address = 0x00000000&lt;BR /&gt;interrupt line = 0x00&lt;BR /&gt;interrupt pin = 0x00&lt;BR /&gt;bridge control = 0x0000&lt;BR /&gt;Capabilities - Power Management &lt;BR /&gt;Capabilities - PCIe: Root Port, IRQ 0&lt;BR /&gt; Device: Max Payload: 256 bytes, Extended Tag: 5-bit&lt;BR /&gt; Acceptable Latency: L0 - &amp;lt;64ns, L1 - &amp;lt;1us&lt;BR /&gt; Errors Enabled: Non-Fatal Fatal Unsupported RequestRelaxed Ordering No Snoop&lt;/P&gt;&lt;P&gt;Max Read Request 512 bytes&lt;BR /&gt; Link: MAX Speed - 5.0Gb/s, MAX Width - by 4 Port - 0 ASPM - L0s&lt;BR /&gt; Latency: L0s - &amp;lt;2us, L1 - &amp;gt;64us&lt;BR /&gt; ASPM - Disabled, RCB - 128bytes&lt;BR /&gt; Speed - 5.0Gb/s, Width - by 2&lt;BR /&gt; Root Control Enabled: &lt;BR /&gt;Ext Capabilities - Advanced Error Reporting. 0x100. Version 1. AER Control: 0xa0 &lt;BR /&gt; Uncorrectable : Mask 0x0. Severity 0x62010 &lt;BR /&gt; Uncorrectable Status: Correctable : Mask 0x2000. &lt;BR /&gt; Correctable Status: &lt;BR /&gt; HeaderLog: &lt;BR /&gt; Error Source Identification: 0x0 0x0&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;&lt;STRONG&gt;FPGA&amp;nbsp; INFORMATION&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;vendor ID = 0x10ee&lt;BR /&gt;device ID = 0x7022&lt;BR /&gt;command register = 0x0007&lt;BR /&gt;status register = 0x0010&lt;BR /&gt;revision ID = 0x00&lt;BR /&gt;class code = 0x05&lt;BR /&gt;sub class code = 0x80&lt;BR /&gt;programming interface = 0x00&lt;BR /&gt;cache line = 0x10&lt;BR /&gt;latency time = 0x00&lt;BR /&gt;header type = 0x00&lt;BR /&gt;BIST = 0x00&lt;BR /&gt;base address 0 = 0xa0000000&lt;BR /&gt;base address 1 = 0x00000000&lt;BR /&gt;base address 2 = 0x00000000&lt;BR /&gt;base address 3 = 0x00000000&lt;BR /&gt;base address 4 = 0x00000000&lt;BR /&gt;base address 5 = 0x00000000&lt;BR /&gt;cardBus CIS pointer = 0x00000000&lt;BR /&gt;sub system vendor ID = 0x10ee&lt;BR /&gt;sub system ID = 0x0007&lt;BR /&gt;expansion ROM base address = 0x00000000&lt;BR /&gt;interrupt line = 0x29&lt;BR /&gt;interrupt pin = 0x01&lt;BR /&gt;min Grant = 0x00&lt;BR /&gt;max Latency = 0x00&lt;BR /&gt;Capabilities - Power Management &lt;BR /&gt;Capabilities - Message Signaled Interrupts: 0x48 control 0x80 Disabled, 64-bit, MME: 0 MMC: 0&lt;BR /&gt; Address: 0000000000000000 Data: 0x0000&lt;BR /&gt; Per-vector Mask: Unsupported &lt;BR /&gt;Capabilities - PCIe: Endpoint, IRQ 0&lt;BR /&gt; Device: Max Payload: 256 bytes, Phantom Funcs 1 msb, Extended Tag: 8-bit&lt;BR /&gt; Acceptable Latency: L0 - &amp;lt;64ns, L1 - &amp;lt;1us&lt;BR /&gt; Errors Enabled: Relaxed Ordering No Snoop&lt;/P&gt;&lt;P&gt;Max Read Request 512 bytes&lt;BR /&gt; Link: MAX Speed - 5.0Gb/s, MAX Width - by 2 Port - 0 ASPM - L0s&lt;BR /&gt; Latency: L0s - &amp;gt;4us, L1 - &amp;gt;64us&lt;BR /&gt; ASPM - Disabled, RCB - 64bytes&lt;BR /&gt; Speed - 5.0Gb/s, Width - by 2&lt;BR /&gt;Ext Capabilities - Device Serial Number. 0x100. Version 1 &lt;BR /&gt; Serial Number: 0x0 0x0 0x0 0x0 0x0 0x0 0x0 0x0&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kindly provide solution where I need to look .into&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 19 Sep 2019 06:30:51 GMT</pubDate>
    <dc:creator>utkarsh_100</dc:creator>
    <dc:date>2019-09-19T06:30:51Z</dc:date>
    <item>
      <title>On Pci Data missing</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/On-Pci-Data-missing/m-p/946273#M2972</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have T1042 processor on PCIe interface with kintex 7 fpga board . I have test application where data communication b/w Processor &amp;amp; fpga we will be continuously . But moment Processor reads data from fpga it was observed data is getting missed . I meant if processor&amp;nbsp; expecting data for example 1,2,3,4,5 &amp;amp; soon , it will get like 1 ,8,9,15,22, &amp;amp; soon .&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On processor side I have checked AER register&amp;nbsp; &amp;amp; other also but could not find error on register level . Please find Log for processor &amp;amp; fpga below&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;&lt;STRONG&gt;PROCESSOR INFORMATION&amp;nbsp;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;vendor ID = 0x1957&lt;BR /&gt;device ID = 0x0825&lt;BR /&gt;command register = 0x0007&lt;BR /&gt;status register = 0x0010&lt;BR /&gt;revision ID = 0x11&lt;BR /&gt;class code = 0x0b&lt;BR /&gt;sub class code = 0x20&lt;BR /&gt;programming interface = 0x00&lt;BR /&gt;cache line = 0x10&lt;BR /&gt;latency time = 0x00&lt;BR /&gt;header type = 0x01&lt;BR /&gt;BIST = 0x00&lt;BR /&gt;base address 0 = 0x00000000&lt;BR /&gt;base address 1 = 0x00000000&lt;BR /&gt;primary bus number = 0x00&lt;BR /&gt;secondary bus number = 0x01&lt;BR /&gt;subordinate bus number = 0x01&lt;BR /&gt;secondary latency timer = 0x00&lt;BR /&gt;IO base = 0xf1&lt;BR /&gt;IO limit = 0x01&lt;BR /&gt;secondary status = 0x0000&lt;BR /&gt;memory base = 0xa000&lt;BR /&gt;memory limit = 0xa030&lt;BR /&gt;prefetch memory base = 0xfff1&lt;BR /&gt;prefetch memory limit = 0x0001&lt;BR /&gt;prefetch memory base upper = 0x00000000&lt;BR /&gt;prefetch memory limit upper = 0x00000000&lt;BR /&gt;IO base upper 16 bits = 0xffff&lt;BR /&gt;IO limit upper 16 bits = 0x000f&lt;BR /&gt;expansion ROM base address = 0x00000000&lt;BR /&gt;interrupt line = 0x00&lt;BR /&gt;interrupt pin = 0x00&lt;BR /&gt;bridge control = 0x0000&lt;BR /&gt;Capabilities - Power Management &lt;BR /&gt;Capabilities - PCIe: Root Port, IRQ 0&lt;BR /&gt; Device: Max Payload: 256 bytes, Extended Tag: 5-bit&lt;BR /&gt; Acceptable Latency: L0 - &amp;lt;64ns, L1 - &amp;lt;1us&lt;BR /&gt; Errors Enabled: Non-Fatal Fatal Unsupported RequestRelaxed Ordering No Snoop&lt;/P&gt;&lt;P&gt;Max Read Request 512 bytes&lt;BR /&gt; Link: MAX Speed - 5.0Gb/s, MAX Width - by 4 Port - 0 ASPM - L0s&lt;BR /&gt; Latency: L0s - &amp;lt;2us, L1 - &amp;gt;64us&lt;BR /&gt; ASPM - Disabled, RCB - 128bytes&lt;BR /&gt; Speed - 5.0Gb/s, Width - by 2&lt;BR /&gt; Root Control Enabled: &lt;BR /&gt;Ext Capabilities - Advanced Error Reporting. 0x100. Version 1. AER Control: 0xa0 &lt;BR /&gt; Uncorrectable : Mask 0x0. Severity 0x62010 &lt;BR /&gt; Uncorrectable Status: Correctable : Mask 0x2000. &lt;BR /&gt; Correctable Status: &lt;BR /&gt; HeaderLog: &lt;BR /&gt; Error Source Identification: 0x0 0x0&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;&lt;STRONG&gt;FPGA&amp;nbsp; INFORMATION&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;vendor ID = 0x10ee&lt;BR /&gt;device ID = 0x7022&lt;BR /&gt;command register = 0x0007&lt;BR /&gt;status register = 0x0010&lt;BR /&gt;revision ID = 0x00&lt;BR /&gt;class code = 0x05&lt;BR /&gt;sub class code = 0x80&lt;BR /&gt;programming interface = 0x00&lt;BR /&gt;cache line = 0x10&lt;BR /&gt;latency time = 0x00&lt;BR /&gt;header type = 0x00&lt;BR /&gt;BIST = 0x00&lt;BR /&gt;base address 0 = 0xa0000000&lt;BR /&gt;base address 1 = 0x00000000&lt;BR /&gt;base address 2 = 0x00000000&lt;BR /&gt;base address 3 = 0x00000000&lt;BR /&gt;base address 4 = 0x00000000&lt;BR /&gt;base address 5 = 0x00000000&lt;BR /&gt;cardBus CIS pointer = 0x00000000&lt;BR /&gt;sub system vendor ID = 0x10ee&lt;BR /&gt;sub system ID = 0x0007&lt;BR /&gt;expansion ROM base address = 0x00000000&lt;BR /&gt;interrupt line = 0x29&lt;BR /&gt;interrupt pin = 0x01&lt;BR /&gt;min Grant = 0x00&lt;BR /&gt;max Latency = 0x00&lt;BR /&gt;Capabilities - Power Management &lt;BR /&gt;Capabilities - Message Signaled Interrupts: 0x48 control 0x80 Disabled, 64-bit, MME: 0 MMC: 0&lt;BR /&gt; Address: 0000000000000000 Data: 0x0000&lt;BR /&gt; Per-vector Mask: Unsupported &lt;BR /&gt;Capabilities - PCIe: Endpoint, IRQ 0&lt;BR /&gt; Device: Max Payload: 256 bytes, Phantom Funcs 1 msb, Extended Tag: 8-bit&lt;BR /&gt; Acceptable Latency: L0 - &amp;lt;64ns, L1 - &amp;lt;1us&lt;BR /&gt; Errors Enabled: Relaxed Ordering No Snoop&lt;/P&gt;&lt;P&gt;Max Read Request 512 bytes&lt;BR /&gt; Link: MAX Speed - 5.0Gb/s, MAX Width - by 2 Port - 0 ASPM - L0s&lt;BR /&gt; Latency: L0s - &amp;gt;4us, L1 - &amp;gt;64us&lt;BR /&gt; ASPM - Disabled, RCB - 64bytes&lt;BR /&gt; Speed - 5.0Gb/s, Width - by 2&lt;BR /&gt;Ext Capabilities - Device Serial Number. 0x100. Version 1 &lt;BR /&gt; Serial Number: 0x0 0x0 0x0 0x0 0x0 0x0 0x0 0x0&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kindly provide solution where I need to look .into&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Sep 2019 06:30:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/On-Pci-Data-missing/m-p/946273#M2972</guid>
      <dc:creator>utkarsh_100</dc:creator>
      <dc:date>2019-09-19T06:30:51Z</dc:date>
    </item>
    <item>
      <title>Re: On Pci Data missing</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/On-Pci-Data-missing/m-p/946274#M2973</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Provided problem description is not clear.&lt;/P&gt;&lt;P&gt;What exactly does it mean: "Processor reads data from fpga"?&lt;/P&gt;&lt;P&gt;What is the read transaction data size?&lt;/P&gt;&lt;P&gt;How exactly the read operation is performed by the T1042?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You wrote:&lt;/P&gt;&lt;P&gt;&amp;gt; expecting data for example 1,2,3,4,5&lt;/P&gt;&lt;P&gt;Please provide example memory dump of this structure.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How exactly the data structure is formed in the FPGA?&lt;/P&gt;&lt;P&gt;Can you check that the data is not corrupted at the FPGA side?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ensure that the T1042 PCIe Outbound Window is configured as cache-inhibited in the MMU.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Sep 2019 08:36:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/On-Pci-Data-missing/m-p/946274#M2973</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2019-09-24T08:36:14Z</dc:date>
    </item>
    <item>
      <title>Re: On Pci Data missing</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/On-Pci-Data-missing/m-p/946275#M2974</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;EM style="background-color: #ffffff; color: #51626f; "&gt;&amp;gt;&amp;gt;&amp;gt;&amp;gt; What exactly does it mean: "Processor reads data from fpga"?&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;Fpga will be continuously writing onto the processor .Sorry for not explaining properly I meant Data is getting missed from the processor . &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;FPGA continuously&amp;nbsp; write data in the series 1,2,3,4,5,6,7,8,9,10,11,12,13,14 &amp;amp; soon, but I guess processor is &lt;STRONG&gt;missing the data &lt;/STRONG&gt;.On processor it gets&amp;nbsp;&amp;nbsp;data like in pattern&amp;nbsp; 1,2,&lt;STRONG&gt;3,5&lt;/STRONG&gt;,6,&lt;STRONG&gt;7,9&lt;/STRONG&gt;,10,&lt;STRONG&gt;11,13&lt;/STRONG&gt;,14,&lt;STRONG&gt;15,17&lt;/STRONG&gt;,18,19. Processor missed the data 4,8,12,16 &amp;amp; soon.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;&lt;/SPAN&gt;&lt;EM style="background-color: #ffffff; color: #51626f; "&gt;&amp;gt;&amp;gt;&amp;gt;&amp;gt; What is the read transaction data size?&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;&lt;SPAN&gt;I guess data size is not the issue, It looks like some logical error.&amp;nbsp;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="background-color: #ffffff; border: 0px;"&gt;&lt;EM&gt;&amp;gt;&amp;gt;&amp;gt;&amp;gt;How exactly the data structure is formed in the FPGA?&lt;/EM&gt;&lt;/P&gt;&lt;P style="background-color: #ffffff; border: 0px;"&gt;&lt;EM&gt;&amp;gt;&amp;gt;&amp;gt;&amp;gt;Can you check that the data is not corrupted at the FPGA side?&lt;/EM&gt;&lt;/P&gt;&lt;P style="background-color: #ffffff; border: 0px;"&gt;Not sure the data structure in the fpga ,as I am looking onto the processor side . Need to check with the fpga team .&amp;nbsp;&lt;/P&gt;&lt;P style="background-color: #ffffff; border: 0px;"&gt;On chip scope we have measure there in no corruption of data on the fpga side&lt;/P&gt;&lt;P style="background-color: #ffffff; border: 0px;"&gt;&lt;/P&gt;&lt;P style="background-color: #ffffff; border: 0px;"&gt;&lt;EM style="color: #51626f; "&gt;&amp;gt;&amp;gt;&amp;gt;&amp;gt;&amp;gt;Ensure that the T1042 PCIe Outbound Window is configured as cache-inhibited in the MMU.&lt;/EM&gt;&lt;/P&gt;&lt;P style="background-color: #ffffff; border: 0px;"&gt;&lt;SPAN style="color: #51626f;"&gt;How to make sure the Outbound window is configured as&amp;nbsp;cache-inhibited&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Sep 2019 10:33:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/On-Pci-Data-missing/m-p/946275#M2974</guid>
      <dc:creator>utkarsh_100</dc:creator>
      <dc:date>2019-09-25T10:33:09Z</dc:date>
    </item>
    <item>
      <title>Re: On Pci Data missing</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/On-Pci-Data-missing/m-p/946276#M2975</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;gt; &lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;&amp;nbsp;Fpga will be continuously writing onto the processor .Sorry for not explaining properly&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Which exactly data transfer is performed.&lt;/P&gt;&lt;P&gt;Please provide detailed explanation from your software/FPGA team.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Sep 2019 14:18:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/On-Pci-Data-missing/m-p/946276#M2975</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2019-09-25T14:18:07Z</dc:date>
    </item>
  </channel>
</rss>