<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MPC5674F  External Multiplex Bus CS need Variable Wait State Access in PowerQUICC Processors</title>
    <link>https://community.nxp.com/t5/PowerQUICC-Processors/MPC5674F-External-Multiplex-Bus-CS-need-Variable-Wait-State/m-p/930182#M2916</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;EM&gt;Most processors have an RDY signal line to tell the bus to hold until I am done&lt;STRONG&gt;.&lt;/STRONG&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;STRONG&gt;Configuration:&lt;/STRONG&gt;&amp;nbsp;&lt;/EM&gt; &lt;STRONG&gt;A&amp;nbsp; MPC5674F processor EBI external Multiplexed mode using chip select&amp;nbsp;Access.&lt;/STRONG&gt;&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;STRONG&gt;&amp;nbsp;&lt;/STRONG&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;STRONG&gt;Problem:&amp;nbsp;&amp;nbsp;&lt;/STRONG&gt;&lt;/EM&gt; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;If a peripheral tied to a single /CS on that external bus needs requires an extra&amp;nbsp; 2-3 wait states only part of the time, and "0" wait for states the majority of the time.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;STRONG&gt;QUESTION:&amp;nbsp;&lt;/STRONG&gt; &lt;/EM&gt;&amp;nbsp; &amp;nbsp; How do I tell the bus to extend add waits when the D_TA (bus acknowledge) signal&amp;nbsp;is automatically internally generated.&amp;nbsp; &amp;nbsp;&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Can I override the D_TA to extend that bus access?&lt;/LI&gt;&lt;LI&gt;Pull another line to inform the processor that the bus transfer is not complete and need more time?&lt;/LI&gt;&lt;/OL&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 02 Jul 2019 16:02:30 GMT</pubDate>
    <dc:creator>spetrofsky</dc:creator>
    <dc:date>2019-07-02T16:02:30Z</dc:date>
    <item>
      <title>MPC5674F  External Multiplex Bus CS need Variable Wait State Access</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/MPC5674F-External-Multiplex-Bus-CS-need-Variable-Wait-State/m-p/930182#M2916</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;EM&gt;Most processors have an RDY signal line to tell the bus to hold until I am done&lt;STRONG&gt;.&lt;/STRONG&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;STRONG&gt;Configuration:&lt;/STRONG&gt;&amp;nbsp;&lt;/EM&gt; &lt;STRONG&gt;A&amp;nbsp; MPC5674F processor EBI external Multiplexed mode using chip select&amp;nbsp;Access.&lt;/STRONG&gt;&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;STRONG&gt;&amp;nbsp;&lt;/STRONG&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;STRONG&gt;Problem:&amp;nbsp;&amp;nbsp;&lt;/STRONG&gt;&lt;/EM&gt; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;If a peripheral tied to a single /CS on that external bus needs requires an extra&amp;nbsp; 2-3 wait states only part of the time, and "0" wait for states the majority of the time.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;STRONG&gt;QUESTION:&amp;nbsp;&lt;/STRONG&gt; &lt;/EM&gt;&amp;nbsp; &amp;nbsp; How do I tell the bus to extend add waits when the D_TA (bus acknowledge) signal&amp;nbsp;is automatically internally generated.&amp;nbsp; &amp;nbsp;&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Can I override the D_TA to extend that bus access?&lt;/LI&gt;&lt;LI&gt;Pull another line to inform the processor that the bus transfer is not complete and need more time?&lt;/LI&gt;&lt;/OL&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 02 Jul 2019 16:02:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/MPC5674F-External-Multiplex-Bus-CS-need-Variable-Wait-State/m-p/930182#M2916</guid>
      <dc:creator>spetrofsky</dc:creator>
      <dc:date>2019-07-02T16:02:30Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5674F  External Multiplex Bus CS need Variable Wait State Access</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/MPC5674F-External-Multiplex-Bus-CS-need-Variable-Wait-State/m-p/930183#M2917</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I am afraid it is not possible. TA signal is explicitly defined as output or input, in accordance to SETA bit definition.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;SETA Select External Transfer Acknowledge&lt;/P&gt;&lt;P&gt;0 Transfer Acknowledge (D_TA) is an output from the EBI, data phase will be terminated by the EBI.&lt;/P&gt;&lt;P&gt;1 Transfer Acknowledge (D_TA) is an input to the EBI, data phase will be terminated by an external device.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In case of using of FPGA, customers typically use externally terminated mode (SETA = 1) or non-CS access what’s the same from the point of view of TA usage just to have possibility to have various access times.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 08 Jul 2019 12:18:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/MPC5674F-External-Multiplex-Bus-CS-need-Variable-Wait-State/m-p/930183#M2917</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2019-07-08T12:18:56Z</dc:date>
    </item>
  </channel>
</rss>