<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: mpc860 codewarrior debug issue in PowerQUICC Processors</title>
    <link>https://community.nxp.com/t5/PowerQUICC-Processors/mpc860-codewarrior-debug-issue/m-p/877319#M2733</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Exception 0x01000 is generated on unimplemented instruction or instruction with unimplemented register.&lt;/P&gt;&lt;P&gt;The following is said in MPC860 Reference Manual, Section 6.1.3.1:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;6.1.3.1 Software Emulation Exception (0x01000)&lt;BR /&gt;An software emulation exception occurs as a result of one of the following conditions:&lt;BR /&gt;• When executing any unimplemented instruction, including all illegal and unimplemented&lt;BR /&gt;optional and floating-point instructions.&lt;BR /&gt;• When executing a mtspr or mfspr that specifies an on-core unimplemented register,&lt;BR /&gt;regardless of SPR[0].&lt;BR /&gt;• When executing a mtspr or mfspr that specifies an off-core unimplemented register and&lt;BR /&gt;SPR[0] = 0 or MSR[PR] = 0 (no program exception condition).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, please run the board under debugger control and check, which particular instruction causes this error. If instruction looks correct, than this means hardware issue - the core reads correct instruction incorreclty due to some hardware reason. In this case please check basic things - reset configuration settings, clock settings, power supply quality, and etc.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Alexander,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 09 Apr 2019 20:05:19 GMT</pubDate>
    <dc:creator>alexander_yakov</dc:creator>
    <dc:date>2019-04-09T20:05:19Z</dc:date>
    <item>
      <title>mpc860 codewarrior debug issue</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/mpc860-codewarrior-debug-issue/m-p/877318#M2732</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;we are using MPC860TCVR66D4 Powerquicc Processor with Codewarrior 8.8 IDE where we are unable enter in to the Debug Mode Can any one help us.&lt;/P&gt;&lt;P&gt;The error we are getting is Exception &lt;span class="lia-inline-image-display-wrapper" image-alt="Screenshot (8).png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/73029i80C10425BD0A5788/image-size/large?v=v2&amp;amp;px=999" role="button" title="Screenshot (8).png" alt="Screenshot (8).png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Apr 2019 08:54:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/mpc860-codewarrior-debug-issue/m-p/877318#M2732</guid>
      <dc:creator>ravadasrikanth3</dc:creator>
      <dc:date>2019-04-04T08:54:32Z</dc:date>
    </item>
    <item>
      <title>Re: mpc860 codewarrior debug issue</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/mpc860-codewarrior-debug-issue/m-p/877319#M2733</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Exception 0x01000 is generated on unimplemented instruction or instruction with unimplemented register.&lt;/P&gt;&lt;P&gt;The following is said in MPC860 Reference Manual, Section 6.1.3.1:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;6.1.3.1 Software Emulation Exception (0x01000)&lt;BR /&gt;An software emulation exception occurs as a result of one of the following conditions:&lt;BR /&gt;• When executing any unimplemented instruction, including all illegal and unimplemented&lt;BR /&gt;optional and floating-point instructions.&lt;BR /&gt;• When executing a mtspr or mfspr that specifies an on-core unimplemented register,&lt;BR /&gt;regardless of SPR[0].&lt;BR /&gt;• When executing a mtspr or mfspr that specifies an off-core unimplemented register and&lt;BR /&gt;SPR[0] = 0 or MSR[PR] = 0 (no program exception condition).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, please run the board under debugger control and check, which particular instruction causes this error. If instruction looks correct, than this means hardware issue - the core reads correct instruction incorreclty due to some hardware reason. In this case please check basic things - reset configuration settings, clock settings, power supply quality, and etc.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Alexander,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Apr 2019 20:05:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/mpc860-codewarrior-debug-issue/m-p/877319#M2733</guid>
      <dc:creator>alexander_yakov</dc:creator>
      <dc:date>2019-04-09T20:05:19Z</dc:date>
    </item>
  </channel>
</rss>