<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MPC8270 booting from SST39VF040 but not booting from S29GL512T ? in PowerQUICC Processors</title>
    <link>https://community.nxp.com/t5/PowerQUICC-Processors/MPC8270-booting-from-SST39VF040-but-not-booting-from-S29GL512T/m-p/875122#M2714</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am working on MPC8270 Power Quic II processor. We designed a board using this processor and because of some doubt we used two bootflashes at Chip Select 0 (CS0), with a selection switch. One bootflash is SST39VF040 (512KB) and other is&amp;nbsp;S29GL512T (64MB). Hardware wise both are okay as our processor can read write erase both these flashes whenever either of these is selected.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Problem&lt;/STRONG&gt;&amp;nbsp;:&lt;/P&gt;&lt;P&gt;Problem comes when we try to boot from these flashes.&amp;nbsp;&lt;SPAN&gt;SST39VF040&amp;nbsp;works fine and processor boots fine. But with&amp;nbsp;S29GL512T&amp;nbsp;processor is not booting.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&lt;SPAN&gt;Speculation :&lt;/SPAN&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;1 - MPC8270 says reset vector lies at 0xFFF00100 and with&amp;nbsp;&lt;SPAN&gt;SST39VF040, when we program the flash starting address is 0xFFF00000 and it works fine. But for&amp;nbsp;S29GL512T&amp;nbsp;we have to give starting address 0xF0000000, beacause it is 64MB flash we cannot give 0xFFF00000. Is this the problem? &lt;STRONG&gt;If this is the problem then it means with MPC8270 we cannot boot from a bootflash greater than 1024KB&lt;/STRONG&gt; because range from 0xFFF00000 - 0xFFF7FFFF is 0xFFFFF (1024Kb) .&amp;nbsp;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN&gt;2 - Access time of&amp;nbsp;SST39VF040 is 45ns and&amp;nbsp;S29GL512T is 100ns. When MPC8270 is fetching HCRW from 0xFFF00100 at CS0, what access time it follows?&amp;nbsp;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 20 Feb 2019 06:30:43 GMT</pubDate>
    <dc:creator>muhammadahmed47</dc:creator>
    <dc:date>2019-02-20T06:30:43Z</dc:date>
    <item>
      <title>MPC8270 booting from SST39VF040 but not booting from S29GL512T ?</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/MPC8270-booting-from-SST39VF040-but-not-booting-from-S29GL512T/m-p/875122#M2714</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am working on MPC8270 Power Quic II processor. We designed a board using this processor and because of some doubt we used two bootflashes at Chip Select 0 (CS0), with a selection switch. One bootflash is SST39VF040 (512KB) and other is&amp;nbsp;S29GL512T (64MB). Hardware wise both are okay as our processor can read write erase both these flashes whenever either of these is selected.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Problem&lt;/STRONG&gt;&amp;nbsp;:&lt;/P&gt;&lt;P&gt;Problem comes when we try to boot from these flashes.&amp;nbsp;&lt;SPAN&gt;SST39VF040&amp;nbsp;works fine and processor boots fine. But with&amp;nbsp;S29GL512T&amp;nbsp;processor is not booting.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&lt;SPAN&gt;Speculation :&lt;/SPAN&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;1 - MPC8270 says reset vector lies at 0xFFF00100 and with&amp;nbsp;&lt;SPAN&gt;SST39VF040, when we program the flash starting address is 0xFFF00000 and it works fine. But for&amp;nbsp;S29GL512T&amp;nbsp;we have to give starting address 0xF0000000, beacause it is 64MB flash we cannot give 0xFFF00000. Is this the problem? &lt;STRONG&gt;If this is the problem then it means with MPC8270 we cannot boot from a bootflash greater than 1024KB&lt;/STRONG&gt; because range from 0xFFF00000 - 0xFFF7FFFF is 0xFFFFF (1024Kb) .&amp;nbsp;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN&gt;2 - Access time of&amp;nbsp;SST39VF040 is 45ns and&amp;nbsp;S29GL512T is 100ns. When MPC8270 is fetching HCRW from 0xFFF00100 at CS0, what access time it follows?&amp;nbsp;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Feb 2019 06:30:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/MPC8270-booting-from-SST39VF040-but-not-booting-from-S29GL512T/m-p/875122#M2714</guid>
      <dc:creator>muhammadahmed47</dc:creator>
      <dc:date>2019-02-20T06:30:43Z</dc:date>
    </item>
    <item>
      <title>Re: MPC8270 booting from SST39VF040 but not booting from S29GL512T ?</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/MPC8270-booting-from-SST39VF040-but-not-booting-from-S29GL512T/m-p/875123#M2715</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You wrote:&lt;/P&gt;&lt;P&gt;&amp;gt; &lt;SPAN&gt;But for&amp;nbsp;S29GL512T&amp;nbsp;we have to give starting address 0xF0000000,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;gt; beacause it is 64MB flash we cannot give 0xFFF00000.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;This is not absolutely required.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;The only limitation is the OR0[AM] reset value which defines 32MB chip-select 0.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;In this case the boot image has to be correctly "positioned" inside the 64MB Flash during programming.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;gt; we cannot boot from a bootflash greater than 1024KB because&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;gt; range from 0xFFF00000 - 0xFFF7FFFF is 0xFFFFF (1024Kb)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;This conclusion is incorrect.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Please consider that the Initial internal space base address is defined in the HRCW[ISB].&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Feb 2019 15:19:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/MPC8270-booting-from-SST39VF040-but-not-booting-from-S29GL512T/m-p/875123#M2715</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2019-02-20T15:19:19Z</dc:date>
    </item>
  </channel>
</rss>