<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>PowerQUICC Processors中的主题 EP8548e - unable to boot linux</title>
    <link>https://community.nxp.com/t5/PowerQUICC-Processors/EP8548e-unable-to-boot-linux/m-p/136876#M27</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hi,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I am using an Embedded Planet board&amp;nbsp; based on the 8548E PowerQuic III processor.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Using the "vmlinux.gz.uboot" and "rootfs.ext2.gz.uboot" from the CDROM "/cdrom/files/", I am unable to boot the kernel on the 8548e.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I'm pretty sure I'm missing something basic, but I'm not too sure what.&amp;nbsp; Can anybody help?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;- Brandon&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;HR /&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;BLOCKQUOTE&gt;&lt;DIV&gt;U-Boot 1.1.4 EKB-22022006 (Apr 28 2006 - 16:02:51)&lt;BR /&gt;CPU: 8548_E, Version: 2.0, (0x80390020)&lt;BR /&gt;Core: E500, Version: 2.0, (0x80210020)&lt;BR /&gt;Clock Configuration:&lt;BR /&gt;CPU:1066 MHz, CCB: 533 MHz,&lt;BR /&gt;DDR: 266 MHz, LBC: 66 MHz&lt;BR /&gt;L1: D-cache 32 kB enabled&lt;BR /&gt;I-cache 32 kB enabled&lt;BR /&gt;Board: MPC8548AMC.&lt;BR /&gt;I2C: ready&lt;BR /&gt;DRAM: Initializing&lt;BR /&gt;MODULE: HITR28UFA 256MB&lt;BR /&gt;DDR: 256 MB&lt;BR /&gt;FLASH: 16 MB&lt;BR /&gt;L2 cache 512KB: enabled&lt;BR /&gt;In: serial&lt;BR /&gt;Out: serial&lt;BR /&gt;Err: serial&lt;BR /&gt;Net: eTSEC0, eTSEC1, eTSEC2, eTSEC3&lt;BR /&gt;AMC=&amp;gt;&lt;BR /&gt;AMC=&amp;gt;&lt;BR /&gt;AMC=&amp;gt;&lt;BR /&gt;AMC=&amp;gt; ping 157.165.28.220&lt;BR /&gt;Speed: 100, full duplex&lt;BR /&gt;Using eTSEC0 device&lt;BR /&gt;host 157.165.28.220 is alive&lt;BR /&gt;AMC=&amp;gt; tftp 1000000 vmlinux.gz.uboot&lt;BR /&gt;Speed: 100, full duplex&lt;BR /&gt;Using eTSEC0 device&lt;BR /&gt;TFTP from server 157.165.28.220; our IP address is 157.165.29.36&lt;BR /&gt;Filename 'vmlinux.gz.uboot'.&lt;BR /&gt;Load address: 0x1000000&lt;BR /&gt;Loading: #################################################################&lt;BR /&gt;#################################################################&lt;BR /&gt;##############################################################&lt;BR /&gt;done&lt;BR /&gt;Bytes transferred = 980940 (ef7cc hex)&lt;BR /&gt;AMC=&amp;gt; tftp 2000000 rootfs.ext2.gz.uboot&lt;BR /&gt;Speed: 100, full duplex&lt;BR /&gt;Using eTSEC0 device&lt;BR /&gt;TFTP from server 157.165.28.220; our IP address is 157.165.29.36&lt;BR /&gt;Filename 'rootfs.ext2.gz.uboot'.&lt;BR /&gt;Load address: 0x2000000&lt;BR /&gt;Loading: #################################################################&lt;BR /&gt;#################################################################&lt;BR /&gt;#################################################################&lt;BR /&gt;#################################################################&lt;BR /&gt;#################################################################&lt;BR /&gt;#################################################################&lt;BR /&gt;#################################################################&lt;BR /&gt;#################################################################&lt;BR /&gt;#################################################################&lt;BR /&gt;#################################################################&lt;BR /&gt;#################################################################&lt;BR /&gt;#################################################################&lt;BR /&gt;#################################################################&lt;BR /&gt;#################################################################&lt;BR /&gt;#################################################&lt;BR /&gt;done&lt;BR /&gt;Bytes transferred = 4908634 (4ae65a hex)&lt;BR /&gt;AMC=&amp;gt;&lt;BR /&gt;AMC=&amp;gt; bootm 1000000 2000000&lt;BR /&gt;## Booting image at 01000000 ...&lt;BR /&gt;Image Name: Linux for ep8548&lt;BR /&gt;Image Type: PowerPC Linux Kernel Image (gzip compressed)&lt;BR /&gt;Data Size: 980876 Bytes = 957.9 kB&lt;BR /&gt;Load Address: 00000000&lt;BR /&gt;Entry Point: 00000000&lt;BR /&gt;Verifying Checksum ... OK&lt;BR /&gt;Uncompressing Kernel Image ... OK&lt;BR /&gt;## Loading RAMDisk Image at 02000000 ...&lt;BR /&gt;Image Name: uboot ext2 ramdisk rootfs&lt;BR /&gt;Image Type: PowerPC Linux RAMDisk Image (gzip compressed)&lt;BR /&gt;Data Size: 4908570 Bytes = 4.7 MB&lt;BR /&gt;Load Address: 00000000&lt;BR /&gt;Entry Point: 00000000&lt;BR /&gt;Verifying Checksum ... OK&lt;BR /&gt;Loading Ramdisk to 0fafe000, end 0ffac61a ... OK&lt;/DIV&gt;&lt;/BLOCKQUOTE&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 15 Jun 2007 06:20:13 GMT</pubDate>
    <dc:creator>acolyte</dc:creator>
    <dc:date>2007-06-15T06:20:13Z</dc:date>
    <item>
      <title>EP8548e - unable to boot linux</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/EP8548e-unable-to-boot-linux/m-p/136876#M27</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hi,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I am using an Embedded Planet board&amp;nbsp; based on the 8548E PowerQuic III processor.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Using the "vmlinux.gz.uboot" and "rootfs.ext2.gz.uboot" from the CDROM "/cdrom/files/", I am unable to boot the kernel on the 8548e.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I'm pretty sure I'm missing something basic, but I'm not too sure what.&amp;nbsp; Can anybody help?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;- Brandon&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;HR /&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;BLOCKQUOTE&gt;&lt;DIV&gt;U-Boot 1.1.4 EKB-22022006 (Apr 28 2006 - 16:02:51)&lt;BR /&gt;CPU: 8548_E, Version: 2.0, (0x80390020)&lt;BR /&gt;Core: E500, Version: 2.0, (0x80210020)&lt;BR /&gt;Clock Configuration:&lt;BR /&gt;CPU:1066 MHz, CCB: 533 MHz,&lt;BR /&gt;DDR: 266 MHz, LBC: 66 MHz&lt;BR /&gt;L1: D-cache 32 kB enabled&lt;BR /&gt;I-cache 32 kB enabled&lt;BR /&gt;Board: MPC8548AMC.&lt;BR /&gt;I2C: ready&lt;BR /&gt;DRAM: Initializing&lt;BR /&gt;MODULE: HITR28UFA 256MB&lt;BR /&gt;DDR: 256 MB&lt;BR /&gt;FLASH: 16 MB&lt;BR /&gt;L2 cache 512KB: enabled&lt;BR /&gt;In: serial&lt;BR /&gt;Out: serial&lt;BR /&gt;Err: serial&lt;BR /&gt;Net: eTSEC0, eTSEC1, eTSEC2, eTSEC3&lt;BR /&gt;AMC=&amp;gt;&lt;BR /&gt;AMC=&amp;gt;&lt;BR /&gt;AMC=&amp;gt;&lt;BR /&gt;AMC=&amp;gt; ping 157.165.28.220&lt;BR /&gt;Speed: 100, full duplex&lt;BR /&gt;Using eTSEC0 device&lt;BR /&gt;host 157.165.28.220 is alive&lt;BR /&gt;AMC=&amp;gt; tftp 1000000 vmlinux.gz.uboot&lt;BR /&gt;Speed: 100, full duplex&lt;BR /&gt;Using eTSEC0 device&lt;BR /&gt;TFTP from server 157.165.28.220; our IP address is 157.165.29.36&lt;BR /&gt;Filename 'vmlinux.gz.uboot'.&lt;BR /&gt;Load address: 0x1000000&lt;BR /&gt;Loading: #################################################################&lt;BR /&gt;#################################################################&lt;BR /&gt;##############################################################&lt;BR /&gt;done&lt;BR /&gt;Bytes transferred = 980940 (ef7cc hex)&lt;BR /&gt;AMC=&amp;gt; tftp 2000000 rootfs.ext2.gz.uboot&lt;BR /&gt;Speed: 100, full duplex&lt;BR /&gt;Using eTSEC0 device&lt;BR /&gt;TFTP from server 157.165.28.220; our IP address is 157.165.29.36&lt;BR /&gt;Filename 'rootfs.ext2.gz.uboot'.&lt;BR /&gt;Load address: 0x2000000&lt;BR /&gt;Loading: #################################################################&lt;BR /&gt;#################################################################&lt;BR /&gt;#################################################################&lt;BR /&gt;#################################################################&lt;BR /&gt;#################################################################&lt;BR /&gt;#################################################################&lt;BR /&gt;#################################################################&lt;BR /&gt;#################################################################&lt;BR /&gt;#################################################################&lt;BR /&gt;#################################################################&lt;BR /&gt;#################################################################&lt;BR /&gt;#################################################################&lt;BR /&gt;#################################################################&lt;BR /&gt;#################################################################&lt;BR /&gt;#################################################&lt;BR /&gt;done&lt;BR /&gt;Bytes transferred = 4908634 (4ae65a hex)&lt;BR /&gt;AMC=&amp;gt;&lt;BR /&gt;AMC=&amp;gt; bootm 1000000 2000000&lt;BR /&gt;## Booting image at 01000000 ...&lt;BR /&gt;Image Name: Linux for ep8548&lt;BR /&gt;Image Type: PowerPC Linux Kernel Image (gzip compressed)&lt;BR /&gt;Data Size: 980876 Bytes = 957.9 kB&lt;BR /&gt;Load Address: 00000000&lt;BR /&gt;Entry Point: 00000000&lt;BR /&gt;Verifying Checksum ... OK&lt;BR /&gt;Uncompressing Kernel Image ... OK&lt;BR /&gt;## Loading RAMDisk Image at 02000000 ...&lt;BR /&gt;Image Name: uboot ext2 ramdisk rootfs&lt;BR /&gt;Image Type: PowerPC Linux RAMDisk Image (gzip compressed)&lt;BR /&gt;Data Size: 4908570 Bytes = 4.7 MB&lt;BR /&gt;Load Address: 00000000&lt;BR /&gt;Entry Point: 00000000&lt;BR /&gt;Verifying Checksum ... OK&lt;BR /&gt;Loading Ramdisk to 0fafe000, end 0ffac61a ... OK&lt;/DIV&gt;&lt;/BLOCKQUOTE&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Jun 2007 06:20:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/EP8548e-unable-to-boot-linux/m-p/136876#M27</guid>
      <dc:creator>acolyte</dc:creator>
      <dc:date>2007-06-15T06:20:13Z</dc:date>
    </item>
    <item>
      <title>Re: EP8548e - unable to boot linux</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/EP8548e-unable-to-boot-linux/m-p/136877#M28</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;Hi all,&lt;BR /&gt;&amp;nbsp;&amp;nbsp; I have found the same problem using the EP8548rev2.&lt;BR /&gt;It seems that, once the Linux image is loaded into the RAM, it doesn't start.&lt;BR /&gt;My configuration is quite different, I'm using a rImage.gz that contains both the kernel image and the RAM disk image. This compressed image is stored in FLASH at the address 0xFF000000&lt;BR /&gt;I have tried to boot the same kernel via NFS and it works fine, and I have tried to use the same rImage.gz on the EP8548rev1 and it also works. I think there is a problem when the kernel must boot once it is placed in the RAM probably&amp;nbsp; due to a misconfigurations of the rev2 board.&lt;BR /&gt;Does anyone have any suggestions?&lt;BR /&gt;&lt;BR /&gt;Thanks, Paolo&lt;BR /&gt;&lt;BR /&gt;Here my u-boot onfiguration:&lt;BR /&gt;&lt;BR /&gt;bootdelay=5&lt;BR /&gt;baudrate=115200&lt;BR /&gt;loads_echo=1&lt;BR /&gt;bootfile="u-boot.amc.rev4"&lt;BR /&gt;loadaddr=1000000&lt;BR /&gt;ethact=eTSEC0&lt;BR /&gt;ethaddr=00:10:ec:00:df:0e&lt;BR /&gt;eth1addr=00:10:ec:80:df:0e&lt;BR /&gt;eth2addr=00:10:ec:40:df:0e&lt;BR /&gt;eth3addr=00:10:ec:c0:df:0e&lt;BR /&gt;serverip.orig=10.0.0.58&lt;BR /&gt;serverip=172.16.0.1&lt;BR /&gt;ipaddr.orig=10.0.0.252&lt;BR /&gt;ipaddr=172.16.0.5&lt;BR /&gt;bootargs.orig=root=/dev/ram rw console=ttyS0,115200 riohdid=0&lt;BR /&gt;bootargs=root=/dev/ram rw console=ttyS0,115200 ip=172.16.0.5:::255.255.255.0::eth0&lt;BR /&gt;bootcmd=bootm 0xFF000000&lt;BR /&gt;pram=131072k&lt;BR /&gt;mem=2097152k&lt;BR /&gt;stdin=serial&lt;BR /&gt;stdout=serial&lt;BR /&gt;stderr=serial&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;Here my output:&lt;BR /&gt;&lt;BR /&gt;U-Boot 1.1.4 EKB-22022006 (Apr 28 2006 - 16:02:51)&lt;BR /&gt;&lt;BR /&gt;CPU:&amp;nbsp;&amp;nbsp; 8548_E, Version: 2.0, (0x80390020)&lt;BR /&gt;Core:&amp;nbsp; E500, Version: 2.0, (0x80210020)&lt;BR /&gt;Clock Configuration:&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; CPU: 999 MHz, CCB: 333 MHz,&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; DDR: 166 MHz, LBC:&amp;nbsp; 41 MHz&lt;BR /&gt;L1:&amp;nbsp;&amp;nbsp;&amp;nbsp; D-cache 32 kB enabled&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I-cache 32 kB enabled&lt;BR /&gt;Board: MPC8548AMC.&lt;BR /&gt;I2C:&amp;nbsp;&amp;nbsp; ready&lt;BR /&gt;DRAM:&amp;nbsp; Initializing&lt;BR /&gt;MODULE:&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; DDR: 256 MB&lt;BR /&gt;FLASH: 16 MB&lt;BR /&gt;L2 cache 512KB: enabled&lt;BR /&gt;In:&amp;nbsp;&amp;nbsp;&amp;nbsp; serial&lt;BR /&gt;Out:&amp;nbsp;&amp;nbsp; serial&lt;BR /&gt;Err:&amp;nbsp;&amp;nbsp; serial&lt;BR /&gt;Net:&amp;nbsp;&amp;nbsp; eTSEC0, eTSEC1, eTSEC2, eTSEC3&lt;BR /&gt;Hit any key to stop autoboot:&amp;nbsp; 0&lt;BR /&gt;## Booting image at ff000000 ...&lt;BR /&gt;&amp;nbsp;&amp;nbsp; Image Name:&amp;nbsp;&amp;nbsp; Kernel and Ramdisk&lt;BR /&gt;&amp;nbsp;&amp;nbsp; Image Type:&amp;nbsp;&amp;nbsp; PowerPC Linux Multi-File Image (gzip compressed)&lt;BR /&gt;&amp;nbsp;&amp;nbsp; Data Size:&amp;nbsp;&amp;nbsp;&amp;nbsp; 3402792 Bytes =&amp;nbsp; 3.2 MB&lt;BR /&gt;&amp;nbsp;&amp;nbsp; Load Address: 00000000&lt;BR /&gt;&amp;nbsp;&amp;nbsp; Entry Point:&amp;nbsp; 00000000&lt;BR /&gt;&amp;nbsp;&amp;nbsp; Contents:&lt;BR /&gt;&amp;nbsp;&amp;nbsp; Image 0:&amp;nbsp; 1012171 Bytes = 988.4 kB&lt;BR /&gt;&amp;nbsp;&amp;nbsp; Image 1:&amp;nbsp; 2390608 Bytes =&amp;nbsp; 2.3 MB&lt;BR /&gt;&amp;nbsp;&amp;nbsp; Verifying Checksum ... OK&lt;BR /&gt;&amp;nbsp;&amp;nbsp; Uncompressing Multi-File Image ... OK&lt;BR /&gt;&amp;nbsp;&amp;nbsp; Loading Ramdisk to 0fd65000, end 0ffaca50 ... OK&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;BR /&gt;&lt;BR /&gt;Message Edited by Paolo Treffiletti on &lt;SPAN class="date_text"&gt;2007-07-09&lt;/SPAN&gt; &lt;SPAN class="time_text"&gt;02:52 PM&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Jul 2007 20:51:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/EP8548e-unable-to-boot-linux/m-p/136877#M28</guid>
      <dc:creator>PaoloTreffilett</dc:creator>
      <dc:date>2007-07-09T20:51:50Z</dc:date>
    </item>
    <item>
      <title>Re: EP8548e - unable to boot linux</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/EP8548e-unable-to-boot-linux/m-p/136878#M29</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Just an update:&lt;BR /&gt;I tried to used the BSP for the EP8548v1.1 on the EP8548v1.2 and it didn't work.&lt;BR /&gt;The "solution" that I have found is to use the BSP for the EP8548v1.2 mezzanine.&lt;BR /&gt;&lt;BR /&gt;Best regards&lt;BR /&gt;Paolo&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Sep 2007 15:47:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/EP8548e-unable-to-boot-linux/m-p/136878#M29</guid>
      <dc:creator>PaoloTreffilett</dc:creator>
      <dc:date>2007-09-21T15:47:57Z</dc:date>
    </item>
  </channel>
</rss>