<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MPC8313 SGMII with 1588 timestamping in PowerQUICC Processors</title>
    <link>https://community.nxp.com/t5/PowerQUICC-Processors/MPC8313-SGMII-with-1588-timestamping/m-p/829316#M2573</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The errata says this problem is fixed in rev. 2.x silicon; but with the latest silicon revision, the reference manual states that timestamping is not supported in SGMII mode 10 / 100; meaning it does not work at 10Mbps and 100Mbps but is working at 1Gbps. Any reason why it does not work with the slower speeds ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yves&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 29 Jun 2018 12:15:18 GMT</pubDate>
    <dc:creator>ybelanger</dc:creator>
    <dc:date>2018-06-29T12:15:18Z</dc:date>
    <item>
      <title>MPC8313 SGMII with 1588 timestamping</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/MPC8313-SGMII-with-1588-timestamping/m-p/829314#M2571</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;According to the MPC8313 Reference Manual :&amp;nbsp;"IEEE 1588 timestamping not supported in conjunction with the SGMII 10/100 interface mode"; why is that ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Jun 2018 18:47:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/MPC8313-SGMII-with-1588-timestamping/m-p/829314#M2571</guid>
      <dc:creator>ybelanger</dc:creator>
      <dc:date>2018-06-28T18:47:03Z</dc:date>
    </item>
    <item>
      <title>Re: MPC8313 SGMII with 1588 timestamping</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/MPC8313-SGMII-with-1588-timestamping/m-p/829315#M2572</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;MPC8313 is quite old device, introduced ~12 years ago, and actually - one of the first devices with hardware timestamping.&lt;/P&gt;&lt;P&gt;According to MPC8313 device errata, IEEE 1588_2: "IEEE 1588 not supported in SGMII mode", timestamping in SGMII mode is not supported because TSEC controller does not properly support timestamping on SGMII interface. Note - MPC8313 device errata states this problem is fixed in rev. 2.0 silicon&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Alexander&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 29 Jun 2018 01:40:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/MPC8313-SGMII-with-1588-timestamping/m-p/829315#M2572</guid>
      <dc:creator>alexander_yakov</dc:creator>
      <dc:date>2018-06-29T01:40:37Z</dc:date>
    </item>
    <item>
      <title>Re: MPC8313 SGMII with 1588 timestamping</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/MPC8313-SGMII-with-1588-timestamping/m-p/829316#M2573</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The errata says this problem is fixed in rev. 2.x silicon; but with the latest silicon revision, the reference manual states that timestamping is not supported in SGMII mode 10 / 100; meaning it does not work at 10Mbps and 100Mbps but is working at 1Gbps. Any reason why it does not work with the slower speeds ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yves&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 29 Jun 2018 12:15:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/MPC8313-SGMII-with-1588-timestamping/m-p/829316#M2573</guid>
      <dc:creator>ybelanger</dc:creator>
      <dc:date>2018-06-29T12:15:18Z</dc:date>
    </item>
  </channel>
</rss>