<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>PowerQUICC Processors中的主题 MPC870 RESET</title>
    <link>https://community.nxp.com/t5/PowerQUICC-Processors/MPC870-RESET/m-p/826200#M2549</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;BR /&gt;My question are related to the MPC870.&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Is s/w watchdog reset reflected on the HRESET* pin? My observations show it is not but the reset process is carried out. I would like your confirmation.&lt;/LI&gt;&lt;LI&gt;The above question follows behavior depicted on the attached picture. I see HRESET* asserted (for unknown reason at this point). The boot process starts but soon the HRESET* asserted again. this scenario repeats itself several times and eventually the HRESET* stays asserted until I (manually) power it up. As said, I do not know what cause the reset at the middle of of work (under investigation, likely h/w issue). Has somebody encountered this scenario or has explanation for this.&lt;/LI&gt;&lt;LI&gt;In order to generate check-stop case I did the following:&lt;BR /&gt; Setting PLPRCR[CSR] bit.&lt;BR /&gt; Clearing MSR[ME] bit.&lt;BR /&gt; Clearing MSR[DR] bit (to avoid MMU exception).&lt;BR /&gt; Access none-existing address.&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;I have experienced check-stop but the RSR[SWRS] was set rather than RSR[CSRS], meaning the s/w watchdog took the lead. If I repeat the above steps after disabling the the s/w watchdog the device was halted but no reset followed. Any idea?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank You&lt;/P&gt;&lt;P&gt;David&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 14 Sep 2018 16:14:53 GMT</pubDate>
    <dc:creator>MPC8313ERDB_h</dc:creator>
    <dc:date>2018-09-14T16:14:53Z</dc:date>
    <item>
      <title>MPC870 RESET</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/MPC870-RESET/m-p/826200#M2549</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;BR /&gt;My question are related to the MPC870.&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Is s/w watchdog reset reflected on the HRESET* pin? My observations show it is not but the reset process is carried out. I would like your confirmation.&lt;/LI&gt;&lt;LI&gt;The above question follows behavior depicted on the attached picture. I see HRESET* asserted (for unknown reason at this point). The boot process starts but soon the HRESET* asserted again. this scenario repeats itself several times and eventually the HRESET* stays asserted until I (manually) power it up. As said, I do not know what cause the reset at the middle of of work (under investigation, likely h/w issue). Has somebody encountered this scenario or has explanation for this.&lt;/LI&gt;&lt;LI&gt;In order to generate check-stop case I did the following:&lt;BR /&gt; Setting PLPRCR[CSR] bit.&lt;BR /&gt; Clearing MSR[ME] bit.&lt;BR /&gt; Clearing MSR[DR] bit (to avoid MMU exception).&lt;BR /&gt; Access none-existing address.&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;I have experienced check-stop but the RSR[SWRS] was set rather than RSR[CSRS], meaning the s/w watchdog took the lead. If I repeat the above steps after disabling the the s/w watchdog the device was halted but no reset followed. Any idea?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank You&lt;/P&gt;&lt;P&gt;David&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 14 Sep 2018 16:14:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/MPC870-RESET/m-p/826200#M2549</guid>
      <dc:creator>MPC8313ERDB_h</dc:creator>
      <dc:date>2018-09-14T16:14:53Z</dc:date>
    </item>
    <item>
      <title>Re: MPC870 RESET</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/MPC870-RESET/m-p/826201#M2550</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; color: black;"&gt;Check the &lt;/SPAN&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;Debug Enable Register (DER) value for reset generation from checkstop.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Pavel Chubakov&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 02 Oct 2018 05:43:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/MPC870-RESET/m-p/826201#M2550</guid>
      <dc:creator>Pavel</dc:creator>
      <dc:date>2018-10-02T05:43:26Z</dc:date>
    </item>
  </channel>
</rss>