<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: How can I install Codewarrior v8.8 in linux OS(Ubuntu 16.04) in PowerQUICC Processors</title>
    <link>https://community.nxp.com/t5/PowerQUICC-Processors/How-can-I-install-Codewarrior-v8-8-in-linux-OS-Ubuntu-16-04/m-p/799458#M2468</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;As I can only get the Windows-hosted installation package for version 8.8, which is .exe file.&lt;/P&gt;&lt;P&gt;Is it suitable to install in Ubuntu?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 31 Jul 2018 08:55:11 GMT</pubDate>
    <dc:creator>jinyu_zhang</dc:creator>
    <dc:date>2018-07-31T08:55:11Z</dc:date>
    <item>
      <title>How can I install Codewarrior v8.8 in linux OS(Ubuntu 16.04)</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/How-can-I-install-Codewarrior-v8-8-in-linux-OS-Ubuntu-16-04/m-p/799456#M2466</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm attemping to install codewarrior IDE in Ubuntu16.04. But I get the installation package from NXP as an exe file. How can I install it into the target OS?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 Jul 2018 09:42:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/How-can-I-install-Codewarrior-v8-8-in-linux-OS-Ubuntu-16-04/m-p/799456#M2466</guid>
      <dc:creator>jinyu_zhang</dc:creator>
      <dc:date>2018-07-30T09:42:31Z</dc:date>
    </item>
    <item>
      <title>Re: How can I install Codewarrior v8.8 in linux OS(Ubuntu 16.04)</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/How-can-I-install-Codewarrior-v8-8-in-linux-OS-Ubuntu-16-04/m-p/799457#M2467</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; color: black;"&gt;Use Ubuntu 10 or Ubuntu 12 for installing CodeWarrior 8.8 for Linux.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Pavel Chubakov&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 31 Jul 2018 06:38:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/How-can-I-install-Codewarrior-v8-8-in-linux-OS-Ubuntu-16-04/m-p/799457#M2467</guid>
      <dc:creator>Pavel</dc:creator>
      <dc:date>2018-07-31T06:38:12Z</dc:date>
    </item>
    <item>
      <title>Re: How can I install Codewarrior v8.8 in linux OS(Ubuntu 16.04)</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/How-can-I-install-Codewarrior-v8-8-in-linux-OS-Ubuntu-16-04/m-p/799458#M2468</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;As I can only get the Windows-hosted installation package for version 8.8, which is .exe file.&lt;/P&gt;&lt;P&gt;Is it suitable to install in Ubuntu?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 31 Jul 2018 08:55:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/How-can-I-install-Codewarrior-v8-8-in-linux-OS-Ubuntu-16-04/m-p/799458#M2468</guid>
      <dc:creator>jinyu_zhang</dc:creator>
      <dc:date>2018-07-31T08:55:11Z</dc:date>
    </item>
  </channel>
</rss>