<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>PowerQUICC ProcessorsのトピックRe: T1014 RGMII</title>
    <link>https://community.nxp.com/t5/PowerQUICC-Processors/T1014-RGMII/m-p/787649#M2440</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;T1014 Ethernet ports are controlled by DPAA. DPAA initialization &lt;BR /&gt;sequence consists of multiple steps, so it is not possible to tell what&lt;BR /&gt;you missed based on the information you provided. Here are some simple &lt;BR /&gt;diagnostic steps you can start with:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. Turn on loopback on the problematic MAC. See T1024DPAARM, &lt;BR /&gt;&amp;nbsp;&amp;nbsp; Section 6.4.3.1.1. If you are not able to send and receive in loopback, &lt;BR /&gt;&amp;nbsp;&amp;nbsp; make sure EC1_GTX_CLK125 clock is active, verify the initialization &lt;BR /&gt;&amp;nbsp;&amp;nbsp; sequence, check for errors returned by your driver and DPAA.&lt;BR /&gt;&amp;nbsp; &amp;nbsp;&lt;BR /&gt;2. If the the MAC-level loopback works, it means DPAA and MAC are initialized&lt;BR /&gt;&amp;nbsp;&amp;nbsp; correctly. Try setting up loopback in the PHY. Refer to your PHY &lt;BR /&gt;&amp;nbsp;&amp;nbsp; documentation on how to do that. If the PHY-level loopback does no&lt;BR /&gt;&amp;nbsp;&amp;nbsp; work, check the RGMII interface. Make sure the PHY data path is&lt;BR /&gt;&amp;nbsp;&amp;nbsp; actually connected to the PHY your MDIO is talking with.&lt;BR /&gt;&amp;nbsp; &amp;nbsp;&lt;BR /&gt;3. If all kinds of loopback work, but you still can't hear from the&lt;BR /&gt;&amp;nbsp;&amp;nbsp; external host, diagnose the PHY and the link to the host. Consult&lt;BR /&gt;&amp;nbsp;&amp;nbsp; at the PHY documentation or manufacturer.&lt;BR /&gt;&amp;nbsp; &amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Platon&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 25 Dec 2018 11:59:13 GMT</pubDate>
    <dc:creator>bpe</dc:creator>
    <dc:date>2018-12-25T11:59:13Z</dc:date>
    <item>
      <title>T1014 RGMII</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/T1014-RGMII/m-p/787648#M2439</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi,&lt;/P&gt;&lt;P&gt;we are using T1014 with EC1-RGMII as management port. In our case MAC4 is detected and BCM PHY is 1000M after AN. but ping is not sucessful even though MAC and IP is assigned .Do I miss something then. by the way ,we can use MDIO access PHY anyway.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Nov 2018 12:50:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/T1014-RGMII/m-p/787648#M2439</guid>
      <dc:creator>jinghui_mou1</dc:creator>
      <dc:date>2018-11-21T12:50:47Z</dc:date>
    </item>
    <item>
      <title>Re: T1014 RGMII</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/T1014-RGMII/m-p/787649#M2440</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;T1014 Ethernet ports are controlled by DPAA. DPAA initialization &lt;BR /&gt;sequence consists of multiple steps, so it is not possible to tell what&lt;BR /&gt;you missed based on the information you provided. Here are some simple &lt;BR /&gt;diagnostic steps you can start with:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. Turn on loopback on the problematic MAC. See T1024DPAARM, &lt;BR /&gt;&amp;nbsp;&amp;nbsp; Section 6.4.3.1.1. If you are not able to send and receive in loopback, &lt;BR /&gt;&amp;nbsp;&amp;nbsp; make sure EC1_GTX_CLK125 clock is active, verify the initialization &lt;BR /&gt;&amp;nbsp;&amp;nbsp; sequence, check for errors returned by your driver and DPAA.&lt;BR /&gt;&amp;nbsp; &amp;nbsp;&lt;BR /&gt;2. If the the MAC-level loopback works, it means DPAA and MAC are initialized&lt;BR /&gt;&amp;nbsp;&amp;nbsp; correctly. Try setting up loopback in the PHY. Refer to your PHY &lt;BR /&gt;&amp;nbsp;&amp;nbsp; documentation on how to do that. If the PHY-level loopback does no&lt;BR /&gt;&amp;nbsp;&amp;nbsp; work, check the RGMII interface. Make sure the PHY data path is&lt;BR /&gt;&amp;nbsp;&amp;nbsp; actually connected to the PHY your MDIO is talking with.&lt;BR /&gt;&amp;nbsp; &amp;nbsp;&lt;BR /&gt;3. If all kinds of loopback work, but you still can't hear from the&lt;BR /&gt;&amp;nbsp;&amp;nbsp; external host, diagnose the PHY and the link to the host. Consult&lt;BR /&gt;&amp;nbsp;&amp;nbsp; at the PHY documentation or manufacturer.&lt;BR /&gt;&amp;nbsp; &amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Platon&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 25 Dec 2018 11:59:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/T1014-RGMII/m-p/787649#M2440</guid>
      <dc:creator>bpe</dc:creator>
      <dc:date>2018-12-25T11:59:13Z</dc:date>
    </item>
  </channel>
</rss>