<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Latest HDLC Capable Processors in PowerQUICC Processors</title>
    <link>https://community.nxp.com/t5/PowerQUICC-Processors/Latest-HDLC-Capable-Processors/m-p/784675#M2434</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi everyone,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm having trouble finding recent processors that support HDLC. My current project uses the 8306 but it looks like that one has already been on the market for a while so I'm concerned about longevity with a new design.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The 8555E looks great as far as CPU speed, but also looks a bit dated and development boards seem to be obsolete.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I saw some threads about the UCC and that possibly being able to do HDLC? Does that mean there are other processors which support it which just may not advertise it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I appreciate everyone's help. I have extensive embedded background but am looking to do my first design with NXP/Freescale. Primary criteria is longevity and an available development board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Kris&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 15 Jun 2018 05:12:34 GMT</pubDate>
    <dc:creator>kris1</dc:creator>
    <dc:date>2018-06-15T05:12:34Z</dc:date>
    <item>
      <title>Latest HDLC Capable Processors</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/Latest-HDLC-Capable-Processors/m-p/784675#M2434</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi everyone,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm having trouble finding recent processors that support HDLC. My current project uses the 8306 but it looks like that one has already been on the market for a while so I'm concerned about longevity with a new design.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The 8555E looks great as far as CPU speed, but also looks a bit dated and development boards seem to be obsolete.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I saw some threads about the UCC and that possibly being able to do HDLC? Does that mean there are other processors which support it which just may not advertise it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I appreciate everyone's help. I have extensive embedded background but am looking to do my first design with NXP/Freescale. Primary criteria is longevity and an available development board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Kris&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Jun 2018 05:12:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/Latest-HDLC-Capable-Processors/m-p/784675#M2434</guid>
      <dc:creator>kris1</dc:creator>
      <dc:date>2018-06-15T05:12:34Z</dc:date>
    </item>
    <item>
      <title>Re: Latest HDLC Capable Processors</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/Latest-HDLC-Capable-Processors/m-p/784676#M2435</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The latest processors with PowerPC core and QE engine are the T-series processors&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/products/processors-and-microcontrollers/applications-processors/qoriq-platforms/t-series:QORIQ-POWER-ARCHITECTURE"&gt;https://www.nxp.com/products/processors-and-microcontrollers/applications-processors/qoriq-platforms/t-series:QORIQ-POWER-ARCHITECTURE&lt;/A&gt;&lt;/P&gt;&lt;P&gt;For example T1023/24&amp;nbsp; (2xe5500 core) and T1013/14(single e5500 core) have 2 UCCs for HDLC and Transparent protocols up to 50 Mbps full-duplex; 256 channels of HDLC/Transparent per UCC (UMCC). It will be available till April 2029. The same HDLC support you can find on the T1040/42 (till 2027).&lt;/P&gt;&lt;P&gt;Also you can check the P-series processors. For example P1025/P1016 (e500 core) have 4 UCCs and will be available till December 2024.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Jun 2018 10:49:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/Latest-HDLC-Capable-Processors/m-p/784676#M2435</guid>
      <dc:creator>r8070z</dc:creator>
      <dc:date>2018-06-15T10:49:33Z</dc:date>
    </item>
  </channel>
</rss>