<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>PowerQUICC Processors中的主题 Re: MPC8360E DDR Calibration</title>
    <link>https://community.nxp.com/t5/PowerQUICC-Processors/MPC8360E-DDR-Calibration/m-p/777671#M2417</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;1. It is up to the user. Automatic calibration was specially implemented to get the process faster/easier. SW override allows to set different output impedance values, e.g. to use fine tuning for your particular DDR system. Automatic calibration always sets value close to 18 Ohm.&lt;BR /&gt;2. DDRCDR is 0x730400001 at reset. Can be found, for example, in table 5-33.&lt;BR /&gt;3. DDRDSR always shows current impedance, for example after automatic calibration.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Bulat&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 03 May 2018 06:15:02 GMT</pubDate>
    <dc:creator>Bulat</dc:creator>
    <dc:date>2018-05-03T06:15:02Z</dc:date>
    <item>
      <title>MPC8360E DDR Calibration</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/MPC8360E-DDR-Calibration/m-p/777669#M2415</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Using the MPC 8360 processor.&amp;nbsp; Our question concerns the DDR Impedance calibration.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;OL style="margin-top: 0in;"&gt;&lt;LI&gt;Is it recommended to use the Automatic hardware Calibration, or the manual software calibration algorithm referenced in &lt;SPAN style="font-size: 12.0pt;"&gt;MPC8360ERM Rev. 3 (section 5.4.3.8)?&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;What is the power up value of the DDRCDR register?&amp;nbsp; I was unable to find it in the manuals.&lt;/LI&gt;&lt;LI&gt;The manual previously referenced does not indicate if the DDRDSR can be checked when using the Automatic hardware calibration to see if the Automatic Hardware calibration appears to be working.&amp;nbsp; Can it be used, or is there another method to determine what the Automatic Hardware calibration is setting the impedance to?&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Gordy Carlson&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 27 Apr 2018 16:57:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/MPC8360E-DDR-Calibration/m-p/777669#M2415</guid>
      <dc:creator>gordycarlson320</dc:creator>
      <dc:date>2018-04-27T16:57:08Z</dc:date>
    </item>
    <item>
      <title>Re: MPC8360E DDR Calibration</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/MPC8360E-DDR-Calibration/m-p/777670#M2416</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;An additional question... &lt;SPAN style="font-size: 11.0pt;"&gt;Is there a recommended (or preferred) way to calibrate the DDR?....ie.. – automatic hardware calibration of the DDR impedance, or manual software calibration of the DDR impedance?&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 Apr 2018 19:52:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/MPC8360E-DDR-Calibration/m-p/777670#M2416</guid>
      <dc:creator>gordycarlson320</dc:creator>
      <dc:date>2018-04-30T19:52:38Z</dc:date>
    </item>
    <item>
      <title>Re: MPC8360E DDR Calibration</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/MPC8360E-DDR-Calibration/m-p/777671#M2417</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;1. It is up to the user. Automatic calibration was specially implemented to get the process faster/easier. SW override allows to set different output impedance values, e.g. to use fine tuning for your particular DDR system. Automatic calibration always sets value close to 18 Ohm.&lt;BR /&gt;2. DDRCDR is 0x730400001 at reset. Can be found, for example, in table 5-33.&lt;BR /&gt;3. DDRDSR always shows current impedance, for example after automatic calibration.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Bulat&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 May 2018 06:15:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/MPC8360E-DDR-Calibration/m-p/777671#M2417</guid>
      <dc:creator>Bulat</dc:creator>
      <dc:date>2018-05-03T06:15:02Z</dc:date>
    </item>
  </channel>
</rss>