<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>PowerQUICC Processors中的主题 Enabling MPC8360 ENET3 interface</title>
    <link>https://community.nxp.com/t5/PowerQUICC-Processors/Enabling-MPC8360-ENET3-interface/m-p/745927#M2320</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We have designed a board based on MPC8360. In this board, we are using four Ethernets: ENET1, ENET2, ENET3 and ENET6. ENET1 and ENET2 are configured for GIG interface while ENET3 and ENET6 are used for 100Mbps (Fast Ethernet mode) using RMII interface. The PHY being used on the ENET3 interface is KSZ8031RNL from Micrel. The Gig interfaces are up using the dtb attached. How do we enable ENET3 and ENET6 in 100Mbps? I modified the dtb for ENET3 alone but it was not coming up!!!!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 18 Apr 2018 11:02:34 GMT</pubDate>
    <dc:creator>kirankumartanka</dc:creator>
    <dc:date>2018-04-18T11:02:34Z</dc:date>
    <item>
      <title>Enabling MPC8360 ENET3 interface</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/Enabling-MPC8360-ENET3-interface/m-p/745927#M2320</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We have designed a board based on MPC8360. In this board, we are using four Ethernets: ENET1, ENET2, ENET3 and ENET6. ENET1 and ENET2 are configured for GIG interface while ENET3 and ENET6 are used for 100Mbps (Fast Ethernet mode) using RMII interface. The PHY being used on the ENET3 interface is KSZ8031RNL from Micrel. The Gig interfaces are up using the dtb attached. How do we enable ENET3 and ENET6 in 100Mbps? I modified the dtb for ENET3 alone but it was not coming up!!!!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Apr 2018 11:02:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/Enabling-MPC8360-ENET3-interface/m-p/745927#M2320</guid>
      <dc:creator>kirankumartanka</dc:creator>
      <dc:date>2018-04-18T11:02:34Z</dc:date>
    </item>
    <item>
      <title>Re: Enabling MPC8360 ENET3 interface</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/Enabling-MPC8360-ENET3-interface/m-p/745928#M2321</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;Try to see if it is software issue or hardware issue is to configure the loopback mode by setting GUMR[DIAG] = 01. If the lookback works, then issue is with hardware: pin configuration error, clock, PHY,&amp;nbsp; or signal problem; if the loopback fails, it is with software configuration problem.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Pavel Chubakov&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Apr 2018 03:53:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/Enabling-MPC8360-ENET3-interface/m-p/745928#M2321</guid>
      <dc:creator>Pavel</dc:creator>
      <dc:date>2018-04-24T03:53:55Z</dc:date>
    </item>
  </channel>
</rss>