<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>PowerQUICC ProcessorsのトピックT4240 LINUX RAID0</title>
    <link>https://community.nxp.com/t5/PowerQUICC-Processors/T4240-LINUX-RAID0/m-p/700712#M2196</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;On the T4240QDS, using two Samsung NVMe SSD 960 PRO to form RAID0, but the write rate is only 1.1GB / s, the official data single disk 2GB / s write speed. PCIE configuration: 4X 5G. I need to modify which LINUX configuration.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 17 Aug 2017 03:20:16 GMT</pubDate>
    <dc:creator>silecy2016</dc:creator>
    <dc:date>2017-08-17T03:20:16Z</dc:date>
    <item>
      <title>T4240 LINUX RAID0</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/T4240-LINUX-RAID0/m-p/700712#M2196</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;On the T4240QDS, using two Samsung NVMe SSD 960 PRO to form RAID0, but the write rate is only 1.1GB / s, the official data single disk 2GB / s write speed. PCIE configuration: 4X 5G. I need to modify which LINUX configuration.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 17 Aug 2017 03:20:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/T4240-LINUX-RAID0/m-p/700712#M2196</guid>
      <dc:creator>silecy2016</dc:creator>
      <dc:date>2017-08-17T03:20:16Z</dc:date>
    </item>
  </channel>
</rss>