<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic power on configuration values latching problem in mpc885 in PowerQUICC Processors</title>
    <link>https://community.nxp.com/t5/PowerQUICC-Processors/power-on-configuration-values-latching-problem-in-mpc885/m-p/684561#M2132</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;At power on ebdf&amp;nbsp; and others are not updating . clk out is 18.75MHz instead of 37.5MHz. Modck is 11 at power on reset. If we see in debug mode PLPRCR ( EBDF) is 00 only instead of 01. Data bus(0:15) transitions are&amp;nbsp; as per configuration set values&amp;nbsp; with respect to Hard reset, but not latching into the processor. PLL is locking to 18.75MHz/75mhz. Please clarify. Once in a while it is locking to 37.5mhz and immediately&amp;nbsp; to 18.75mhz.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 13 Jun 2017 08:16:57 GMT</pubDate>
    <dc:creator>Pamid</dc:creator>
    <dc:date>2017-06-13T08:16:57Z</dc:date>
    <item>
      <title>power on configuration values latching problem in mpc885</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/power-on-configuration-values-latching-problem-in-mpc885/m-p/684561#M2132</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;At power on ebdf&amp;nbsp; and others are not updating . clk out is 18.75MHz instead of 37.5MHz. Modck is 11 at power on reset. If we see in debug mode PLPRCR ( EBDF) is 00 only instead of 01. Data bus(0:15) transitions are&amp;nbsp; as per configuration set values&amp;nbsp; with respect to Hard reset, but not latching into the processor. PLL is locking to 18.75MHz/75mhz. Please clarify. Once in a while it is locking to 37.5mhz and immediately&amp;nbsp; to 18.75mhz.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Jun 2017 08:16:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/power-on-configuration-values-latching-problem-in-mpc885/m-p/684561#M2132</guid>
      <dc:creator>Pamid</dc:creator>
      <dc:date>2017-06-13T08:16:57Z</dc:date>
    </item>
    <item>
      <title>Re: power on configuration values latching problem in mpc885</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/power-on-configuration-values-latching-problem-in-mpc885/m-p/684562#M2133</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please connect TRST pin to ground directly or via strong (1K or less) resistor and check again.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Alexander&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Jun 2017 12:17:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/power-on-configuration-values-latching-problem-in-mpc885/m-p/684562#M2133</guid>
      <dc:creator>alexander_yakov</dc:creator>
      <dc:date>2017-06-13T12:17:02Z</dc:date>
    </item>
    <item>
      <title>Re: power on configuration values latching problem in mpc885</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/power-on-configuration-values-latching-problem-in-mpc885/m-p/684563#M2134</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;trst is pulled down to 1kohm. also tried by connecting gnd to trst. Problem remains same. If i see hard reset config values in view registes by connecting tab. It is showing wrong values.SIUMCR it is showing all zeroes. If&amp;nbsp; i activate the debug by&amp;nbsp; connect. hardreset should not generate .But it is giving hard reset also. If i load the configuration file it is not giving hardreset.&amp;nbsp; i am able to run the code in debug mode.why hardreset is coming in debug connect case,though it is accessing internal register.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 Jun 2017 12:25:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/power-on-configuration-values-latching-problem-in-mpc885/m-p/684563#M2134</guid>
      <dc:creator>Pamid</dc:creator>
      <dc:date>2017-06-15T12:25:22Z</dc:date>
    </item>
  </channel>
</rss>