<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: T4240 thermal diode in PowerQUICC Processors</title>
    <link>https://community.nxp.com/t5/PowerQUICC-Processors/T4240-thermal-diode/m-p/672621#M2097</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;There are two thermal diodes located at different locations on the die. One that is close to core clusters and the other one is more close to platform logic, thus each diodes has two pins the cathode and the anode, you need to use the cathode and anode to measure temperature for each site/diode. Some times there are difference in temperature between different sites on die, the difference can be large, up to 20C in extreme cases and thus it is wise to do measurement on both available sites.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Alexander&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 09 May 2017 15:48:00 GMT</pubDate>
    <dc:creator>alexander_yakov</dc:creator>
    <dc:date>2017-05-09T15:48:00Z</dc:date>
    <item>
      <title>T4240 thermal diode</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/T4240-thermal-diode/m-p/672620#M2096</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I find the T4240 has&amp;nbsp;have two on-die&amp;nbsp;diodes,but I cant find&amp;nbsp;Their differences.&lt;/P&gt;&lt;P&gt;in datasheet only introduce which pin is&amp;nbsp;thermal diodes&lt;/P&gt;&lt;P&gt;I want to know which issue I need use&amp;nbsp;two diode&lt;/P&gt;&lt;P&gt;and which issue i only use&amp;nbsp;one diode&amp;nbsp;&lt;/P&gt;&lt;P&gt;thank you&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 May 2017 10:06:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/T4240-thermal-diode/m-p/672620#M2096</guid>
      <dc:creator>jeffcao</dc:creator>
      <dc:date>2017-05-09T10:06:50Z</dc:date>
    </item>
    <item>
      <title>Re: T4240 thermal diode</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/T4240-thermal-diode/m-p/672621#M2097</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;There are two thermal diodes located at different locations on the die. One that is close to core clusters and the other one is more close to platform logic, thus each diodes has two pins the cathode and the anode, you need to use the cathode and anode to measure temperature for each site/diode. Some times there are difference in temperature between different sites on die, the difference can be large, up to 20C in extreme cases and thus it is wise to do measurement on both available sites.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Alexander&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 May 2017 15:48:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/T4240-thermal-diode/m-p/672621#M2097</guid>
      <dc:creator>alexander_yakov</dc:creator>
      <dc:date>2017-05-09T15:48:00Z</dc:date>
    </item>
  </channel>
</rss>