<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>PowerQUICC ProcessorsのトピックRe: MPC8379 Sata driver problems</title>
    <link>https://community.nxp.com/t5/PowerQUICC-Processors/MPC8379-Sata-driver-problems/m-p/630604#M1805</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The RX FIFO size is fixed - it's just a watermark adjustment.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 07 Nov 2016 14:40:42 GMT</pubDate>
    <dc:creator>ufedor</dc:creator>
    <dc:date>2016-11-07T14:40:42Z</dc:date>
    <item>
      <title>MPC8379 Sata driver problems</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/MPC8379-Sata-driver-problems/m-p/630601#M1802</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I've developed a NVR using the MPC8379. We are using the four Sata interfaces to connect 4 Hard Disks. However I'm experiencing communication errors while reading high rates of information of those disks (For example while rebuilding a RAID)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The registers I've programmed are the following:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Serdes:&lt;UL&gt;&lt;LI&gt;CPU_SRDS_RESTCTL --&amp;gt; 0x00444500&lt;/LI&gt;&lt;LI&gt;CPU_SRDS_RESTCTL --&amp;gt; 0x0000000F&lt;/LI&gt;&lt;LI&gt;CPU_SRDS_RESTCTL --&amp;gt; 0x00444500&lt;/LI&gt;&lt;LI&gt;CPU_SRDS_CR1 --&amp;gt; 0x00000000&lt;/LI&gt;&lt;LI&gt;CPU_SRDS_CR2 --&amp;gt; 0x00001414&lt;/LI&gt;&lt;LI&gt;CPU_SRDS_CR3 --&amp;gt; 0x15150505&lt;/LI&gt;&lt;LI&gt;CPU_SRDS_CR4 --&amp;gt; 0x00000808&lt;/LI&gt;&lt;LI&gt;CPU_SRDS_RESTCTL --&amp;gt; 0x80000000&lt;/LI&gt;&lt;/UL&gt;&lt;/LI&gt;&lt;LI&gt;SATA&lt;UL&gt;&lt;LI&gt;&lt;P&gt;CPU_SATA_H_STATUS --&amp;gt; 0xFFFFFFFF&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;CPU_SATA_H_CONTROL --&amp;gt; 0&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;CPU_SATA_S_ERROR --&amp;gt; 0xFFFFFFFF&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;CPU_SATA_CHBA --&amp;gt; 0x88AB102&amp;nbsp;&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;CPU_SATA_S_CONTROL --&amp;gt; 0x10030000&lt;/LI&gt;&lt;LI&gt;CPU_SATA_H_CONTROL --&amp;gt; 0x3F050080&lt;/LI&gt;&lt;/UL&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I program the 2 SerDes and the 4 SATA interfaces with the same registers. While rebuilding one drive from another I suddenly get an error in a Read communication, where&amp;nbsp;CPU_SATA_H_STATUS has the following value: 0x230100A0.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have no clue in what am I doing wrong. In normal writing and reading from the Hard drives I'm not experiencing any problem, only while rebuilding systems.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Nov 2016 16:46:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/MPC8379-Sata-driver-problems/m-p/630601#M1802</guid>
      <dc:creator>carlessilva</dc:creator>
      <dc:date>2016-11-03T16:46:59Z</dc:date>
    </item>
    <item>
      <title>Re: MPC8379 Sata driver problems</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/MPC8379-Sata-driver-problems/m-p/630602#M1803</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please check whether the TransCfg[RX_WATER_MARK] value is 0x16.&lt;/P&gt;&lt;P&gt;If "yes", can you please change it to 0x10 ant re-test.&lt;/P&gt;&lt;P&gt;Here is the location to modify the SATA watermarker level in U-Boot (./drivers/fsl_sata.c):&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;out_le32(&amp;amp;reg&amp;gt;transcfg, 0x08000016);&lt;/P&gt;&lt;P&gt;It should be:&lt;/P&gt;&lt;P&gt;out_le32(&amp;amp;reg-&amp;gt;transcfg, 0x08000010);&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 Nov 2016 12:06:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/MPC8379-Sata-driver-problems/m-p/630602#M1803</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2016-11-04T12:06:29Z</dc:date>
    </item>
    <item>
      <title>Re: MPC8379 Sata driver problems</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/MPC8379-Sata-driver-problems/m-p/630603#M1804</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for your answer. It looks like it works, but won't it make it slower if you reduce the rxFifo?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 07 Nov 2016 14:23:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/MPC8379-Sata-driver-problems/m-p/630603#M1804</guid>
      <dc:creator>carlessilva</dc:creator>
      <dc:date>2016-11-07T14:23:18Z</dc:date>
    </item>
    <item>
      <title>Re: MPC8379 Sata driver problems</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/MPC8379-Sata-driver-problems/m-p/630604#M1805</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The RX FIFO size is fixed - it's just a watermark adjustment.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 07 Nov 2016 14:40:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/MPC8379-Sata-driver-problems/m-p/630604#M1805</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2016-11-07T14:40:42Z</dc:date>
    </item>
  </channel>
</rss>