<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>PowerQUICC ProcessorsのトピックReprogramming DDR controller on PowerQUICC III</title>
    <link>https://community.nxp.com/t5/PowerQUICC-Processors/Reprogramming-DDR-controller-on-PowerQUICC-III/m-p/212604#M179</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is it possible to reprogram the DDR controller on PowerQUICC III more than once after power-up?&amp;nbsp; Our system uses two bootROM (once factory installed, one field-upgradable) and the DDR is programmed in both (not necessarily with the same settings).&amp;nbsp; Is there a different program sequence needed the second time though?&amp;nbsp; Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 14 Jul 2010 02:08:36 GMT</pubDate>
    <dc:creator>ConfusedInOR</dc:creator>
    <dc:date>2010-07-14T02:08:36Z</dc:date>
    <item>
      <title>Reprogramming DDR controller on PowerQUICC III</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/Reprogramming-DDR-controller-on-PowerQUICC-III/m-p/212604#M179</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is it possible to reprogram the DDR controller on PowerQUICC III more than once after power-up?&amp;nbsp; Our system uses two bootROM (once factory installed, one field-upgradable) and the DDR is programmed in both (not necessarily with the same settings).&amp;nbsp; Is there a different program sequence needed the second time though?&amp;nbsp; Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Jul 2010 02:08:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/Reprogramming-DDR-controller-on-PowerQUICC-III/m-p/212604#M179</guid>
      <dc:creator>ConfusedInOR</dc:creator>
      <dc:date>2010-07-14T02:08:36Z</dc:date>
    </item>
  </channel>
</rss>