<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>PowerQUICC ProcessorsのトピックMPC8323E with SD/MMC Card</title>
    <link>https://community.nxp.com/t5/PowerQUICC-Processors/MPC8323E-with-SD-MMC-Card/m-p/209841#M175</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi.&lt;BR /&gt;&lt;BR /&gt;I am doing a project where I need to access the SD card.&lt;BR /&gt;I'm using the development kit for Freescale MPC8323E PowerQUICC processor with kernel-2.6.20.&lt;BR /&gt;&lt;BR /&gt;When I compile the kernel, in device driver I select the option to have support for SD / MMC Card.&lt;BR /&gt;When I look at dmesg | grep sd, he brings me the following:&lt;BR /&gt;&lt;BR /&gt;sdhci: Secure Digital Host Controller Interface driver, 0.12&lt;BR /&gt;wbsd: winbond W83L51xd SD / MMC card interface driver, 1.6&lt;BR /&gt;&lt;BR /&gt;But when I stick the SD card, there was no message and I can not mounter hardware, because it has no option in the /dev&lt;BR /&gt;&lt;BR /&gt;The procedure that I am doing is correct or am I missing something essential?&lt;BR /&gt;The Kernell 2.6.20 has support for reading and writing to SD card correct? I need to write documents in it (file.sh)&lt;BR /&gt;&lt;BR /&gt;graciously&lt;BR /&gt;lucas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 30 Jun 2010 02:57:41 GMT</pubDate>
    <dc:creator>lasfclestat</dc:creator>
    <dc:date>2010-06-30T02:57:41Z</dc:date>
    <item>
      <title>MPC8323E with SD/MMC Card</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/MPC8323E-with-SD-MMC-Card/m-p/209841#M175</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi.&lt;BR /&gt;&lt;BR /&gt;I am doing a project where I need to access the SD card.&lt;BR /&gt;I'm using the development kit for Freescale MPC8323E PowerQUICC processor with kernel-2.6.20.&lt;BR /&gt;&lt;BR /&gt;When I compile the kernel, in device driver I select the option to have support for SD / MMC Card.&lt;BR /&gt;When I look at dmesg | grep sd, he brings me the following:&lt;BR /&gt;&lt;BR /&gt;sdhci: Secure Digital Host Controller Interface driver, 0.12&lt;BR /&gt;wbsd: winbond W83L51xd SD / MMC card interface driver, 1.6&lt;BR /&gt;&lt;BR /&gt;But when I stick the SD card, there was no message and I can not mounter hardware, because it has no option in the /dev&lt;BR /&gt;&lt;BR /&gt;The procedure that I am doing is correct or am I missing something essential?&lt;BR /&gt;The Kernell 2.6.20 has support for reading and writing to SD card correct? I need to write documents in it (file.sh)&lt;BR /&gt;&lt;BR /&gt;graciously&lt;BR /&gt;lucas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 Jun 2010 02:57:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/MPC8323E-with-SD-MMC-Card/m-p/209841#M175</guid>
      <dc:creator>lasfclestat</dc:creator>
      <dc:date>2010-06-30T02:57:41Z</dc:date>
    </item>
    <item>
      <title>Re: MPC8323E with SD/MMC Card</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/MPC8323E-with-SD-MMC-Card/m-p/209842#M176</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am trying to use microSD on my ADS5121.&lt;/P&gt;&lt;P&gt;I had your problem, I had to uncomment SD config in .dts file and comment PATA (they share pins).&lt;/P&gt;&lt;P&gt;Now, I had others problems &lt;IMG alt=":smileysad:" class="emoticon emoticon-smileysad" id="smileysad" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-sad.gif" title="Smiley Sad" /&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I hope it helps.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 Aug 2010 16:51:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/MPC8323E-with-SD-MMC-Card/m-p/209842#M176</guid>
      <dc:creator>moi</dc:creator>
      <dc:date>2010-08-05T16:51:46Z</dc:date>
    </item>
  </channel>
</rss>