<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: How to access UART2 on MPC8323E-RDB in PowerQUICC Processors</title>
    <link>https://community.nxp.com/t5/PowerQUICC-Processors/How-to-access-UART2-on-MPC8323E-RDB/m-p/609246#M1696</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;According to board schematic, I see only one UART is routed out, for UART2 I do not see standard DB-9 connector.&lt;/P&gt;&lt;P&gt;I see only several signals UART2_* internally routed to header for internal use, but these signals have TTL levels, and can not be used as UART without TTL to RS-232 converter type MAX3232 or similar.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Alexander&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 02 Mar 2017 05:59:25 GMT</pubDate>
    <dc:creator>alexander_yakov</dc:creator>
    <dc:date>2017-03-02T05:59:25Z</dc:date>
    <item>
      <title>How to access UART2 on MPC8323E-RDB</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/How-to-access-UART2-on-MPC8323E-RDB/m-p/609245#M1695</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; I am working on MPC8323E-RDB Board and I am using Linux2.6.20.6-rt8. I am trying to access UART2 on board. But I am not able to recognize which device is available for UART2. Is there any way to print data on UART2 directly by using device or can I create device for it?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;I am using LTIB for cross compilation. Is LTIB will support for device creation and mapping?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;V JYOTHI.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Mar 2017 10:43:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/How-to-access-UART2-on-MPC8323E-RDB/m-p/609245#M1695</guid>
      <dc:creator>vadrevujyothi</dc:creator>
      <dc:date>2017-03-01T10:43:53Z</dc:date>
    </item>
    <item>
      <title>Re: How to access UART2 on MPC8323E-RDB</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/How-to-access-UART2-on-MPC8323E-RDB/m-p/609246#M1696</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;According to board schematic, I see only one UART is routed out, for UART2 I do not see standard DB-9 connector.&lt;/P&gt;&lt;P&gt;I see only several signals UART2_* internally routed to header for internal use, but these signals have TTL levels, and can not be used as UART without TTL to RS-232 converter type MAX3232 or similar.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Alexander&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Mar 2017 05:59:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/How-to-access-UART2-on-MPC8323E-RDB/m-p/609246#M1696</guid>
      <dc:creator>alexander_yakov</dc:creator>
      <dc:date>2017-03-02T05:59:25Z</dc:date>
    </item>
  </channel>
</rss>