<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>PowerQUICC ProcessorsのトピックRe: Need suggestions on MPC8377 reset problem.</title>
    <link>https://community.nxp.com/t5/PowerQUICC-Processors/Need-suggestions-on-MPC8377-reset-problem/m-p/198996#M162</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;This problem was resolved.&amp;nbsp; I test pin was being held at an improper level during device reset, so it was going into a test mode.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 27 Sep 2012 16:31:01 GMT</pubDate>
    <dc:creator>mvonahnen</dc:creator>
    <dc:date>2012-09-27T16:31:01Z</dc:date>
    <item>
      <title>Need suggestions on MPC8377 reset problem.</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/Need-suggestions-on-MPC8377-reset-problem/m-p/198994#M160</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a failed board (others of the same design are working).&amp;nbsp; The symptoms are that the MPC8377 comes out of reset, attempts to read the configuration words, but the DDR clocks are never turned on.&amp;nbsp; After about 6 seconds, the /HRESET line goes low and the process repeats, continually.&amp;nbsp; When we tried to connect via the emulator, we were unable to load the DDR memory, it was not configured even with Code Warrior.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;At one time, the board was operational, booting U-Boot and running LINUX.&amp;nbsp; Any suggestions of what to look at?&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Jul 2009 20:00:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/Need-suggestions-on-MPC8377-reset-problem/m-p/198994#M160</guid>
      <dc:creator>mvonahnen</dc:creator>
      <dc:date>2009-07-14T20:00:52Z</dc:date>
    </item>
    <item>
      <title>Re: Need suggestions on MPC8377 reset problem.</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/Need-suggestions-on-MPC8377-reset-problem/m-p/198995#M161</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Are you sure? May be it is floating bug...&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Aug 2009 14:48:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/Need-suggestions-on-MPC8377-reset-problem/m-p/198995#M161</guid>
      <dc:creator>gleb_itech</dc:creator>
      <dc:date>2009-08-06T14:48:01Z</dc:date>
    </item>
    <item>
      <title>Re: Need suggestions on MPC8377 reset problem.</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/Need-suggestions-on-MPC8377-reset-problem/m-p/198996#M162</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;This problem was resolved.&amp;nbsp; I test pin was being held at an improper level during device reset, so it was going into a test mode.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Sep 2012 16:31:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/Need-suggestions-on-MPC8377-reset-problem/m-p/198996#M162</guid>
      <dc:creator>mvonahnen</dc:creator>
      <dc:date>2012-09-27T16:31:01Z</dc:date>
    </item>
  </channel>
</rss>