<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: tcp ip stack in PowerQUICC Processors</title>
    <link>https://community.nxp.com/t5/PowerQUICC-Processors/tcp-ip-stack/m-p/528493#M1533</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I do not think this is "not possible" to port standalone tcp/ip stack to MPC8309 processor, however this is usually used for microcontrollers. As long as mpc8309 is not a "microcontroller", but processor from networking product segment, it is recommended to use it with Linux or other OS.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Alexander&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 31 Aug 2016 10:46:19 GMT</pubDate>
    <dc:creator>alexander_yakov</dc:creator>
    <dc:date>2016-08-31T10:46:19Z</dc:date>
    <item>
      <title>tcp ip stack</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/tcp-ip-stack/m-p/528492#M1532</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Like to port tcp ip stack into powerquicc mpc8309 processor without OS. Is it possible? If yes please suggest&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Aug 2016 04:14:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/tcp-ip-stack/m-p/528492#M1532</guid>
      <dc:creator>garimella</dc:creator>
      <dc:date>2016-08-16T04:14:14Z</dc:date>
    </item>
    <item>
      <title>Re: tcp ip stack</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/tcp-ip-stack/m-p/528493#M1533</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I do not think this is "not possible" to port standalone tcp/ip stack to MPC8309 processor, however this is usually used for microcontrollers. As long as mpc8309 is not a "microcontroller", but processor from networking product segment, it is recommended to use it with Linux or other OS.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Alexander&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 31 Aug 2016 10:46:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/tcp-ip-stack/m-p/528493#M1533</guid>
      <dc:creator>alexander_yakov</dc:creator>
      <dc:date>2016-08-31T10:46:19Z</dc:date>
    </item>
  </channel>
</rss>