<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: NAND bitflip correction on 8314 in PowerQUICC Processors</title>
    <link>https://community.nxp.com/t5/PowerQUICC-Processors/NAND-bitflip-correction-on-8314/m-p/495169#M1428</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;NXP confirmed the 8314 does not have the register.&amp;nbsp; The double-read method works but is slow as expected.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jeff&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 14 Apr 2016 19:46:37 GMT</pubDate>
    <dc:creator>jefftharris</dc:creator>
    <dc:date>2016-04-14T19:46:37Z</dc:date>
    <item>
      <title>NAND bitflip correction on 8314</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/NAND-bitflip-correction-on-8314/m-p/495167#M1426</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Does the NAND controller on the 8314 CPU provide notification for an ECC-corrected bitflip error?&amp;nbsp; The 8313 CPU contains the LTECCR register.&amp;nbsp; Does the 8314 support this register as well?&amp;nbsp; If not, is there another method to detect the condition so the Linux UBI driver can scrub the block before an unrecoverable error occurs?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 29 Feb 2016 15:50:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/NAND-bitflip-correction-on-8314/m-p/495167#M1426</guid>
      <dc:creator>jefftharris</dc:creator>
      <dc:date>2016-02-29T15:50:21Z</dc:date>
    </item>
    <item>
      <title>Re: NAND bitflip correction on 8314</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/NAND-bitflip-correction-on-8314/m-p/495168#M1427</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes there are MPC83xx eLBC which do not have LTECCR register. According to MPC8314 documentation there is not LTECCR. The Freescale Enhanced Local Bus Controller NAND driver (fsl_elbc_nand.c) says that "if the ELBC doesn't have the lteccr register it reads 0".So it read it always &lt;/P&gt;&lt;PRE class="jive-pre"&gt;if (lteccr &amp;amp; 0x000F0000) {&lt;/PRE&gt;&lt;PRE class="jive-pre"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;A href="http://lxr.free-electrons.com/ident?i=mtd" rel="nofollow noopener noreferrer" target="_blank"&gt;mtd&lt;/A&gt;-&amp;gt;ecc_stats.corrected++;&lt;/PRE&gt;&lt;PRE class="jive-pre"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; elbc_fcm_ctrl-&amp;gt;max_bitflips = 1;&lt;/PRE&gt;&lt;PRE class="jive-pre"&gt; &lt;/PRE&gt;&lt;P&gt;but without LTECCR ecc_stats.corrected will be not incremented. I do not see another method with hardware support in this case. Of course there is bulky method when we read the same page two times first when ECC correction is enabled and second when it is disabled and then compare. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Mar 2016 09:34:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/NAND-bitflip-correction-on-8314/m-p/495168#M1427</guid>
      <dc:creator>r8070z</dc:creator>
      <dc:date>2016-03-03T09:34:16Z</dc:date>
    </item>
    <item>
      <title>Re: NAND bitflip correction on 8314</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/NAND-bitflip-correction-on-8314/m-p/495169#M1428</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;NXP confirmed the 8314 does not have the register.&amp;nbsp; The double-read method works but is slow as expected.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jeff&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Apr 2016 19:46:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/NAND-bitflip-correction-on-8314/m-p/495169#M1428</guid>
      <dc:creator>jefftharris</dc:creator>
      <dc:date>2016-04-14T19:46:37Z</dc:date>
    </item>
  </channel>
</rss>