<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>PowerQUICC Processors中的主题 Re: PQII/ PQIII Flash Programmer</title>
    <link>https://community.nxp.com/t5/PowerQUICC-Processors/PQII-PQIII-Flash-Programmer/m-p/486896#M1412</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Sorry, we do not offer JTAG/COP interface specification to customers, so you can not implement your own flash programmer for PQ2/PQ3 devices using internal debugging interface of PQ2/PQ3 device.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The only thing I can offer here is implement flash programming via standard JTAG commands, i.e. place PQ2/PQ3 device to JTAG boundary scan mode and program external flash, connected to PQ2/PQ3 device by "bit-banging" on PQ2/PQ3 pins using JTAG boundary scan commands. In this case the processor itself will be in reset mode, so you do not need PQ2/PQ3 debug interface description.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Alexander&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 23 Mar 2016 14:33:11 GMT</pubDate>
    <dc:creator>alexander_yakov</dc:creator>
    <dc:date>2016-03-23T14:33:11Z</dc:date>
    <item>
      <title>PQII/ PQIII Flash Programmer</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/PQII-PQIII-Flash-Programmer/m-p/486895#M1411</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We would like to make a Flash Programmer for PQ2/PQ3 based boards, fully hosted on a SBC (Raspberry Pi, Beagle Board/ etc.). This is to make it easy to for the Lab and Field people to recover boards where Flash has been corrupted.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How do we start about this? Where do we get the supported JTAG / cmd specifications supported by PQ2/3?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 18 Mar 2016 05:49:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/PQII-PQIII-Flash-Programmer/m-p/486895#M1411</guid>
      <dc:creator>dijo</dc:creator>
      <dc:date>2016-03-18T05:49:27Z</dc:date>
    </item>
    <item>
      <title>Re: PQII/ PQIII Flash Programmer</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/PQII-PQIII-Flash-Programmer/m-p/486896#M1412</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Sorry, we do not offer JTAG/COP interface specification to customers, so you can not implement your own flash programmer for PQ2/PQ3 devices using internal debugging interface of PQ2/PQ3 device.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The only thing I can offer here is implement flash programming via standard JTAG commands, i.e. place PQ2/PQ3 device to JTAG boundary scan mode and program external flash, connected to PQ2/PQ3 device by "bit-banging" on PQ2/PQ3 pins using JTAG boundary scan commands. In this case the processor itself will be in reset mode, so you do not need PQ2/PQ3 debug interface description.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Alexander&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 23 Mar 2016 14:33:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/PQII-PQIII-Flash-Programmer/m-p/486896#M1412</guid>
      <dc:creator>alexander_yakov</dc:creator>
      <dc:date>2016-03-23T14:33:11Z</dc:date>
    </item>
  </channel>
</rss>