<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Compatibility between different MPC8309 core frequency in PowerQUICC Processors</title>
    <link>https://community.nxp.com/t5/PowerQUICC-Processors/Compatibility-between-different-MPC8309-core-frequency/m-p/459406#M1297</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, they are 10% compatible. If you just replace 266 Mhz part by 400 Mhz part in 266 Mhz design, it will work at 266 Mhz without any changes required.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Alexander&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 30 May 2016 15:50:11 GMT</pubDate>
    <dc:creator>alexander_yakov</dc:creator>
    <dc:date>2016-05-30T15:50:11Z</dc:date>
    <item>
      <title>Compatibility between different MPC8309 core frequency</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/Compatibility-between-different-MPC8309-core-frequency/m-p/459405#M1296</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I would like to know if part MPC8309CVMAGDCA (which runs at 400MHz) is 100% compatible with the MPC8309VMADDCA (which runs at 266MHz)? By compatible I mean if I just replace the 266MHz one by the 400MHz all functionalities will be the same, or it is needed to change any component around it (crystal and so on).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 May 2016 14:30:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/Compatibility-between-different-MPC8309-core-frequency/m-p/459405#M1296</guid>
      <dc:creator>brunoschmitt</dc:creator>
      <dc:date>2016-05-30T14:30:43Z</dc:date>
    </item>
    <item>
      <title>Re: Compatibility between different MPC8309 core frequency</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/Compatibility-between-different-MPC8309-core-frequency/m-p/459406#M1297</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, they are 10% compatible. If you just replace 266 Mhz part by 400 Mhz part in 266 Mhz design, it will work at 266 Mhz without any changes required.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Alexander&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 May 2016 15:50:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/Compatibility-between-different-MPC8309-core-frequency/m-p/459406#M1297</guid>
      <dc:creator>alexander_yakov</dc:creator>
      <dc:date>2016-05-30T15:50:11Z</dc:date>
    </item>
  </channel>
</rss>