<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Maximum 8349 processor frequency for temperature range -40°C ... +105°C in PowerQUICC Processors</title>
    <link>https://community.nxp.com/t5/PowerQUICC-Processors/Maximum-8349-processor-frequency-for-temperature-range-40-C-105/m-p/450564#M1263</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for the answer.&lt;/P&gt;&lt;P&gt;Do you know if there is a version of the 8349 (or a compatible processor) that works at higher frequency in the extended temperature range?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 20 May 2015 16:38:13 GMT</pubDate>
    <dc:creator>danielefranco</dc:creator>
    <dc:date>2015-05-20T16:38:13Z</dc:date>
    <item>
      <title>Maximum 8349 processor frequency for temperature range -40°C ... +105°C</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/Maximum-8349-processor-frequency-for-temperature-range-40-C-105/m-p/450562#M1261</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Quote from:&lt;/P&gt;&lt;P data-canvas-width="339.1605" style="font-size: 15px; font-family: sans-serif;"&gt;"MPC8349EA PowerQUICC II Pro Integrated Host Processor Hardware Specifications, Rev. 13"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;"For temperature range = C, processor frequency is limited to&amp;nbsp; &lt;/EM&gt;&lt;/P&gt;&lt;P data-canvas-width="408.4439999999998" style="font-size: 15px; font-family: sans-serif;"&gt;&lt;EM&gt;with a platform frequency of 266 and up to 533 with a platform &lt;/EM&gt;&lt;/P&gt;&lt;P data-canvas-width="111.55950000000001" style="font-size: 15px; font-family: sans-serif;"&gt;&lt;EM&gt;frequency of 333"&lt;/EM&gt;&lt;/P&gt;&lt;P data-canvas-width="111.55950000000001" style="font-size: 15px; font-family: sans-serif;"&gt;&lt;/P&gt;&lt;P data-canvas-width="111.55950000000001" style="font-size: 15px; font-family: sans-serif;"&gt;It seems that there is a type in the statement above. Which is the maximum processor frequency for the temperature range "C" (i.e. -40...+105)?&lt;/P&gt;&lt;P data-canvas-width="111.55950000000001" style="font-size: 15px; font-family: sans-serif;"&gt;With a platform frequency of 333Mhz it is clear to be 533Mhz, but with a platform frequency of 266?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 May 2015 10:32:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/Maximum-8349-processor-frequency-for-temperature-range-40-C-105/m-p/450562#M1261</guid>
      <dc:creator>danielefranco</dc:creator>
      <dc:date>2015-05-20T10:32:37Z</dc:date>
    </item>
    <item>
      <title>Re: Maximum 8349 processor frequency for temperature range -40°C ... +105°C</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/Maximum-8349-processor-frequency-for-temperature-range-40-C-105/m-p/450563#M1262</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Actually for all 834x family (MPC8343, MPC8347 and MPC8349) this note says&lt;/P&gt;&lt;P&gt;For temperature range = C, processor frequency is limited to 400 (PBGA) with a platform frequency of 266 and up to 533 (TBGA) with a platform frequency of 333&lt;/P&gt;&lt;P&gt;Because MPC8349 is TBGA only they change it in way you have read in the MPC8349 hardware specs. For the MPC8343 they correspondingly change it to &lt;/P&gt;&lt;P&gt;“For temperature range = C, processor frequency is limited to 400 with a platform frequency of 266 and up to with a platform frequency of 333”&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 May 2015 14:11:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/Maximum-8349-processor-frequency-for-temperature-range-40-C-105/m-p/450563#M1262</guid>
      <dc:creator>r8070z</dc:creator>
      <dc:date>2015-05-20T14:11:27Z</dc:date>
    </item>
    <item>
      <title>Re: Maximum 8349 processor frequency for temperature range -40°C ... +105°C</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/Maximum-8349-processor-frequency-for-temperature-range-40-C-105/m-p/450564#M1263</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for the answer.&lt;/P&gt;&lt;P&gt;Do you know if there is a version of the 8349 (or a compatible processor) that works at higher frequency in the extended temperature range?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 May 2015 16:38:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/Maximum-8349-processor-frequency-for-temperature-range-40-C-105/m-p/450564#M1263</guid>
      <dc:creator>danielefranco</dc:creator>
      <dc:date>2015-05-20T16:38:13Z</dc:date>
    </item>
  </channel>
</rss>