<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: ltib networking problem in PowerQUICC Processors</title>
    <link>https://community.nxp.com/t5/PowerQUICC-Processors/ltib-networking-problem/m-p/440583#M1219</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;1. Which board you are using? Please specify board name or exact partnumber&lt;/P&gt;&lt;P&gt;2. Which BSP you are using? Please specify BSP file name and where it was downloaded&lt;/P&gt;&lt;P&gt;3. What happens if you burn pre-built binary image, which is typically supplied in BSP?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 21 Aug 2015 05:22:25 GMT</pubDate>
    <dc:creator>alexander_yakov</dc:creator>
    <dc:date>2015-08-21T05:22:25Z</dc:date>
    <item>
      <title>ltib networking problem</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/ltib-networking-problem/m-p/440582#M1218</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi&lt;/P&gt;&lt;P&gt;i have an mpc8568 eval board and i configured a linux kernel for it with ltib.&lt;/P&gt;&lt;P&gt;i tested several configurations in ltib but in no one i recieved a working networking system (the device couldn't ping anything on the network and doesn't have /etc/interfaces or ...)&lt;/P&gt;&lt;P&gt;i tried changing ip address manually, adding dhcp support and trying several setting in the linux but the result not changed so i used wireshark to catch output packets and there was some output but no arp or dhcp packets and in fact no ip packets.&lt;/P&gt;&lt;P&gt;plz help me&lt;/P&gt;&lt;P&gt;thanks&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;mohammad&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 15 Aug 2015 13:10:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/ltib-networking-problem/m-p/440582#M1218</guid>
      <dc:creator>ssssss</dc:creator>
      <dc:date>2015-08-15T13:10:42Z</dc:date>
    </item>
    <item>
      <title>Re: ltib networking problem</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/ltib-networking-problem/m-p/440583#M1219</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;1. Which board you are using? Please specify board name or exact partnumber&lt;/P&gt;&lt;P&gt;2. Which BSP you are using? Please specify BSP file name and where it was downloaded&lt;/P&gt;&lt;P&gt;3. What happens if you burn pre-built binary image, which is typically supplied in BSP?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Aug 2015 05:22:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/ltib-networking-problem/m-p/440583#M1219</guid>
      <dc:creator>alexander_yakov</dc:creator>
      <dc:date>2015-08-21T05:22:25Z</dc:date>
    </item>
  </channel>
</rss>