<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>PowerQUICC Processors中的主题 Re: MPC8260A(Hip4) startup problem?</title>
    <link>https://community.nxp.com/t5/PowerQUICC-Processors/MPC8260A-Hip4-startup-problem/m-p/434665#M1189</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In MPC8260ACE, &lt;/P&gt;&lt;P&gt;G3. PLL does not lock on the rising edge of the input clock CLKIN&lt;/P&gt;&lt;P&gt;In correct operation, the PLL of the MPC826x devices will lock on the rising edge of the input clock.&lt;/P&gt;&lt;P&gt;However, on the MPC826xA (Hip4) silicon, the PLL locks on the falling edge of the input clock if an integer&lt;/P&gt;&lt;P&gt;CPM multiplication factor is used. This will affect the skew between CLKIN and internal clock at the rising&lt;/P&gt;&lt;P&gt;edge since the skew is dependent on the duty cycle of the input clock. This will affect synchronous designs&lt;/P&gt;&lt;P&gt;where the same clock source is used as an input to CLKIN as well as to an external synchronous device (e.g.&lt;/P&gt;&lt;P&gt;a peripheral or ASIC). The MPC826xA internal logic assumes that the internal clocks rising edge will be in&lt;/P&gt;&lt;P&gt;sync with CLKIN.&lt;/P&gt;&lt;P&gt;Workaround: Use a non-integer CPM multiplication factor. This workaround does not apply to PCI agent&lt;/P&gt;&lt;P&gt;mode, since the multiplication factor in PCI agent mode must be an integer.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My clock setting is 200/133/66Mhz, MF =2 ,&amp;nbsp; so the main PLL locks on the falling edge of CLKIN, but the FPGA on my board is a 60x Slave and use the same clock source with CLKIN by a clock buffer(CY2309). Does this affect the CPU startup?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 29 Oct 2015 12:40:52 GMT</pubDate>
    <dc:creator>mengjunling</dc:creator>
    <dc:date>2015-10-29T12:40:52Z</dc:date>
    <item>
      <title>MPC8260A(Hip4) startup problem?</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/MPC8260A-Hip4-startup-problem/m-p/434662#M1186</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P style="font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f;"&gt;Hi:&lt;/P&gt;&lt;P style="font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f;"&gt;Now I buy MPC8260ACZUMHBB chips from RS,&amp;nbsp; and assembly on my board.&lt;/P&gt;&lt;P style="font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f;"&gt;I read the PVR and IMMR, the values indicates Hip4 revision, the package marking (4K25A QQDK1036 MALAYSIA) is identical to PVR/IMMR.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f;"&gt;Now I have a new problem, when I power up my board, the UART(from SMC1) can't output anything, but keep powering on after about several minutes, I reset my board or recycle the power,&lt;/P&gt;&lt;P style="font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f;"&gt;UART can output correctly, I don't know why? &lt;/P&gt;&lt;P style="font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f;"&gt;&lt;/P&gt;&lt;P style="font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f;"&gt;But another board assembled MPC8260(Hip3) device boots correctly everytime, and the only difference between two board is different CPU revisions(one is Hip3, another is Hip4).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f;"&gt;In my design I don't control the power sequence,VDD_Core(1.8V) and VDDH(3.3V) power up at the same time, but the VDD_Core powers quickly,&lt;/P&gt;&lt;P style="font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f;"&gt;In AN2290, I find the following states, I want to know if the power sequence affect the MPC8260 boot and cause my problem?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f;"&gt;&lt;SPAN style="font-weight: inherit; font-family: inherit;"&gt;&lt;EM&gt;2.3 Power Sequencing&lt;/EM&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f;"&gt;&lt;SPAN style="font-weight: inherit; font-family: inherit;"&gt;&lt;EM&gt;One consequence of multiple power supplies is that when power is initially applied the voltage rails ramp&lt;/EM&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f;"&gt;&lt;SPAN style="font-weight: inherit; font-family: inherit;"&gt;&lt;EM&gt;up at different rates. The rates depend on the nature of the power supply, the type of load on each power&lt;/EM&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f;"&gt;&lt;SPAN style="font-weight: inherit; font-family: inherit;"&gt;&lt;EM&gt;supply, and the manner in which different voltages are derived. The following restrictions apply:&lt;/EM&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f;"&gt;&lt;SPAN style="font-weight: inherit; font-family: inherit;"&gt;&lt;EM&gt;• VDD/VCCSYN—Must not exceed VDDH by more than 0.4 V at any time, including during&lt;/EM&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f;"&gt;&lt;SPAN style="font-weight: inherit; font-family: inherit;"&gt;&lt;EM&gt;power-on reset.&lt;/EM&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f;"&gt;&lt;SPAN style="font-weight: inherit; font-family: inherit;"&gt;&lt;EM&gt;• VDDH—Can exceed VDD/VCCSYN by 3.3 V during power on reset by no more than 100 msec.&lt;/EM&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f;"&gt;&lt;SPAN style="font-weight: inherit; font-family: inherit;"&gt;&lt;EM&gt;During normal operation, should not exceed VDD/VCCSYN by more than 2.0 V (HiP3) or 2.5V&lt;/EM&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f;"&gt;&lt;SPAN style="font-weight: inherit; font-family: inherit;"&gt;&lt;EM&gt;(HiP4).&lt;/EM&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f;"&gt;&lt;SPAN style="font-weight: inherit; font-family: inherit;"&gt;&lt;EM&gt;• VIN—Must not exceed VDDH by more than 2.5 V at any time, including during power-on reset.&lt;/EM&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f;"&gt;I&lt;/P&gt;&lt;P style="font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f;"&gt;&lt;SPAN style="font-weight: inherit; font-style: inherit; font-family: inherit;"&gt;On my board, the spare pins U5, V4, and AE11 (on PCI devices, AE11 is CLKIN2) is grouded.&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f;"&gt;&lt;SPAN style="font-weight: inherit; font-style: inherit; font-family: inherit;"&gt;and the AF25(PCI_MODE#) pin is pulled up. XFC pin capacitor is 1200pF.&amp;nbsp; Clocking setting is 200/133/66Mhz(0101_111, Local mode), clock input is 66Mhz&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f;"&gt;&lt;SPAN style="font-weight: inherit; font-style: inherit; font-family: inherit;"&gt;The Local bus interface is not used, so I left it floating, only fewer pins is connected.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Oct 2015 13:48:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/MPC8260A-Hip4-startup-problem/m-p/434662#M1186</guid>
      <dc:creator>mengjunling</dc:creator>
      <dc:date>2015-10-27T13:48:34Z</dc:date>
    </item>
    <item>
      <title>Re: MPC8260A(Hip4) startup problem?</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/MPC8260A-Hip4-startup-problem/m-p/434663#M1187</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Sorry, we need to look your schematic to debug this problem. Please create a Service Request to Freescale Online Technical support and attach your schematic to Service Request.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.freescale.com/webapp/servicerequest.create_SR.framework" title="https://www.freescale.com/webapp/servicerequest.create_SR.framework"&gt;New Service Request&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Alexander&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Oct 2015 02:01:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/MPC8260A-Hip4-startup-problem/m-p/434663#M1187</guid>
      <dc:creator>alexander_yakov</dc:creator>
      <dc:date>2015-10-28T02:01:23Z</dc:date>
    </item>
    <item>
      <title>Re: MPC8260A(Hip4) startup problem?</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/MPC8260A-Hip4-startup-problem/m-p/434664#M1188</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have created a new SR, and attached my schematic for you. Please help me to fix the problem.&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Oct 2015 12:49:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/MPC8260A-Hip4-startup-problem/m-p/434664#M1188</guid>
      <dc:creator>mengjunling</dc:creator>
      <dc:date>2015-10-28T12:49:05Z</dc:date>
    </item>
    <item>
      <title>Re: MPC8260A(Hip4) startup problem?</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/MPC8260A-Hip4-startup-problem/m-p/434665#M1189</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In MPC8260ACE, &lt;/P&gt;&lt;P&gt;G3. PLL does not lock on the rising edge of the input clock CLKIN&lt;/P&gt;&lt;P&gt;In correct operation, the PLL of the MPC826x devices will lock on the rising edge of the input clock.&lt;/P&gt;&lt;P&gt;However, on the MPC826xA (Hip4) silicon, the PLL locks on the falling edge of the input clock if an integer&lt;/P&gt;&lt;P&gt;CPM multiplication factor is used. This will affect the skew between CLKIN and internal clock at the rising&lt;/P&gt;&lt;P&gt;edge since the skew is dependent on the duty cycle of the input clock. This will affect synchronous designs&lt;/P&gt;&lt;P&gt;where the same clock source is used as an input to CLKIN as well as to an external synchronous device (e.g.&lt;/P&gt;&lt;P&gt;a peripheral or ASIC). The MPC826xA internal logic assumes that the internal clocks rising edge will be in&lt;/P&gt;&lt;P&gt;sync with CLKIN.&lt;/P&gt;&lt;P&gt;Workaround: Use a non-integer CPM multiplication factor. This workaround does not apply to PCI agent&lt;/P&gt;&lt;P&gt;mode, since the multiplication factor in PCI agent mode must be an integer.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My clock setting is 200/133/66Mhz, MF =2 ,&amp;nbsp; so the main PLL locks on the falling edge of CLKIN, but the FPGA on my board is a 60x Slave and use the same clock source with CLKIN by a clock buffer(CY2309). Does this affect the CPU startup?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Oct 2015 12:40:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/MPC8260A-Hip4-startup-problem/m-p/434665#M1189</guid>
      <dc:creator>mengjunling</dc:creator>
      <dc:date>2015-10-29T12:40:52Z</dc:date>
    </item>
    <item>
      <title>Re: MPC8260A(Hip4) startup problem?</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/MPC8260A-Hip4-startup-problem/m-p/434666#M1190</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Now I set the SMC in Loopback mode to exclude the affects of external MAX3232,. After power-up, the SMC still can't generate interrupt.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In MPC8260UM, Table 27-2 describe SMC parameter RAM, &lt;/P&gt;&lt;P&gt;"Note 2 Not accessed for normal operation. May hold helpful information for experienced users and for debugging." And how can I get detailed internal state information?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I compared the parameter RAM between Hip3 and Hip4 devices, and found some differences at offset 0x14/0x18.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 Nov 2015 14:10:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/MPC8260A-Hip4-startup-problem/m-p/434666#M1190</guid>
      <dc:creator>mengjunling</dc:creator>
      <dc:date>2015-11-05T14:10:50Z</dc:date>
    </item>
  </channel>
</rss>