<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>PowerQUICC ProcessorsのトピックeTSEC1-RGMII and eTSEC2-MII in MPC8308</title>
    <link>https://community.nxp.com/t5/PowerQUICC-Processors/eTSEC1-RGMII-and-eTSEC2-MII-in-MPC8308/m-p/424097#M1155</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt; In MPC8308 processor i am using eTSEC1 in RGMII mode and eTSEC2 in MII mode,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In MII mode i have two clarifications,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1) i have connected TSEC2_GTX_CLK pin to ground through 1K resistor but in datasheet it is mentioned like &lt;STRONG&gt;This signal feeds back the uninverted transmit clock in MII mode in Detailed Signal Descriptionsso &lt;/STRONG&gt;and i gone through the Design Checklist there it is clearly mentioned like it is not used in MII mode.&lt;/P&gt;&lt;P&gt;2) TSECn_TX_ER this pin in eTSEC1 used as a configuration ECC pin where as in MII mode it suggested to connect to PHY but this pin is not there in the PHY having Part Number &lt;STRONG&gt;KSZ8041NL from MIcrel &lt;/STRONG&gt;so kindly check the need of this signal and kindly share me any reference design which has got MII mode in this series of processors(eTSEC).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;3) TSEC2_TX_CLK i have connected this pin to TX_CLK pin of PHY.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 03 Sep 2015 10:43:06 GMT</pubDate>
    <dc:creator>venkateshn</dc:creator>
    <dc:date>2015-09-03T10:43:06Z</dc:date>
    <item>
      <title>eTSEC1-RGMII and eTSEC2-MII in MPC8308</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/eTSEC1-RGMII-and-eTSEC2-MII-in-MPC8308/m-p/424097#M1155</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt; In MPC8308 processor i am using eTSEC1 in RGMII mode and eTSEC2 in MII mode,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In MII mode i have two clarifications,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1) i have connected TSEC2_GTX_CLK pin to ground through 1K resistor but in datasheet it is mentioned like &lt;STRONG&gt;This signal feeds back the uninverted transmit clock in MII mode in Detailed Signal Descriptionsso &lt;/STRONG&gt;and i gone through the Design Checklist there it is clearly mentioned like it is not used in MII mode.&lt;/P&gt;&lt;P&gt;2) TSECn_TX_ER this pin in eTSEC1 used as a configuration ECC pin where as in MII mode it suggested to connect to PHY but this pin is not there in the PHY having Part Number &lt;STRONG&gt;KSZ8041NL from MIcrel &lt;/STRONG&gt;so kindly check the need of this signal and kindly share me any reference design which has got MII mode in this series of processors(eTSEC).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;3) TSEC2_TX_CLK i have connected this pin to TX_CLK pin of PHY.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Sep 2015 10:43:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/eTSEC1-RGMII-and-eTSEC2-MII-in-MPC8308/m-p/424097#M1155</guid>
      <dc:creator>venkateshn</dc:creator>
      <dc:date>2015-09-03T10:43:06Z</dc:date>
    </item>
    <item>
      <title>Re: eTSEC1-RGMII and eTSEC2-MII in MPC8308</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/eTSEC1-RGMII-and-eTSEC2-MII-in-MPC8308/m-p/424098#M1156</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt; &lt;/P&gt;&lt;P&gt; 1) Yes TSEC2_GTX_CLK is not required for MII interface.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2) According to MII specifications TX_ER (MAC to PHY Transmit error) is an optional signal. PHY’s TX_ER input allows the system MAC to force PHY to deliberately corrupt the transmitted packet. A similar function can be accomplished by having the MAC signal the PHY to stop transmission mid-packet. Since the function of aborting a transmit packet is more easily attained with the latter method, the TX_ER pin may be not implement by PHY.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;3) Yes in MII mode TSEC2_TX_CLK pin is input for transmit clock that provides a timing reference for the TSECn_TX_EN, TSECn_TXD signals.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Sep 2015 15:47:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/eTSEC1-RGMII-and-eTSEC2-MII-in-MPC8308/m-p/424098#M1156</guid>
      <dc:creator>r8070z</dc:creator>
      <dc:date>2015-09-03T15:47:48Z</dc:date>
    </item>
    <item>
      <title>Re: eTSEC1-RGMII and eTSEC2-MII in MPC8308</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/eTSEC1-RGMII-and-eTSEC2-MII-in-MPC8308/m-p/424099#M1157</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN class="j-post-author"&gt;&lt;STRONG&gt;&lt;A href="https://community.nxp.com/people/r8070z"&gt;r8070z&lt;/A&gt;​,&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="j-post-author"&gt;Thanks for your replay,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="j-post-author"&gt;with reference to point no.1 TSEC2_GTX_CLK in the above post please clarify me the below query,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="j-post-author"&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="j-post-author"&gt;For &lt;SPAN class="j-post-author"&gt;TSEC2_GTX_CLK &lt;/SPAN&gt;it is mentioned in datasheet like &lt;STRONG&gt;This signal feeds back the uninverted transmit clock in MII mode &lt;/STRONG&gt;if we are not used this signal in MII mode why they have included above description.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="j-post-author"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="j-post-author"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="j-post-author"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="j-post-author"&gt;&amp;nbsp; &lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 Sep 2015 05:05:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/eTSEC1-RGMII-and-eTSEC2-MII-in-MPC8308/m-p/424099#M1157</guid>
      <dc:creator>venkateshn</dc:creator>
      <dc:date>2015-09-04T05:05:00Z</dc:date>
    </item>
    <item>
      <title>Re: eTSEC1-RGMII and eTSEC2-MII in MPC8308</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/eTSEC1-RGMII-and-eTSEC2-MII-in-MPC8308/m-p/424100#M1158</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I do not know why they wrote that. I think just for information. In any case because in MII mode this pin is an output and do not required for MII so it can be left open.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 Sep 2015 15:52:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/eTSEC1-RGMII-and-eTSEC2-MII-in-MPC8308/m-p/424100#M1158</guid>
      <dc:creator>r8070z</dc:creator>
      <dc:date>2015-09-10T15:52:11Z</dc:date>
    </item>
    <item>
      <title>Re: eTSEC1-RGMII and eTSEC2-MII in MPC8308</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/eTSEC1-RGMII-and-eTSEC2-MII-in-MPC8308/m-p/424101#M1159</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your kind replay,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have following clarification on layer stack up for MPC8308 processor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am going for 8 layer PCB and the stack up is as shown below,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Layer Number&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Layer Name&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Material Type&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Top&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Dielectric&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;	&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Conductive&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;GND1&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Dielectric&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;	&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Conductive&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;3&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sig1&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Dielectric&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;	&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Conductive&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;4&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sig2&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Dielectric&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;	&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Conductive&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;5&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PWR&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Dielectric&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;	&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Conductive&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;6&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sig3&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Dielectric&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;	&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Conductive&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;7&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;GND2&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Dielectric&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;	&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Conductive&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;8&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Bottom&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Dielectric&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;	&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Conductive&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;  Kindly check the reference which I considered is ok r not, waiting for your early replay.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Venkatesh N&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 11 Sep 2015 11:42:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/eTSEC1-RGMII-and-eTSEC2-MII-in-MPC8308/m-p/424101#M1159</guid>
      <dc:creator>venkateshn</dc:creator>
      <dc:date>2015-09-11T11:42:02Z</dc:date>
    </item>
  </channel>
</rss>