<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Signals of CodeWarrior USB TAP Connector. in PowerQUICC Processors</title>
    <link>https://community.nxp.com/t5/PowerQUICC-Processors/Signals-of-CodeWarrior-USB-TAP-Connector/m-p/422892#M1152</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm looking at my USB TAP (CWH-UTP-PPCC-HE) and is confused by the Pins of the connector. The red signal of the ribbon is the first one on the upper side. Does that denote Pin 1? I'm asking because I can't find the user manual for it. The only one I found is CodeWarrior USB TAP Probe, which has the red signal as the last one on the lower side of the ribbon.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Btw, where can I download the driver for CWH-UTP-PPCC-HE?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="IMG_20151118_172615.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/1921i3CD92EFECD121001/image-size/large?v=v2&amp;amp;px=999" role="button" title="IMG_20151118_172615.jpg" alt="IMG_20151118_172615.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 18 Nov 2015 22:34:46 GMT</pubDate>
    <dc:creator>frankzh</dc:creator>
    <dc:date>2015-11-18T22:34:46Z</dc:date>
    <item>
      <title>Signals of CodeWarrior USB TAP Connector.</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/Signals-of-CodeWarrior-USB-TAP-Connector/m-p/422892#M1152</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm looking at my USB TAP (CWH-UTP-PPCC-HE) and is confused by the Pins of the connector. The red signal of the ribbon is the first one on the upper side. Does that denote Pin 1? I'm asking because I can't find the user manual for it. The only one I found is CodeWarrior USB TAP Probe, which has the red signal as the last one on the lower side of the ribbon.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Btw, where can I download the driver for CWH-UTP-PPCC-HE?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="IMG_20151118_172615.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/1921i3CD92EFECD121001/image-size/large?v=v2&amp;amp;px=999" role="button" title="IMG_20151118_172615.jpg" alt="IMG_20151118_172615.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Nov 2015 22:34:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/Signals-of-CodeWarrior-USB-TAP-Connector/m-p/422892#M1152</guid>
      <dc:creator>frankzh</dc:creator>
      <dc:date>2015-11-18T22:34:46Z</dc:date>
    </item>
    <item>
      <title>Re: Signals of CodeWarrior USB TAP Connector.</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/Signals-of-CodeWarrior-USB-TAP-Connector/m-p/422893#M1153</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Red stipe denotes Pin 1 of the COP connector.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The USBTAP driver is provided with CodeWarrior and it is typically installed during CW setup.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can remove/reinstall it following instruction at \CW PA V8.8\ccs\drivers\usb\resdme.txt&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Pavel&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Nov 2015 09:02:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/Signals-of-CodeWarrior-USB-TAP-Connector/m-p/422893#M1153</guid>
      <dc:creator>LPP</dc:creator>
      <dc:date>2015-11-20T09:02:48Z</dc:date>
    </item>
    <item>
      <title>Re: Signals of CodeWarrior USB TAP Connector.</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/Signals-of-CodeWarrior-USB-TAP-Connector/m-p/422894#M1154</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you Pavel.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Nov 2015 21:23:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/Signals-of-CodeWarrior-USB-TAP-Connector/m-p/422894#M1154</guid>
      <dc:creator>frankzh</dc:creator>
      <dc:date>2015-11-20T21:23:05Z</dc:date>
    </item>
  </channel>
</rss>