<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>PowerQUICC ProcessorsのトピックRe: Debugging DMA corruption - MPC8555</title>
    <link>https://community.nxp.com/t5/PowerQUICC-Processors/Debugging-DMA-corruption-MPC8555/m-p/421084#M1148</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;gt;Protection is done through TLBs.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;MMU is located between the core and memory. So, it can provide protection for accesses from core.&lt;/P&gt;&lt;P&gt;DMA has direct access to the memory. MMU can't protect memory from DMA accesses and can't be a reason of DMA fault.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt; Can you share a link to Pro &amp;amp; Linux App Edition Targeting Manual.pdf?&lt;/P&gt;&lt;P&gt;Please, see documentation at CW installation&amp;nbsp; .\CodeWarrior PA V8.8\Help\Pdf\&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Pavel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 23 Nov 2015 10:08:38 GMT</pubDate>
    <dc:creator>LPP</dc:creator>
    <dc:date>2015-11-23T10:08:38Z</dc:date>
    <item>
      <title>Debugging DMA corruption - MPC8555</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/Debugging-DMA-corruption-MPC8555/m-p/421081#M1145</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;wanted to know on how to rule out or convict :-) DMA for a particular memory corruption.&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;It's MPC8555&lt;/LI&gt;&lt;LI&gt;The corruption is in the vector area (starts at 0x0 in our system)&lt;/LI&gt;&lt;LI&gt;The vector area is protected against writes.&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;Can we set a watchpoint on the DAR (DMA Controller)? for the corrupted adddress?&lt;/P&gt;&lt;P&gt;What are the other methods to debug DMA bugs?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Dijo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Nov 2015 10:49:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/Debugging-DMA-corruption-MPC8555/m-p/421081#M1145</guid>
      <dc:creator>dijo</dc:creator>
      <dc:date>2015-11-18T10:49:47Z</dc:date>
    </item>
    <item>
      <title>Re: Debugging DMA corruption - MPC8555</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/Debugging-DMA-corruption-MPC8555/m-p/421082#M1146</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;gt;vector area is protected against writes.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is it DDR? How do you implement protection?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt;What are the other methods to debug DMA bugs?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;CW provides trace buffer support. You can capture information such as transaction types, source ID, and other attributes.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can configure the trace buffer to record all transactions or to record only:&lt;/P&gt;&lt;P&gt;• transactions with a specified source ID&lt;/P&gt;&lt;P&gt;• transactions with a specified target ID&lt;/P&gt;&lt;P&gt;• transactions whose address matches a specified masked address&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Trace window is usedo see the events captured in the trace buffer during a debug session.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please refer to section "EPPC Trace Buffer Support" in "Pro &amp;amp; Linux App Edition Targeting Manual.pdf"&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Pavel&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Nov 2015 10:10:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/Debugging-DMA-corruption-MPC8555/m-p/421082#M1146</guid>
      <dc:creator>LPP</dc:creator>
      <dc:date>2015-11-20T10:10:20Z</dc:date>
    </item>
    <item>
      <title>Re: Debugging DMA corruption - MPC8555</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/Debugging-DMA-corruption-MPC8555/m-p/421083#M1147</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks again! Pavel.&lt;/P&gt;&lt;P&gt;Yes, it's DDR. Protection is done through TLBs.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you share a link to Pro &amp;amp; Linux App Edition Targeting Manual.pdf?&lt;/P&gt;&lt;P&gt;Was not successful in locating one.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Dijo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Nov 2015 11:27:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/Debugging-DMA-corruption-MPC8555/m-p/421083#M1147</guid>
      <dc:creator>dijo</dc:creator>
      <dc:date>2015-11-20T11:27:01Z</dc:date>
    </item>
    <item>
      <title>Re: Debugging DMA corruption - MPC8555</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/Debugging-DMA-corruption-MPC8555/m-p/421084#M1148</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;gt;Protection is done through TLBs.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;MMU is located between the core and memory. So, it can provide protection for accesses from core.&lt;/P&gt;&lt;P&gt;DMA has direct access to the memory. MMU can't protect memory from DMA accesses and can't be a reason of DMA fault.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt; Can you share a link to Pro &amp;amp; Linux App Edition Targeting Manual.pdf?&lt;/P&gt;&lt;P&gt;Please, see documentation at CW installation&amp;nbsp; .\CodeWarrior PA V8.8\Help\Pdf\&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Pavel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 Nov 2015 10:08:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/Debugging-DMA-corruption-MPC8555/m-p/421084#M1148</guid>
      <dc:creator>LPP</dc:creator>
      <dc:date>2015-11-23T10:08:38Z</dc:date>
    </item>
  </channel>
</rss>