<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MPC8379E - 128Mbyte Nor flash interface in PowerQUICC Processors</title>
    <link>https://community.nxp.com/t5/PowerQUICC-Processors/MPC8379E-128Mbyte-Nor-flash-interface/m-p/417912#M1121</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;128Mbyte Nor flash (64M x 16) has 25 address inputs A[0:24], where A0 is the least significant (lsb). The MPC8379 eLBC in Non-Multiplexed mode can support only (32M x 16) because in this mode only 24 lsb of the 31-bit address of 16-bit word can be provided on the LA pins. Hence you need use Multiplexed mode i.e. to use external latch controlled by LALE outputs and latch address from LAD[6:26] pins. The latch outputs need to be connected to the 21 most significant of the NOR flash address inputs (A[24:4]):&lt;/P&gt;&lt;P&gt;8379-&amp;gt;latch--NOR&lt;/P&gt;&lt;P&gt;LAD[6] -&amp;gt;LBA[6]---A24&lt;/P&gt;&lt;P&gt;LAD[7] -&amp;gt;LBA[7]---A23&lt;/P&gt;&lt;P&gt;…&lt;/P&gt;&lt;P&gt;LAD[26] -&amp;gt;LBA[7]---A4&lt;/P&gt;&lt;P&gt;The rest addr. inputs A[4:0] can be connected to the non-multiplexed LA[27:30] outputs&lt;/P&gt;&lt;P&gt;8379 --NOR&lt;/P&gt;&lt;P&gt;LA27—A3&lt;/P&gt;&lt;P&gt;LA28—A2&lt;/P&gt;&lt;P&gt;LA29—A1&lt;/P&gt;&lt;P&gt;LA30—A0&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;16 – bit data are provided on the LAD[0:15] (LAD0 is msb) so recommended connection is&lt;/P&gt;&lt;P&gt;8379 –NOR&lt;/P&gt;&lt;P&gt;LAD[0]—D15&lt;/P&gt;&lt;P&gt;LAD[1]—D14&lt;/P&gt;&lt;P&gt;…&lt;/P&gt;&lt;P&gt;LAD[15]—D0&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Control signals connection is straightforward&lt;/P&gt;&lt;P&gt;LWE to the NOR WE &lt;/P&gt;&lt;P&gt;LOE to the NOR OE&lt;/P&gt;&lt;P&gt;Any one of LCSn to the NOR CE &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can get explanation how to connect NOR Flash in the app. note AN3665 “PowerQUICC Design Checklist. For PowerQUICC II Pro (MPC837x) Devices” You can download it from the Freescale page&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=MPC8379E&amp;amp;fpsp=1&amp;amp;tab=Documentation_Tab" rel="nofollow" target="_blank"&gt;http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=MPC8379E&amp;amp;fpsp=1&amp;amp;tab=Documentation_Tab&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 22 Jun 2015 17:37:48 GMT</pubDate>
    <dc:creator>r8070z</dc:creator>
    <dc:date>2015-06-22T17:37:48Z</dc:date>
    <item>
      <title>MPC8379E - 128Mbyte Nor flash interface</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/MPC8379E-128Mbyte-Nor-flash-interface/m-p/417911#M1120</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Need to interface 128Mbyte Nor flash (64M x 16) to MPC8379E Enhanced Local Bus. Can I have reference.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 22 Jun 2015 09:59:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/MPC8379E-128Mbyte-Nor-flash-interface/m-p/417911#M1120</guid>
      <dc:creator>saravanakumar_s</dc:creator>
      <dc:date>2015-06-22T09:59:42Z</dc:date>
    </item>
    <item>
      <title>Re: MPC8379E - 128Mbyte Nor flash interface</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/MPC8379E-128Mbyte-Nor-flash-interface/m-p/417912#M1121</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;128Mbyte Nor flash (64M x 16) has 25 address inputs A[0:24], where A0 is the least significant (lsb). The MPC8379 eLBC in Non-Multiplexed mode can support only (32M x 16) because in this mode only 24 lsb of the 31-bit address of 16-bit word can be provided on the LA pins. Hence you need use Multiplexed mode i.e. to use external latch controlled by LALE outputs and latch address from LAD[6:26] pins. The latch outputs need to be connected to the 21 most significant of the NOR flash address inputs (A[24:4]):&lt;/P&gt;&lt;P&gt;8379-&amp;gt;latch--NOR&lt;/P&gt;&lt;P&gt;LAD[6] -&amp;gt;LBA[6]---A24&lt;/P&gt;&lt;P&gt;LAD[7] -&amp;gt;LBA[7]---A23&lt;/P&gt;&lt;P&gt;…&lt;/P&gt;&lt;P&gt;LAD[26] -&amp;gt;LBA[7]---A4&lt;/P&gt;&lt;P&gt;The rest addr. inputs A[4:0] can be connected to the non-multiplexed LA[27:30] outputs&lt;/P&gt;&lt;P&gt;8379 --NOR&lt;/P&gt;&lt;P&gt;LA27—A3&lt;/P&gt;&lt;P&gt;LA28—A2&lt;/P&gt;&lt;P&gt;LA29—A1&lt;/P&gt;&lt;P&gt;LA30—A0&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;16 – bit data are provided on the LAD[0:15] (LAD0 is msb) so recommended connection is&lt;/P&gt;&lt;P&gt;8379 –NOR&lt;/P&gt;&lt;P&gt;LAD[0]—D15&lt;/P&gt;&lt;P&gt;LAD[1]—D14&lt;/P&gt;&lt;P&gt;…&lt;/P&gt;&lt;P&gt;LAD[15]—D0&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Control signals connection is straightforward&lt;/P&gt;&lt;P&gt;LWE to the NOR WE &lt;/P&gt;&lt;P&gt;LOE to the NOR OE&lt;/P&gt;&lt;P&gt;Any one of LCSn to the NOR CE &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can get explanation how to connect NOR Flash in the app. note AN3665 “PowerQUICC Design Checklist. For PowerQUICC II Pro (MPC837x) Devices” You can download it from the Freescale page&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=MPC8379E&amp;amp;fpsp=1&amp;amp;tab=Documentation_Tab" rel="nofollow" target="_blank"&gt;http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=MPC8379E&amp;amp;fpsp=1&amp;amp;tab=Documentation_Tab&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 22 Jun 2015 17:37:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/MPC8379E-128Mbyte-Nor-flash-interface/m-p/417912#M1121</guid>
      <dc:creator>r8070z</dc:creator>
      <dc:date>2015-06-22T17:37:48Z</dc:date>
    </item>
  </channel>
</rss>