<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MPC8306_SOM in PowerQUICC Processors</title>
    <link>https://community.nxp.com/t5/PowerQUICC-Processors/MPC8306-SOM/m-p/399732#M1049</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Good morning,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a question about FREESCALE MPC8306_SOM.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have the MPC830x kit, that includes:&lt;/P&gt;&lt;P&gt; - MPC830X carrier card&lt;/P&gt;&lt;P&gt; - MPC 8306 SOM Rev C&lt;/P&gt;&lt;P&gt;I use the CodeWarrior TAP in order to program the MPC 8306 SOM.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have installed the codewarrior v8.8, and I have connected the TAP to PC by USB cable and I set the speed of TAP at 10MHz.&lt;/P&gt;&lt;P&gt;I have done a simply project in codewarrior that writes a phrase on serial (COM2).&lt;/P&gt;&lt;P&gt;In order to program the MPC8306, I have done the procedure that erase the flash memory with codewarrior (Tools-&amp;gt;Flash programmer, etc..).&lt;/P&gt;&lt;P&gt;I tryed my program on MPC8306 SOM and it works correctly.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My problem is that sometimes I can't erase the Flash, and I can't write into it..&lt;/P&gt;&lt;P&gt;If I can't erase/write the flash one time, I can't do it anymore.. &lt;/P&gt;&lt;P&gt;If I retry, I can't write or erase anymore the flash..&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tryed several attempts:&lt;/P&gt;&lt;P&gt; - I have restarted the MPC8306 SOM&lt;/P&gt;&lt;P&gt; - I have restarted the codeWarrior TAP&lt;/P&gt;&lt;P&gt; - I have restarted the codeWarrior&lt;/P&gt;&lt;P&gt; - I also rebooted the PC..&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Despite attempts I cant write or erase the flash on MPC8306 SOM..&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Did Someone had problems with codeWarrior TAP? And with MPC8306 SOM rev C?&lt;/P&gt;&lt;P&gt;How can I solve my problems of programming?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;/P&gt;&lt;P&gt;Marco.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 15 Jun 2015 07:32:55 GMT</pubDate>
    <dc:creator>marcomaioli</dc:creator>
    <dc:date>2015-06-15T07:32:55Z</dc:date>
    <item>
      <title>MPC8306_SOM</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/MPC8306-SOM/m-p/399732#M1049</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Good morning,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a question about FREESCALE MPC8306_SOM.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have the MPC830x kit, that includes:&lt;/P&gt;&lt;P&gt; - MPC830X carrier card&lt;/P&gt;&lt;P&gt; - MPC 8306 SOM Rev C&lt;/P&gt;&lt;P&gt;I use the CodeWarrior TAP in order to program the MPC 8306 SOM.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have installed the codewarrior v8.8, and I have connected the TAP to PC by USB cable and I set the speed of TAP at 10MHz.&lt;/P&gt;&lt;P&gt;I have done a simply project in codewarrior that writes a phrase on serial (COM2).&lt;/P&gt;&lt;P&gt;In order to program the MPC8306, I have done the procedure that erase the flash memory with codewarrior (Tools-&amp;gt;Flash programmer, etc..).&lt;/P&gt;&lt;P&gt;I tryed my program on MPC8306 SOM and it works correctly.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My problem is that sometimes I can't erase the Flash, and I can't write into it..&lt;/P&gt;&lt;P&gt;If I can't erase/write the flash one time, I can't do it anymore.. &lt;/P&gt;&lt;P&gt;If I retry, I can't write or erase anymore the flash..&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tryed several attempts:&lt;/P&gt;&lt;P&gt; - I have restarted the MPC8306 SOM&lt;/P&gt;&lt;P&gt; - I have restarted the codeWarrior TAP&lt;/P&gt;&lt;P&gt; - I have restarted the codeWarrior&lt;/P&gt;&lt;P&gt; - I also rebooted the PC..&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Despite attempts I cant write or erase the flash on MPC8306 SOM..&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Did Someone had problems with codeWarrior TAP? And with MPC8306 SOM rev C?&lt;/P&gt;&lt;P&gt;How can I solve my problems of programming?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;/P&gt;&lt;P&gt;Marco.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 15 Jun 2015 07:32:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/MPC8306-SOM/m-p/399732#M1049</guid>
      <dc:creator>marcomaioli</dc:creator>
      <dc:date>2015-06-15T07:32:55Z</dc:date>
    </item>
    <item>
      <title>Re: MPC8306_SOM</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/MPC8306-SOM/m-p/399733#M1050</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Marco Maioli,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What's your detail error? You can share at which step is your failure?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For CodeWarrior 8.8, please be aware that patch 8.8.6 and 8.8.5 are needed for CodeWarrior TAP and Windows 7.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Lunmin&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 15 Jun 2015 09:43:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/MPC8306-SOM/m-p/399733#M1050</guid>
      <dc:creator>lunminliang</dc:creator>
      <dc:date>2015-06-15T09:43:03Z</dc:date>
    </item>
  </channel>
</rss>