<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>PowerQUICC ProcessorsのトピックProblem setting SRDS registers</title>
    <link>https://community.nxp.com/t5/PowerQUICC-Processors/Problem-setting-SRDS-registers/m-p/399432#M1046</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm trying to use the SATA devices in the MPC8379 evalutaion board. I'm having problems while updating the SRDS registers so it's programmed to use SATA interface. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm trying to set the following values:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;SRDSCR0: 0x1100CC30&lt;/P&gt;&lt;P&gt;SRDSCR1: 0x00000040&lt;/P&gt;&lt;P&gt;SRDSCR2: 0x00001414&lt;/P&gt;&lt;P&gt;SRDSCR3: 0x15150528&lt;/P&gt;&lt;P&gt;SRDSCR4: 0x40000808&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However this registers are always with the reset values. Should I do something else before being able to edit those registers?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 27 May 2015 11:06:13 GMT</pubDate>
    <dc:creator>carlessilva</dc:creator>
    <dc:date>2015-05-27T11:06:13Z</dc:date>
    <item>
      <title>Problem setting SRDS registers</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/Problem-setting-SRDS-registers/m-p/399432#M1046</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm trying to use the SATA devices in the MPC8379 evalutaion board. I'm having problems while updating the SRDS registers so it's programmed to use SATA interface. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm trying to set the following values:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;SRDSCR0: 0x1100CC30&lt;/P&gt;&lt;P&gt;SRDSCR1: 0x00000040&lt;/P&gt;&lt;P&gt;SRDSCR2: 0x00001414&lt;/P&gt;&lt;P&gt;SRDSCR3: 0x15150528&lt;/P&gt;&lt;P&gt;SRDSCR4: 0x40000808&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However this registers are always with the reset values. Should I do something else before being able to edit those registers?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 May 2015 11:06:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/Problem-setting-SRDS-registers/m-p/399432#M1046</guid>
      <dc:creator>carlessilva</dc:creator>
      <dc:date>2015-05-27T11:06:13Z</dc:date>
    </item>
    <item>
      <title>Re: Problem setting SRDS registers</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/Problem-setting-SRDS-registers/m-p/399433#M1047</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN lang="EN-US" style="font-size: 10.0pt;"&gt;Look at the Section 19.4 of the MPC8379 Reference Manual. This Section contains command sequence for &lt;/SPAN&gt;&lt;SPAN lang="EN-US" style="font-size: 10.0pt;"&gt;SerDes and PHY initialization and Reset. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="EN-US" style="font-size: 10.0pt;"&gt;Test your board using this command sequence.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Pavel&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 May 2015 05:42:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/Problem-setting-SRDS-registers/m-p/399433#M1047</guid>
      <dc:creator>Pavel</dc:creator>
      <dc:date>2015-05-28T05:42:34Z</dc:date>
    </item>
    <item>
      <title>Re: Problem setting SRDS registers</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/Problem-setting-SRDS-registers/m-p/399434#M1048</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Pavel,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks for your response. This is exactly the sequence I'm following but still SATA device's are not working. I'm following the code I'm using in the MPC8315, adding the initialization of the SerDes PHY. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any clue in what the problem may be?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 May 2015 10:40:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/Problem-setting-SRDS-registers/m-p/399434#M1048</guid>
      <dc:creator>carlessilva</dc:creator>
      <dc:date>2015-05-28T10:40:44Z</dc:date>
    </item>
  </channel>
</rss>