<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Multiple Targets and PE in Processor Expert Software</title>
    <link>https://community.nxp.com/t5/Processor-Expert-Software/Multiple-Targets-and-PE/m-p/204851#M827</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Erich-&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So does adding a CPU in PE automatically add a build configuration? I didn't notice it doing that on our systems, but has that changed in the 10.3 beta?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 12 Dec 2012 13:14:10 GMT</pubDate>
    <dc:creator>Jeinstei</dc:creator>
    <dc:date>2012-12-12T13:14:10Z</dc:date>
    <item>
      <title>Multiple Targets and PE</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Multiple-Targets-and-PE/m-p/204849#M825</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is there an easy way to manage build/debug configurations when adding CPUs in PE? We want to be able to easily switch between our target and the TWR kits, but it looks like PE doesn't automatically add Debug and Build configurations. Any tips?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Dec 2012 21:27:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Multiple-Targets-and-PE/m-p/204849#M825</guid>
      <dc:creator>Jeinstei</dc:creator>
      <dc:date>2012-12-11T21:27:14Z</dc:date>
    </item>
    <item>
      <title>Re: Multiple Targets and PE</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Multiple-Targets-and-PE/m-p/204850#M826</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, you can do this. Simply add your Debug build configuration.&lt;/P&gt;&lt;P&gt;On the PE side, there are configurations as well (you can add a configuration, and then disable/enable components for it.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Dec 2012 05:06:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Multiple-Targets-and-PE/m-p/204850#M826</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2012-12-12T05:06:45Z</dc:date>
    </item>
    <item>
      <title>Re: Multiple Targets and PE</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Multiple-Targets-and-PE/m-p/204851#M827</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Erich-&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So does adding a CPU in PE automatically add a build configuration? I didn't notice it doing that on our systems, but has that changed in the 10.3 beta?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Dec 2012 13:14:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Multiple-Targets-and-PE/m-p/204851#M827</guid>
      <dc:creator>Jeinstei</dc:creator>
      <dc:date>2012-12-12T13:14:10Z</dc:date>
    </item>
    <item>
      <title>Re: Multiple Targets and PE</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Multiple-Targets-and-PE/m-p/204852#M828</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Joshua,&lt;/P&gt;&lt;P&gt;no, you need to add a configuration for it. See &lt;A href="http://mcuoneclipse.com/2012/03/07/configurations-with-processor-expert/" title="http://mcuoneclipse.com/2012/03/07/configurations-with-processor-expert/"&gt;Configurations with Processor Expert | MCU on Eclipse.&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Dec 2012 14:12:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Multiple-Targets-and-PE/m-p/204852#M828</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2012-12-12T14:12:49Z</dc:date>
    </item>
    <item>
      <title>Re: Multiple Targets and PE</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Multiple-Targets-and-PE/m-p/204853#M829</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Erich- I understand this. But I am wondering about the higher (lower?) level eclipse build configurations, such as PK40X256_INTERNAL_FLASH. These are separate from the PE configurations, and are where files are pulled from for the Debug configurations. PE can be set to use a K10, and still have all it's object files pushed to a K40 build configuration at a higher level.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It makes sense to have these decoupled for code generation, but it would be nice to have an option in the PE configurations to "Generate a CW build configuration for this PE configuration"&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Dec 2012 14:16:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Multiple-Targets-and-PE/m-p/204853#M829</guid>
      <dc:creator>Jeinstei</dc:creator>
      <dc:date>2012-12-12T14:16:34Z</dc:date>
    </item>
    <item>
      <title>Re: Multiple Targets and PE</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Multiple-Targets-and-PE/m-p/204854#M830</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Joshua,&lt;/P&gt;&lt;P&gt;Maybe I have misunderstood your question?&lt;/P&gt;&lt;P&gt;In any case: to manage build configurations, use the menu Project &amp;gt; Build Configurations &amp;gt; Manage.&lt;/P&gt;&lt;P&gt;The output folder is controlled by the build tool settings (Project &amp;gt; Properties &amp;gt; C/C++ build &amp;gt; Builder Settings &amp;gt; Build Location.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If it is about to tie Processor Expert configurations to Eclipse Build configurations: I think this is possible, but I have not used it like this.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Dec 2012 14:23:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Multiple-Targets-and-PE/m-p/204854#M830</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2012-12-12T14:23:56Z</dc:date>
    </item>
    <item>
      <title>Re: Multiple Targets and PE</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Multiple-Targets-and-PE/m-p/204855#M831</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Erich. I guess the answer is: maybe then.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the help! We'll try to work something out on our end then.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Dec 2012 14:26:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Multiple-Targets-and-PE/m-p/204855#M831</guid>
      <dc:creator>Jeinstei</dc:creator>
      <dc:date>2012-12-12T14:26:46Z</dc:date>
    </item>
    <item>
      <title>Re: Multiple Targets and PE</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Multiple-Targets-and-PE/m-p/204856#M832</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using KDS 3.2.0 for K10.&amp;nbsp; Have been trying to tie the PE Generator_Configuration to the Eclipse Build Configuration, i.e., PE has RAM and FLASH configs.&amp;nbsp; But I want also to have different Build Configs that select different PE configs, having trouble with that.&amp;nbsp; Oddly the PE beans get correctly selected (one of two CPU configs), but the RAM/FLASH config does not follow the Eclipse Build config at all.&amp;nbsp; Any ideas?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 Mar 2016 20:08:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Multiple-Targets-and-PE/m-p/204856#M832</guid>
      <dc:creator>talktrn</dc:creator>
      <dc:date>2016-03-30T20:08:45Z</dc:date>
    </item>
  </channel>
</rss>