<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Processor Expert SoftwareのトピックRe: Enable RX pin pull-ups using AsynchroSerial component</title>
    <link>https://community.nxp.com/t5/Processor-Expert-Software/Enable-RX-pin-pull-ups-using-AsynchroSerial-component/m-p/203947#M822</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am sorry, unforrtunatelly there is no such option available in PEx for HCS08 now. However it should be supported in the future within the planned PinMuxig tool.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;For now as workaround there is the only possibility to handle the pull-up functionality in user code.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;best regards&lt;BR /&gt;Vojtech Filip&lt;BR /&gt;Processor Expert Support Team&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 08 Feb 2012 23:46:01 GMT</pubDate>
    <dc:creator>ProcessorExpert</dc:creator>
    <dc:date>2012-02-08T23:46:01Z</dc:date>
    <item>
      <title>Enable RX pin pull-ups using AsynchroSerial component</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Enable-RX-pin-pull-ups-using-AsynchroSerial-component/m-p/203946#M821</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am working with the HC(S)08 and have integrated the AsynchroSerial component.&amp;nbsp; I need to enable the pull-up on the RxD pin, so the pin does not float when the component is disabled.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;There are no pull-up options for the port pin in the AsynchroSerial properties.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I see some pull-up options for Port E in the CPU component, but this is for unused pins only.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I tried adding a Init_GPIO component and of course this says there is a conflict with the AsynchroSerial component and it won't build.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Without just resorting to writing directly to the port register in the code, what is the correct way to control the pull-up register for the RxD pin?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 Feb 2012 07:23:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Enable-RX-pin-pull-ups-using-AsynchroSerial-component/m-p/203946#M821</guid>
      <dc:creator>jgirard1</dc:creator>
      <dc:date>2012-02-08T07:23:30Z</dc:date>
    </item>
    <item>
      <title>Re: Enable RX pin pull-ups using AsynchroSerial component</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Enable-RX-pin-pull-ups-using-AsynchroSerial-component/m-p/203947#M822</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am sorry, unforrtunatelly there is no such option available in PEx for HCS08 now. However it should be supported in the future within the planned PinMuxig tool.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;For now as workaround there is the only possibility to handle the pull-up functionality in user code.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;best regards&lt;BR /&gt;Vojtech Filip&lt;BR /&gt;Processor Expert Support Team&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 Feb 2012 23:46:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Enable-RX-pin-pull-ups-using-AsynchroSerial-component/m-p/203947#M822</guid>
      <dc:creator>ProcessorExpert</dc:creator>
      <dc:date>2012-02-08T23:46:01Z</dc:date>
    </item>
  </channel>
</rss>