<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Missing SPI PEx bean / CodeWarrior 10.2 in Processor Expert Software</title>
    <link>https://community.nxp.com/t5/Processor-Expert-Software/Missing-SPI-PEx-bean-CodeWarrior-10-2/m-p/202932#M800</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think that the best way to find corresponding component(s) to the device is to right click on the CPU component in the project and select "View Target CPU package" command. After that go to this window and right click on the device. In the pop-up menu you should be able to see the list of the available components.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;best regards&lt;/P&gt;&lt;P&gt;Vojtech Filip&lt;/P&gt;&lt;P&gt;Processor Expert Support Team&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 11 Dec 2012 07:50:07 GMT</pubDate>
    <dc:creator>vfilip</dc:creator>
    <dc:date>2012-12-11T07:50:07Z</dc:date>
    <item>
      <title>Missing SPI PEx bean / CodeWarrior 10.2</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Missing-SPI-PEx-bean-CodeWarrior-10-2/m-p/202931#M799</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;MC9S08GT32 - this has hardware SPI. Looking under CPU -&amp;gt; Used -&amp;gt; Peripheral Modules in Component Inspector, I can see SPI1 "ready for use in PE."&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, if I look under the alphabetical listing in Components Library, the only mention of SPI I can find is the bit-banged SWSPI and INIT_SPI.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Am I missing something here? All the other internal peripherals I'm using are there.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 10 Dec 2012 22:18:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Missing-SPI-PEx-bean-CodeWarrior-10-2/m-p/202931#M799</guid>
      <dc:creator>Smiffytech</dc:creator>
      <dc:date>2012-12-10T22:18:01Z</dc:date>
    </item>
    <item>
      <title>Re: Missing SPI PEx bean / CodeWarrior 10.2</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Missing-SPI-PEx-bean-CodeWarrior-10-2/m-p/202932#M800</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think that the best way to find corresponding component(s) to the device is to right click on the CPU component in the project and select "View Target CPU package" command. After that go to this window and right click on the device. In the pop-up menu you should be able to see the list of the available components.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;best regards&lt;/P&gt;&lt;P&gt;Vojtech Filip&lt;/P&gt;&lt;P&gt;Processor Expert Support Team&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Dec 2012 07:50:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Missing-SPI-PEx-bean-CodeWarrior-10-2/m-p/202932#M800</guid>
      <dc:creator>vfilip</dc:creator>
      <dc:date>2012-12-11T07:50:07Z</dc:date>
    </item>
    <item>
      <title>Re: Missing SPI PEx bean / CodeWarrior 10.2</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Missing-SPI-PEx-bean-CodeWarrior-10-2/m-p/202933#M801</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The hardware SPI components are named 'SynchroMaster' (for master) and 'SynchroSlave' for SPI slave.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Dec 2012 08:00:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Missing-SPI-PEx-bean-CodeWarrior-10-2/m-p/202933#M801</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2012-12-11T08:00:23Z</dc:date>
    </item>
    <item>
      <title>Re: Missing SPI PEx bean / CodeWarrior 10.2</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Missing-SPI-PEx-bean-CodeWarrior-10-2/m-p/202934#M802</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ah, now that's something worth knowing - didn't know you could do that. Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Dec 2012 19:44:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Missing-SPI-PEx-bean-CodeWarrior-10-2/m-p/202934#M802</guid>
      <dc:creator>Smiffytech</dc:creator>
      <dc:date>2012-12-11T19:44:50Z</dc:date>
    </item>
    <item>
      <title>Re: Missing SPI PEx bean / CodeWarrior 10.2</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Missing-SPI-PEx-bean-CodeWarrior-10-2/m-p/202935#M803</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ah, nothing like being consistent in how things are named :smileywink:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks, Erich.&amp;nbsp; Now I just have to try to remember it's called something else for next time!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Dec 2012 19:45:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Missing-SPI-PEx-bean-CodeWarrior-10-2/m-p/202935#M803</guid>
      <dc:creator>Smiffytech</dc:creator>
      <dc:date>2012-12-11T19:45:55Z</dc:date>
    </item>
  </channel>
</rss>