<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Processor Expert SoftwareのトピックRe: How to Reserve JTAG pins</title>
    <link>https://community.nxp.com/t5/Processor-Expert-Software/How-to-Reserve-JTAG-pins/m-p/202530#M798</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I’m afraid that for MC56F8257 it is not possible to show JTAG pins on package view or reserve them for JTAG purpose as there is no JTAG/EOnCE component available.&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Calibri','sans-serif'; font-size: 11pt;"&gt;As a workaround, it is possible to add Init_GPIO component to the project and configure it to use JTAG pins, however you have to switch to “no” the &lt;EM&gt;Call Init metod&lt;/EM&gt; property in &lt;EM&gt;Initialization&lt;/EM&gt; group (placed at the bottom of Init_GPIO component). This is necessary, otherwise, after the Processor Expert initialization, the pins will be re-routed as GPIO instead of default JTAG functionality. This way, the pins will be shown as used (although as by Init_GPIO) in the Processor package view.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 11 Dec 2012 11:30:35 GMT</pubDate>
    <dc:creator>Lukas_Heczko</dc:creator>
    <dc:date>2012-12-11T11:30:35Z</dc:date>
    <item>
      <title>How to Reserve JTAG pins</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/How-to-Reserve-JTAG-pins/m-p/202529#M797</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using a MC56F8257.&amp;nbsp; In Processor Expert, what component can I configure so that the JTAG pins will show up as "used" in the Processor window? I understand that they are JTAG pins by default, and hence don't really need to be configured - but there must be something I can select so that the pins are shown as used on the processor pinout.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 10 Dec 2012 19:27:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/How-to-Reserve-JTAG-pins/m-p/202529#M797</guid>
      <dc:creator>ivekengineer</dc:creator>
      <dc:date>2012-12-10T19:27:13Z</dc:date>
    </item>
    <item>
      <title>Re: How to Reserve JTAG pins</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/How-to-Reserve-JTAG-pins/m-p/202530#M798</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I’m afraid that for MC56F8257 it is not possible to show JTAG pins on package view or reserve them for JTAG purpose as there is no JTAG/EOnCE component available.&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Calibri','sans-serif'; font-size: 11pt;"&gt;As a workaround, it is possible to add Init_GPIO component to the project and configure it to use JTAG pins, however you have to switch to “no” the &lt;EM&gt;Call Init metod&lt;/EM&gt; property in &lt;EM&gt;Initialization&lt;/EM&gt; group (placed at the bottom of Init_GPIO component). This is necessary, otherwise, after the Processor Expert initialization, the pins will be re-routed as GPIO instead of default JTAG functionality. This way, the pins will be shown as used (although as by Init_GPIO) in the Processor package view.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Dec 2012 11:30:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/How-to-Reserve-JTAG-pins/m-p/202530#M798</guid>
      <dc:creator>Lukas_Heczko</dc:creator>
      <dc:date>2012-12-11T11:30:35Z</dc:date>
    </item>
  </channel>
</rss>