<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Processor Expert SoftwareのトピックKinetis Can frame retransmission</title>
    <link>https://community.nxp.com/t5/Processor-Expert-Software/Kinetis-Can-frame-retransmission/m-p/200621#M761</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi , I am trying to use FlexCan on K60 with PLL 96MHz ( cristal 8MHz). When I set up bitrate from Processor Expert to 20kbps and standard parameters (Propagation segment:0, seg1 : 7, seg 2: 3, RSJ: 1, One Sample) everything is ok. After changing value of bit rate to 250kbps or 500kbps Can frame is retransmitted 3 and 5 times ( I dont change anything in code just parameters in Processor Expert ) to external device . &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 25 Sep 2012 16:27:28 GMT</pubDate>
    <dc:creator>bataliero</dc:creator>
    <dc:date>2012-09-25T16:27:28Z</dc:date>
    <item>
      <title>Kinetis Can frame retransmission</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Kinetis-Can-frame-retransmission/m-p/200621#M761</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi , I am trying to use FlexCan on K60 with PLL 96MHz ( cristal 8MHz). When I set up bitrate from Processor Expert to 20kbps and standard parameters (Propagation segment:0, seg1 : 7, seg 2: 3, RSJ: 1, One Sample) everything is ok. After changing value of bit rate to 250kbps or 500kbps Can frame is retransmitted 3 and 5 times ( I dont change anything in code just parameters in Processor Expert ) to external device . &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 25 Sep 2012 16:27:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Kinetis-Can-frame-retransmission/m-p/200621#M761</guid>
      <dc:creator>bataliero</dc:creator>
      <dc:date>2012-09-25T16:27:28Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis Can frame retransmission</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Kinetis-Can-frame-retransmission/m-p/200622#M762</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There might be a problem with CAN settings - please see check properties Segment, segment1,2. These settings are sensitive especially for high CAN bitrates. These settings should be set according to capacitance of the CAN bus. The repeated transmissions may occur because MK60 doesn't get acknowledge from the counterpart device, so the FlexCAN repeats sending frame while invoking the OnError event. Please try to enable OnError event and put there an error handling code. You can use there the GetError() method that returns a type of the error (e.g. ACK error).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;best regards&lt;/P&gt;&lt;P&gt;Petr Hradsky&lt;/P&gt;&lt;P&gt;Processor Expert Support Team&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Oct 2012 12:37:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Kinetis-Can-frame-retransmission/m-p/200622#M762</guid>
      <dc:creator>Petr_H</dc:creator>
      <dc:date>2012-10-09T12:37:54Z</dc:date>
    </item>
  </channel>
</rss>