<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Processor Expert Software中的主题 Re: CPU Bean Disable</title>
    <link>https://community.nxp.com/t5/Processor-Expert-Software/CPU-Bean-Disable/m-p/199840#M758</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I think that in case of bootloader project it´s not neceesary to disable re-generation of the whole CPU.c module. Processor Expert (PE) provides features to rediretion of reset vector or redirection the vector table - please see “Internal resource mapping“ group in CPU component.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;You can find PE bootloader example project beased on AN3561 under the following link.&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.freescale.com/message/61051#61051" title="https://community.freescale.com/message/61051#61051"&gt;https://community.freescale.com/message/61051#61051&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;best regards&lt;BR /&gt;Vojtech Filip&lt;BR /&gt;Processor Expert Support Team&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 26 Apr 2011 21:51:42 GMT</pubDate>
    <dc:creator>ProcessorExpert</dc:creator>
    <dc:date>2011-04-26T21:51:42Z</dc:date>
    <item>
      <title>CPU Bean Disable</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/CPU-Bean-Disable/m-p/199835#M753</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a code which requires CPU bean to be disabled in order to prevent user changes. However, with processor expert I can disable all other beans but not the CPU Bean. By not able to do this, I need to manually edit in cpu.c everytime it is compiled for teh first time, else it gives linker error. So, is there a way to disable CPU bean generation in PE?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Apr 2011 06:52:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/CPU-Bean-Disable/m-p/199835#M753</guid>
      <dc:creator>Punit</dc:creator>
      <dc:date>2011-04-20T06:52:22Z</dc:date>
    </item>
    <item>
      <title>Re: CPU Bean Disable</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/CPU-Bean-Disable/m-p/199836#M754</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Are you using CW MCU10.1? There you can right click on the CPU and select 'Code Generation' &amp;gt; 'Don't write generated component module'.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;BK&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Apr 2011 12:07:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/CPU-Bean-Disable/m-p/199836#M754</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2011-04-20T12:07:00Z</dc:date>
    </item>
    <item>
      <title>Re: CPU Bean Disable</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/CPU-Bean-Disable/m-p/199837#M755</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using CW V6.3 and it has this option disabled ie "'Don't write generated component module" is disabled/not highted so you can not select. However, this is not the case for any of the other beans.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Apr 2011 23:35:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/CPU-Bean-Disable/m-p/199837#M755</guid>
      <dc:creator>Punit</dc:creator>
      <dc:date>2011-04-20T23:35:31Z</dc:date>
    </item>
    <item>
      <title>Re: CPU Bean Disable</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/CPU-Bean-Disable/m-p/199838#M756</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;It´s not possible to disable code generation of CPU component in CW Classic. In this case it´s necessary to freeze the whole project using "Freeze Generated Code" menu command from "Processor Expert" menu. You can find more details also in PE help: User Interface &amp;gt; Main Menu &amp;gt; Freeze Generate Code&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;There are also options "User code before PE initialization" and "User code after PE initialization" in Build options tab in CPU component that allow add a user code into CPU initialization function (__initialize_hardware, _EntryPoint, etc.).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Could you please specify what exactly do you need to do?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;best regards&lt;BR /&gt;Vojtech Filip&lt;BR /&gt;Processor Expert Support Team&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Apr 2011 15:19:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/CPU-Bean-Disable/m-p/199838#M756</guid>
      <dc:creator>ProcessorExpert</dc:creator>
      <dc:date>2011-04-21T15:19:50Z</dc:date>
    </item>
    <item>
      <title>Re: CPU Bean Disable</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/CPU-Bean-Disable/m-p/199839#M757</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a project which uses two programs in Flash. So the Program 1 is bootloader code and program 2 is Application code.&lt;/P&gt;&lt;P&gt;I am using&amp;nbsp;vector table in&amp;nbsp;Bootloader code. Whenever there is an Interrupt the Programn jumps to Bootlaoder code space which redirects to Application code. So in my application code I need to rename all the ISRs to general functions, which I can do except for CPU ISR. If you need&amp;nbsp;further information you can search for the questions asked by me previously.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;So, everything works great but when some other programmer opens&amp;nbsp;this application&amp;nbsp;code, due to auto generation feature of CPU Bean the user defined functions gets changed into ISR and linker errors.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 Apr 2011 04:25:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/CPU-Bean-Disable/m-p/199839#M757</guid>
      <dc:creator>Punit</dc:creator>
      <dc:date>2011-04-22T04:25:55Z</dc:date>
    </item>
    <item>
      <title>Re: CPU Bean Disable</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/CPU-Bean-Disable/m-p/199840#M758</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I think that in case of bootloader project it´s not neceesary to disable re-generation of the whole CPU.c module. Processor Expert (PE) provides features to rediretion of reset vector or redirection the vector table - please see “Internal resource mapping“ group in CPU component.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;You can find PE bootloader example project beased on AN3561 under the following link.&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.freescale.com/message/61051#61051" title="https://community.freescale.com/message/61051#61051"&gt;https://community.freescale.com/message/61051#61051&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;best regards&lt;BR /&gt;Vojtech Filip&lt;BR /&gt;Processor Expert Support Team&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Apr 2011 21:51:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/CPU-Bean-Disable/m-p/199840#M758</guid>
      <dc:creator>ProcessorExpert</dc:creator>
      <dc:date>2011-04-26T21:51:42Z</dc:date>
    </item>
  </channel>
</rss>